Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum My Christmas RPi is rockin, my Wi-Pi..not so much. What am I doing wrong....
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 707 subscribers
  • Views 2304 views
  • Users 0 members are here
  • raspi-config
  • raspberry_pi
  • wipi
  • raspberry_pi_accessories
Related

My Christmas RPi is rockin, my Wi-Pi..not so much. What am I doing wrong....

e14 Contributor
e14 Contributor over 13 years ago

Because I know it's something I'm doing wrong.

 

I saw the Adafruit video of the Motorola Atrix lapdock being used with the RPi and I thought "gotta do that". So I made the cable and for the first time powered up my Christmas RPi and it worked perfectly. I had downloaded the Wheezy (2012-10-28) image off the RPi Foundation site and burned an SD card and it all worked bloody perfect.  Then I installed the Wi-Pi and ground to a halt as I tried to figure out why the WiPi refused to work. I followed the PDF instructions on the Element14 site and modified the 'interfaces' file and checked it a bunch of times but no go. The indicator light on the WiPi is not on and although it appears the OS is sensing the dongle it does not appear to be able to connect to the access point.

Here's what I appended in the interfaces file;

 

 

auto wlan0

iface wlan0 inet dhcp

wpa-ssid Le-Mars

wpa-psk #############   (this was the actual password)

 

 

Oct 28 22:59:47 raspberrypi kernel: [    3.283301] usb 1-1.2: new high-speed USB device number 4 using dwc_otg
Oct 28 22:59:47 raspberrypi kernel: [    3.411226] usb 1-1.2: New USB device found, idVendor=148f, idProduct=5370
Oct 28 22:59:47 raspberrypi kernel: [    3.423516] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
Oct 28 22:59:47 raspberrypi kernel: [    3.437190] usb 1-1.2: Product: 802.11 n WLAN
Oct 28 22:59:47 raspberrypi kernel: [    3.446827] usb 1-1.2: Manufacturer: Ralink
Oct 28 22:59:47 raspberrypi kernel: [    3.456369] usb 1-1.2: SerialNumber: 1.0
Oct 28 22:59:47 raspberrypi kernel: [    3.563310] usb 1-1.3: new high-speed USB device number 5 using dwc_otg
Oct 28 22:59:47 raspberrypi kernel: [    3.693815] usb 1-1.3: New USB device found, idVendor=0424, idProduct=2517
Oct 28 22:59:47 raspberrypi kernel: [    3.715064] usb 1-1.3: New USB device strings: Mfr=0, Product=0, SerialNumber=0

The router is looking for 802.11g using WPA. It can output 'n' as well but my old Mac Mini gets extra stupid when 'n' packets are mixed into the stream.

this is a snippet of the bootup syslog which (I think) shows that the RPi is seeing the WiPi however later when it tries to do a DHCP it fails out completly.

 

I also measured the voltage between TP1 and TP2 and it showed 4.80v with the WiPi in and 4.85v with it out. The lapdock certainly appears to be delivering solid power to the RPi with the added benefit of battery backup power for 'free'.

 

I'm kinda stumped and I don't know where to go If anybody has got any ideas I would be extremely gratefull.

 

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Glad you got it working Bill.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

     

    Paul Bryant wrote:

     

    It's plugged directly into the RPi top USB slot, and it works perfectly. I read on another board that you don't want to plug the WiFi dongle into a hub and that it only works reliably if it's directly connected to the RPi. I have to say I am gobsmacked at how cool the Atrix lapdock works with the RPi. How it works out the correct screen res I do not know. It will be a bit of a giggle to take over the Lapdock/RPi and sit in Starbucks on battery power just like all the big kids do....

           Paul,

           I had my WiPi plugged into the USB port on the Pi and I was having problems, I plugged it into a powered hub (Belkin) and it works fine.  I checked the voltage (TP1-TP2) and it is 5.0. The Lapdock is the greatest!

     

           Bill, I think you have a German keyboard like I do.  It takes a little getting used to especially since it is marked like a US keyboard. Maybe someone knows how to change Debian from thinking it is German!



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    George Golden wrote:

     

           Bill, I think you have a German keyboard like I do.  It takes a little getting used to especially since it is marked like a US keyboard. Maybe someone knows how to change Debian from thinking it is German!

    There are instructions for changing the default "gb" = Great Britain keyboard mapping to something else at the RasPi Troubleshooting Wiki.  The instructions are for Debian Squeeze, but may work with Wheezy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Actually George, regarding the dongle you are absolutly right. I'm having trouble with Scratch (who isn't?) and I switched the dongle from the RasPi to the USB ports on the back of the Lapdock. Voltage across TP1/TP2 went up by 0.6V to 4.8V and Scratch seemed to be a bit more reliable although it still hangs unpredictably enough that my son want's nothing to do with it (sorry, I know, this is another thread.)

     

    On the subject of the German keyboard, have you tried something as simple as raspi-config? I seem to remember a whole host of keyboard alternatives in there and you can run it any time from the command line.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<