Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum WiPi and Pi Face
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 709 subscribers
  • Views 2187 views
  • Users 0 members are here
Related

WiPi and Pi Face

e14 Contributor
e14 Contributor over 13 years ago

HI,

 

Not sure if this is the right forum but could not see how to ask a quesion when I searched for WiPi.

 

I bought a RPi from Element14 and a PiFace too. The SD card came preloaded with Wheezy but nothing on the PiFace. So I downloaded the OS from Manchester Uni site http://pi.cs.man.ac.uk/download/rpi_raspbian_piface_4gb_sandisk.img

 

I installed into the RPi and it worked fine - got the emulator up and running etc. Problem is the Wifi enabl Config seems to have disappeared. element14 sent the WiPi with the kit I ordered and when I read the instructions (RTFM) it says it needs Debian6.0 "Squeeze" to work and to install this on the SD card from elinux or element14's site. To be honest I do not know what version of Squeeze (if any) is on the OS from the Manchester Uni site.

 

I thought about copying the PiFcae Folder from the OS SD card from Macnhester Uni to the SD Card that came from Element 14 but am not clera how to do that! I created a directory under the ROOT and copied all the PiFace folders and files into it but then when I looked on my Win7 machine at the SD card I cannot see any of this info at all. So I assume I can only see this wehn looking from within a Linux Terminal. The only Linux I have is on the Pi and so it is not possile to copy from one SD card to another unless I hook up a USB hard drive - but to be honest I am not that familar with Linux and have no idea how to format it for Linus etc. Please excuse my ignorance.

 

Can you let me know how an can get the WiPi working with the OS that I downloaded from manchester uni  site? Is it possible?

 

Thanks,

Mike

  • Sign in to reply
  • Cancel
  • GreenYamo
    GreenYamo over 13 years ago

    Hi Mike,

    I would get the latest version of Raspbian from the Foundation's site, get wireless working on that (using the wireless config tool on the desktop) and then use the manual install guide on the 'getting started with Piface PDF' (http://www.element14.com/community/docs/DOC-53057/l/piface-get-started-guide) to manually install the software you need.

     

    Steve

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to GreenYamo

    I recommend Steve's advice.  The U of Man's image isn't based on the most recent image of Raspbian.  The installation process is pretty simple.  Post if you have problems.  I've done on the current 2013-Feb-09 Raspbian image from raspberrypi.org.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to fustini

    @fustini: Thanks for letting us know! I have a question related to the image that you've shared with us its ok to write it to a 8 GB SD card? I imagine that it won't be no problems with that...

     

    Thanks,

    Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to e14 Contributor

    Hi - yeah, you can write it to a bigger card.  The raspi-config utlitiy will allow you to expand the existing partition to take up the whole card if you'd like.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to fustini

    A word of caution about cards...

    The class10 cards are designed for faster access, but only ONE file at a time.

     

    Many people had issues in the earlier days with the OS not happy and it seems that the class10 may have been the cause.

    I've used the cheap Class4 cards without a hitch.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • interested1
    interested1 over 13 years ago in reply to mcb1

    Mark,

      This is really interesting about the Class10 cards.  Is it fair to guess that the Class10 cards are faster one file at a time because they are used primarily for digital cameras?  Thanks for the insights and I look foreward to any responses to my surmise.

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to interested1

    David

    I'm not the expert, but that's what I summise.

    There was some very interesting discussions about what is inside most of the lower cost SD cards.

     

    If I recall the issues surfaced March 2012 when the Pi became available, and are probably in the Pi site forum/blogs.

     

    I have used Adata, Kingston, Sandisk usually Class4 and they all seem to work.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    You sort of need to be careful how you interpret some of this, 'Class 10' really only says the card can support 10MB/s sequential writes. Of more interest to the Pi is what underlying write modes (1 bit, 4 bit, SPI, SDR, DDR) the card uses and what voltage (1.8v, 3.3v) and clock speeds the card needs.

     

    The problem being that the Pi doesn't support all of the possible modes a card may support, for example the Pi can't do 1.8v, and especially in the early days there were bugs with incorrectly picking the clock speeds.  So card supports "mode A" Pi tries to use "mode B" and the mismatch caused problems, even for otherwise perfectly good cards.

     

    You then have cards labelled as Class 10 that really want UHS or 1.8v signalling in order to do that - and the Pi can't.. So depending on what else the card does or doesn't support a very slow failsafe mode might be chosen.

     

    The final clue is in the definition of Class 10 meaning 10MB/s sequential writes. It's not so much about a single file as it is about being able to write a file in a single sequential, contiguous block. This is perfect for cameras saving a big digital image, but may not match up with the random read/write patterns of a generic OS.

     

    Then just after you thought you'd worked everything out you have the usual problems of it being difficult to match up the manufacturers claims with the device inside the card. The manufacturer claims the best possible theoretical performance under some ideal condidions, or you have a counterfeit card that's not what it claims to be at all.

     

    Lots of potential pitfalls for the unwary.

     

    These days, with a recent OS image most cards will just work. There will always be exceptions.

     

    I've used class 4,6, 10 & UHS-1 cards with success, some of which wouldn't even allow the Pi to boot a year ago.  In general my best results are with Class 6 cards, but that's on a very small sample of available cards.

     

    If you can be bothered there's loads of discussions on this stuff over on the RPF forums from around April/May 2012, today most of the issues have been fixed so only go looking if you have archaeological interest image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • interested1
    interested1 over 13 years ago in reply to e14 Contributor

    Thanks for the great post, selsinork!  After I thought about it, and before I read your post, a single file transfer didn't quite add up... you shed quite a bit of insight on the issue for me!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to interested1

    Thanks selsinork

    That explanation better describes the situation.

    Sorry if I created confusion.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>