Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Development effort on Pi's USB problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 708 subscribers
  • Views 2152 views
  • Users 0 members are here
  • raspberry_pi
Related

Development effort on Pi's USB problems

morgaine
morgaine over 13 years ago

The long-standing problem of faulty USB handling on Pi may have some partial solutions up ahead, judging by progress being made in the "USB FIQ testing" thread on the RPF forum.   The thread is well worth reading start to end to gain a feeling for the magnitude of the problems being faced.  One of gsh's many interesting comments midway in the thread was:

 

gsh wrote:

 

Found a fix today for the dequeuing issue...  This should be interesting for anyone having trouble with the USB dropping out and ending up with errors from the smsc9512 ethernet

 

That would indeed be a very useful class of improvement, as it's long been a bugbear  that Pi's USB idiosyncracies impact on your networking as a consequence of Ethernet being implemented as a USB device rather than native in the SoC.

 

Even if a solution is only partial, I think this direction of development still provides a very useful ray of hope for the future.

  • Sign in to reply
  • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Morgaine Dinova wrote:

     

    Hopefully it died a death in well-deserved ignomy.  There is no price range in which badly sucking product is acceptable.

    While I don't disagree, there's something to be said for the level of pragmatism that realises that if you buy cheap crap you really do get what you pay for.

     

    But there's a difference between "sucking badly" and being manufactured with an eye to extreme low cost.  "Cheap crap" is different to just plain "cheap".  Many things that are extremely cheap are not crap at all, and low cost should never be used as an excuse for "sucking badly".

     

    Generalities aside, in our specific area of ARM technology, it is completely unacceptable to try to justify failure to operate correctly on the basis of "Well it's cheap, what do you expect?", particularly when the faulty feature in question is listed as adhering to a commercial standard such as USB.  A USB device that drops USB data isn't "a cheap USB device", it's a faulty USB device.  (Think about USB devices in general, not Pi specifically.)

     

    In analogue electronics it is very common and normal for cheaper devices to have poor specifications, but even the cheapest are required to work as specified.  In the mostly yes/no world of digital electronics, working in accordance with a specification is even easier to distinguish.  For both kinds, there is no price range at all in which faulty operation is acceptable.

     

     

    Addendum:  "You get what you pay for" doesn't extend to faulty operation.  Cheap stuff may be manufactured poorly or use low quality materials, but it will still work or it won't be of merchantable quality, at least in this corner of the world.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

     

    But there's a difference between "sucking badly" and being manufactured with an eye to extreme low cost.  "Cheap crap" is different to just plain "cheap".  Many things that are extremely cheap are not crap at all, and low cost should never be used as an excuse for "sucking badly".

    I'm not suggesting it's an excuse, just observing that in reality cheap often does equal crap.  However much we wish it wasn't the case, that doesn't change the reality.  The only way to change the reality is to hurt the profits of the companies who produce this stuff by not buying their products.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    The only way to change the reality is to hurt the profits of the companies who produce this stuff by not buying their products.

     

    Indeed, and when stuff doesn't work, I'm certain that happens. image

     

    And in these days of  Internet forums and blogs and social networking sites, the negative feedback resulting from a poor experience with a product is much greater than just the linear effect of voting with your money.

     

    Neither form of feedback has anything to do with cost though.  Costly and cheap items are both expected to work, or their manufacturers will suffer the wrath of the masses. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    selsinork wrote:

     

    The only way to change the reality is to hurt the profits of the companies who produce this stuff by not buying their products.

     

    Indeed, and when stuff doesn't work, I'm certain that happens. image

     

    And in these days of  Internet forums and blogs and social networking sites, the negative feedback resulting from a poor experience with a product is much greater than just the linear effect of voting with your money.

     

    Neither form of feedback has anything to do with cost though.  Costly and cheap items are both expected to work, or their manufacturers will suffer the wrath of the masses. image

    I'll toss another factor into the conversation.  Sometimes you have cheap items that don't comply with a standard, but most users won't notice so the seller can get away with it.  My favorite example is cheap HDMI cables that don't implement the individual ground wires, but instead use a foil shield for all grounds which is connected to the connector shells at both ends of the cable.  Such a cable will work fine for most HDMI uses, especially if it's a short cable.  This is because most HDMI products short together all the grounds and the shield, and since HDMI uses differential twisted pairs for the fast signals they really don't need individual grounds.

     

    However, some devices do need the individual grounds.  For example, the Motorola Atrix Lapdock uses one of the individual grounds lines to detect that an Atrix phone (or Rasperry Pi) is plugged in.  The cheap cable won't work, and have fun figuring out why not.

     

    The nasty part is that you usually can't find out whether the item is compliant or not without ordering one -- often from China.  And you don't know when you order the next one whether it will be compilant either, since the seller may have changed manufacturers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    Very good point, John!

     

    That reminded me of our extensive discussions about USB compliance in powered hubs that backfeed power to the upstream host.  Yes indeed, standards compliance is a very thorny issue, and it's clear that compliance checking is not given much importance in some parts of the world.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    It looks like Raspbian was updated on July 26.

    AFAIK there aren't any release notes, but presumably it must fix something.

    I see a July 20 post by jdb on the FIQ thread regarding USB audio DAC issues that says:

          

    These aren't going to be quick or simple fixes.

     

    So apparently there's still more known work to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<