Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 is unstable.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 711 subscribers
  • Views 3919 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi 2 is unstable.

e14 Contributor
e14 Contributor over 11 years ago

Today has received the Pi2 and was totally disappointed. Is very unstable. I do not even managed to set up the system. After a minute or two system is down. Then apparently fray fs continue after any issues downloading the same message "End Kernel panic - not syncing: VFS Unable to mount root fs on unknown-block(0,0)". That's all.image

  • Sign in to reply
  • Cancel
  • hawkeyethehacker
    hawkeyethehacker over 11 years ago in reply to e14 Contributor

    Noooooooooooo!

     

    Don't run those on top of those anti-static bags - while the inside is nice and protective the outside is a farmhouse for static charges.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to hawkeyethehacker

    while the inside is nice and protective the outside is a farmhouse for static charges

    Well I would disagree.

    The HDMI lead plugged into the monitor will be providing a ground.

     

    This is the pdf of the bags supplied with the RPi2.

    http://www.antistat-esd.pl/doc/torebki_ekran_otwarte.pdf

     

    Please note the inner and outler layers are conductive.

     

    For the reasons of conductivity and possibly thermal, its not the best idea to run them like sitting on the bags.

    For a few dollars you can buy cases ... which aren't listed as conductive or antistatic coated ....image

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor

    Glad you solved it.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hawkeyethehacker
    hawkeyethehacker over 11 years ago in reply to mcb1

    I stand corrected. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to hawkeyethehacker

    Your advice was appropriate for some bags.

    It just happens that these are a very good quality bag  .... better than I thought.

     

    Static builds up and unless it is discharged or dissapated it can cause issues where a pin is raised to a potential higher than the others.

    Discharging one's self by making contact with an earthed surface BEFORE touching the electronics is preferable.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 11 years ago in reply to hawkeyethehacker

    Hang on a moment though... surely if the outer layer is actually 'conductive' (as stated above) that surely implies that it will conduct electricity, and could therefore connect, and possibly 'short out' some of the exposed components on the underside of an otherwise protected board?

     

    Personally I would NOT advise placing a 'live' RasPi on on of these. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Montala

    surely if the outer layer is actually 'conductive'

    Did you actually read the pdf I referenced above.?

    10 ^8 to 10^11 ohms is 100M ohms to 100 G ohms

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 11 years ago in reply to mcb1

    Yes I did, thank you Mark, but just having a high resistance, doesn't necessarily make it non-conductive.

     

    It is obviously up to each individual to make up his own mind on what to use, but I will stick by my comments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to Montala

    Well. Just having a high resistance is exactly what makes things non-conductive.

     

    Everything conducts electricity to some point. Above some arbitrary threshold you call things "non contductive" because for all practical purposes no electrical current is conducted. In this case "10^8 ohms" is for all practical purposes "non conductive". Put a 5V over this and you'll get a "short" that carries about 2*10^-7 A. or about 0.02 micro amps. THAT will be difficult to measure, let alone influence the raspberry pi. (the influence of "at some time in the past few years you've touched the 'pi with your bare hands" is on the same order of magnitude. You don't worry about that, do you?).

     

    A friend of mine works with voltages of around 3MV. Megavolts. A current of 0.03A at 3MV represents 100kW and that is something that could be quite deadly if overlooked....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago

    I would be more concerned about the RasPi 2 building up heat on the bottom while it's sitting on top of that bag.  After it's been running a while, pick up the board and see how hot the bag is.  DRAM can get quite warm depending on what it's doing.

     

    I run my RasPi Model B (v1.0 PCB with 256MB DRAM) vertically mounted so I can get air flow on both sides.  That prevents it from overheating, especially the USB/LAN chip which otherwise gets very hot due to design problems that were fixed in the 2.0 PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>