Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29169 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi

    I am a newbie, and received recently a raspi3 + NOOB + a cirrus audio card.

     

    * * * * * * * * * * * * * * * * * * * * * * * * * * * * * * * *

    I fisrt want to report the successfull recognition of the Cirrus audio card using the info from http://www.horus.com/~hias/cirrus-driver.html, installing the pre-compiled version of the 4.4.6 kernel.

     

    Everything went smoothly; got in the end:

     

    pi@raspberrypi:~ $  aplay -l

    **** List of PLAYBACK Hardware Devices ****

    card 0: ALSA [bcm2835 ALSA], device 0: bcm2835 ALSA [bcm2835 ALSA]

      Subdevices: 8/8

      Subdevice #0: subdevice #0

      Subdevice #1: subdevice #1

      Subdevice #2: subdevice #2

      Subdevice #3: subdevice #3

      Subdevice #4: subdevice #4

      Subdevice #5: subdevice #5

      Subdevice #6: subdevice #6

      Subdevice #7: subdevice #7

    card 0: ALSA [bcm2835 ALSA], device 1: bcm2835 ALSA [bcm2835 IEC958/HDMI]

      Subdevices: 1/1

      Subdevice #0: subdevice #0

    card 1: sndrpiwsp [snd_rpi_wsp], device 0: WM5102 AiFi wm5102-aif1-0 []

      Subdevices: 1/1

      Subdevice #0: subdevice #0

     

    along with:

    pi@raspberrypi:~ $ i2cdetect -y 1

        0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

    00:          -- -- -- -- -- -- -- -- -- -- -- -- --

    10: -- -- -- -- -- -- -- -- -- -- 1a -- -- -- -- --

    20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

    30: -- -- -- -- -- -- -- -- -- -- -- UU -- -- -- --

    40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

    50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

    60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

    70: -- -- -- -- -- -- -- --

    pi@raspberrypi:~ $

     

     

    imageimageimage

     

    Now, I have some questions:

     

    QUESTIONS  * * * * * * * * * * * * * * * * * * * * * * * * * * * * * * * *

     

    >What is the bit-depth of the data on the [snd_rpi_wsp] ? / what possibility to adjust ?

     

    >What it the data rate on the [snd_rpi_wsp]  ? / what possibility to adjust ?

     

    >Is it possible to run concurently audio-in and audio-out / how ?

     

    > what would be your advice (looking for a possibly nearly ready made program or sub-module) for displaying on the raspi video monitor the live incoming audio data in a XY plot (X for the left audio channel, Y for the right audio channel) ?

     

    Thanks,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi,Hias

    Thanks for your hard work producing these kernel patches. I used your precompiled 4.4.6+ kernel (tested with original Wolfson card on RPi B and Cirrus card on RPi 3):

    just do the following as you said:

    • Do a standard raspbian installation
    • Do a "sudo apt-mark hold raspberrypi-bootloader"
    • Download the precompiled Cirrus kernel 4.4.6 and install them (unpack the kernel in the root directory and unpack the usescase script tarball  /home/pi/bin)
    • Edit /boot/config.txt and create the /etc/modprobe.d/cirrus.conf file as described

    All above is done and everything seems wonderful. The output of command aplay -l is okay. However, when I plugged in the speakers and tried to play a song using mplayer, I heard nothing. I want to know what's the problem. Thanks for your help!

    aplay -l http://paste.debian.net/693318/

    vcdbg log msg 2>&1 http://paste.debian.net/693320/

    dmesg http://paste.debian.net/693321/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    Your logs look fine.

     

    Have you run the appropriate usecase script (eg Playback_to_Lineout.sh) at least once?

     

    Also better disable the RPi on-board sound (remove dtparam=audio=on from config.txt), otherwise you might have that one registered as the default sound device and playback might be using that instead of the Cirrus card.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Thank you very much!

    I have tried all the methods you mentioned above, but it still doesn't work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello,

     

    I  bought Pi3 and cirrus audio card and currently I am trying to record audio files of the specific length, let's say 3sec. I followed instructions and installed kernel that you provided. Everything seems to be working. However, when I try to record sudo arecord -Dhw:sndrpiwsp -r 44100 -c 3 -d 2 -f S32_LE /tmp/del.wav command doesn't terminate and I am getting multiple files .. The first del-01.wav normally is bigger of few kB and the rest are 44bytes size. Do you have any idea what can be wrong?

     

    debian Pastezone

     

    The main task here is to record audio and at the same time process it. Do you know if this is possible to do, that arecord would save data and at the same time, maybe in different thread process it and get spectrum? Other way probably is to record let's say 1sec, process it and maybe at the same time record the other 1sec file for next process.

     

    Best regards,

    Algis

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    Hi Algis!

    However, when I try to record sudo arecord -Dhw:sndrpiwsp -r 44100 -c 3 -d 2 -f S32_LE /tmp/del.wav command doesn't terminate and I am getting multiple files ..

    This is a known bug "arecord -d" is broken in Debian/Raspbian Jessie

    https://bugs.debian.org/cgi-bin/bugreport.cgi?bug=821048

     

    You could try using arecord from Raspbian Wheezy or compile a newer version of arecord by yourself.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    志飞 姜 schrieb:

     

    Thank you very much!

    I have tried all the methods you mentioned above, but it still doesn't work.

    OK, lets do this step-by-step.

     

    First make sure you've disabled onboard sound and that "aplay -l" lists only the Cirrus card:

    pi@rpi3:~ $ aplay -l
    **** List of PLAYBACK Hardware Devices ****
    card 0: sndrpiwsp [snd_rpi_wsp], device 0: WM5102 AiFi wm5102-aif1-0 []
      Subdevices: 1/1
      Subdevice #0: subdevice #0
    pi@rpi3:~ $

     

    Then enter these 3 commands to configure output to Lineout and Headset out.

    Reset_paths.sh -q
    Playback_to_Lineout.sh -q
    Playback_to_Headset.sh -q

     

    Make sure that you don't get any error messages printed on the console, entering these commands should just return to the command prompt. It has to look like this:

    pi@rpi3:~ $ Reset_paths.sh -q
    pi@rpi3:~ $ Playback_to_Lineout.sh -q
    pi@rpi3:~ $ Playback_to_Headset.sh -q
    pi@rpi3:~ $

     

    Now run "speaker-test -c 2 -t sine", this produce a 440Hz sine tone alternating on the left and right channel. The output should look like this:

    pi@rpi3:~ $ speaker-test -c 2 -t sine
    
    speaker-test 1.0.28
    
    Playback device is default
    Stream parameters are 48000Hz, S16_LE, 2 channels
    Sine wave rate is 440.0000Hz
    Rate set to 48000Hz (requested 48000Hz)
    Buffer size range from 16 to 131072
    Period size range from 8 to 16383
    Using max buffer size 131072
    Periods = 4
    was set period_size = 8192
    was set buffer_size = 131072
     0 - Front Left
     1 - Front Right
    Time per period = 3.141148
     0 - Front Left
     1 - Front Right

     

    If you still can't hear anything make sure everything's plugged in correctly. Also try connecting a headphone to the headphone out connector and check if you get sound there.

     

    If you get any error messages on the console or the output looks different please post it here.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Hello,

     

    thank you for the information.

    I am quite new in the RPI field. Can you write more about how to use Raspbian Wheezy arecord opn Jessie and how to compile arecord? I can see that the current version of arecord is 1.0.25.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    thank you for the information.

    I am quite new in the RPI field. Can you write more about how to use Raspbian Wheezy arecord opn Jessie and how to compile arecord? I can see that the current version of arecord is 1.0.25.

    Using the wheezy version is the easier solution. Just download the wheezy alsa-utils package, extract it and then copy the extracted arecord for example to ~/bin/arecord-wheezy:

    pi@rpi3:~ $ cd /tmp
    pi@rpi3:/tmp $ wget http://mirrordirector.raspbian.org/raspbian/pool/main/a/alsa-utils/alsa-utils_1.0.25-4_armhf.deb
    pi@rpi3:/tmp $ mkdir unpack
    pi@rpi3:/tmp $ dpkg -x alsa-utils_1.0.25-4_armhf.deb unpack
    pi@rpi3:/tmp $ cp unpack/usr/bin/arecord ~/bin/arecord-wheezy

     

    Compiling from source is a little bit trickier. First you have to uncomment the deb-src lines in /etc/apt/sources.list and /etc/apt/sources.list.d/raspi.list. Then run the following 2 commands to download all packages required for building alsa-utils:

    pi@rpi3:~ $ sudo apt-get update
    pi@rpi3:~ $ sudo apt-get build-dep alsa-utils

    That'll download the build dependencies of alsa-utils 1.0.28 in jessie, but ATM that's fine for compiling the latest version (1.1.1).

     

    Then do the usual download - extract - configure - make steps to compile the source code:

    pi@rpi3:~ $ mkdir install
    pi@rpi3:~ $ cd install
    pi@rpi3:~/install $ wget ftp://ftp.alsa-project.org/pub/utils/alsa-utils-1.1.1.tar.bz2
    pi@rpi3:~/install $ tar jxf alsa-utils-1.1.1.tar.bz2
    pi@rpi3:~/install $ cd alsa-utils-1.1.1
    pi@rpi3:~/install/alsa-utils-1.1.1 $ ./configure
    pi@rpi3:~/install/alsa-utils-1.1.1 $ make

     

    A minute or 2 later the build is finished, but you might notice that there's no arecord. Nothing to worry about, aplay is a "combined" executable and contains both aplay and arecord - depending on the filename you'll either get aplay or arecord functionality (on standard installation arecord is a symlink to aplay).

     

    To make things easier, just copy the freshly compiled aplay for example to ~/bin/arecord-1.1.1

    pi@rpi3:~/install/alsa-utils-1.1.1 $ cp aplay/aplay ~/bin/arecord-1.1.1

     

    By naming the older/newer versions differently you can easily choose between the official Raspbian version (use "arecord") or your user-installed versions ("arecord-wheezy" / "arecord-1.1.1"). Of course you could name the older/newer versions "arecord" and install them in ~/bin or /usr/local/bin but that might bite you some time later when there are updates in Raspbian and entering "arecord" will use your manually installed version. OTOH entering "which arecord" will show which version is used, so you can still go that route if you prefer that.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi Mathias, and thank you for the work you put into this (i used your guide to setup my soundcard some months ago)
    Now i have a problem with my sound, and i think i have traced it back to the soundcard.. so i'm writing here, since you are the person that comes in mind who would have the knowledge image

     

     

    The problem is this: I am trying to write interleaved samples to the sound buffer using snd_pcm_writei() (link = ALSA project - the C library reference: PCM Interface), but i realized that only one of the earplugs i use is playing sound, the sound frequency is lower and i have noise as well.
    My educated guess is that the samples are not being written interleaved from the soundcard, but rather all samples to one channel, which would also account for the frequency distortion and noise.
    So my question is if there is a way to set up an output to accept interleaved samples?( btw. i use your shells "reset paths.sh" "playback_to_headset.sh" etc in the beginning of my program)

     

    Thanks for your time!
    soren

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>