Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PSOC 5LP Hat for a Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 83 replies
  • Answers 22 answers
  • Subscribers 713 subscribers
  • Views 13400 views
  • Users 0 members are here
  • raspberry_pi
Related

PSOC 5LP Hat for a Raspberry Pi

clem57
clem57 over 10 years ago

     I was checking Kickstarter today and found this: https://www.kickstarter.com/projects/land-boards/pisoc?ref=home_recs.

The project incorporates PSOC 5LP from Cypress on a custom hat. What do you think?

 

image

  • Sign in to reply
  • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hi Clem,

     

    should I be really sincere? It's in perfect Kickstarter style. As probably you already know (I wrote articles here and there on E14 about this) I am a PSoC lover and I have adopted them for their versatility in projects associated to the Raspberry, the TI launchpad MSP432 and also standalone. As they are small and powerful well adapt to high level SBC.

    Without creating a campaign, just creating a thing image

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago

    Hi Clem!

     

    Kind of odd why they would wire the entire 40-pin connector (all 29 I/0 according to the text on that page) to the PSoC chip.. maybe I'm missing something, but I can't see what.. it doesn't make sense to me : (

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to shabaz

    That is a wonderful question, shabaz. I did he mentioned 3 were needed to flash the HEX file onto the PSOC 5LP which makes sense. The other 26, who knows?

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to clem57

    It is like making chicken but then only serving the gravy. Or buy an outfit but go out without the pants. Why would they do it?

    Also, ouch, just saw the price. $55 (plus $5 shipping in the US, total of $60) is a rip-off.

    There is this board CY8CKIT-059 PSoCRegistered 5LP Prototyping Kit With Onboard Programmer and Debugger | Cypress

    which is just $10, and has a better part by the looks of it (twice the memory and higher speed).

    It would just take a few jumper cables to plug onto the Pi.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to clem57

    Excuse my ignorance, but what happens if you want to implement One Wire on the Pi, or perhas the serial TTy connection.

     

    Can the PSOC ignore those pins and not have any influence??

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    IMHO this is a gigantic bullshit.

     

    1. PSoC5 by Cypress (now cost only $7) has two USB ina just for programming. What differs FSLN the PSoC4 is just that it includes the psiuc programmer (the part that can bw broken from the chip) whike the model 4 only can be programmed with the bootloader or buying separately the programmer.

     

    2. The psoc can be connected easily through extra pins  via seria or usb or another couple of ways.

     

    3. Any make is abkw to connect the two devices via usb and access from the raspberry pi the other device.

     

    Sound very strange to me if they have ported the psoc creator on the PI (I think it impossoble)

     

    So where is the innovatiom? And the sense of this project???

     

    And many other objections can be added...

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to mcb1

    PSOC can reassign pins for any function you want. So I would guess all is possible.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    For $10 you can get CY8CKIT-059 PSoCRegistered 5LP Prototyping Kit With Onboard Programmer and Debugger | Cypress . Solder some pins and breadboard together! image

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to clem57

    I'm embarrassed to admit I have a number of PSOC boards and no time to start coming to grips with the software.

    I'm sure once I start using them I'll wish I had earlier, but in the meantime ....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to mcb1

    When PSOC4 was coming to the market I got myself one. I was interested in the analog configurabiltiy.

     

    Turns out I got a 4000 model and the analog stuff requires a 4100 or 4200. The "complete analog configurability" has to be taken with a grain of salt too... For example, you can choose which pin the ADC operates on... Ehhh... Isn't that called an "ADMUX"? The smallest AVR or PIC has that!

     

    Oh and then they say: "Supports bootloading over serial"... Turns out that what they mean is that you could write a bootloader and use the expensive debugger to put the bootloader you wrote into the chip and that from then on the chip can self program using any protocol you might want.... Ehhh. Doesn't every microcontroller have that ability? "Supports serial bootloading" to me means that I don't need an expensive debugger.


    Anyway, I have a Cypress-branded paperweight. It's not good at being a paperweight either. It's too small.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>