Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum There is a broken chip on my Rpi3 motherboard labeled: 4R7. I just bought it and it broke while trying to install it inside the case. Will the board still work with that chip broken? Can I cover it with epoxy?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 12 answers
  • Subscribers 708 subscribers
  • Views 13520 views
  • Users 0 members are here
  • broken chip
Related

There is a broken chip on my Rpi3 motherboard labeled: 4R7. I just bought it and it broke while trying to install it inside the case. Will the board still work with that chip broken? Can I cover it with epoxy?

unsagicois
unsagicois over 9 years ago

There is a broken chip on my Rpi3 labeled: "4R7". I just bought it and it broke while while trying to install inside the case.

Will that chip: "4R7 being cracked will prevent the Rpi3 from working properly? Can I simply coat the chip with epoxy?

This is my first experience with Raspberry. I never heard of it before until I saw an advertisement for Cayenne in Facebook last month.

image

  • Sign in to reply
  • Cancel
  • michaelwylie
    0 michaelwylie over 9 years ago in reply to unsagicois

    Looks fine to me, just the package is broken. If the package is ferrite, the inductance will be slightly different. I don't think it's a big deal.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to michaelwylie

    I would agree with michaelwylie, based on the observed damage, as long as the windings are intact, the change in inductance could be compensated for by the power controller, it may run a little warmer but I would have fairly good confidence it will still work ok (If this is the only damage

     

    This should be fairly straight forward to replace if you are confident with surface mount soldering and if you can get the right part. Care would be needed to not damage surrounding parts or to get the board too hot. A hot air soldering gun would help here too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to unsagicois

    Very Compact wrote:

    No real worries if it's just a little bit of a corner.

    (You can also feel free to glue on the broken bits if you wish.)

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to michaelwylie

    If the ferrite is cracked it makes sense to make the airgap as small as possible and keep it in place. Epoxy is fine for that.

     

    If the ferrite is broken that the body of the inductor is loose and it is just hanging on by the wires, then it makes sense to lock it in place. Epoxy is fine for that.

     

    But in the pictures it looks as if part of the ferrite broke off. In that case there is not much else you can do. Just power it up and see if it works. As michael says, the inductance may be a bit different, but they don't normally make anything between 2.2uH and 4.7uH, so even if they calculated the ideal value to be 3.7uH they will be using this one, and you dropped the inductance by a few percent. Nothing to worry about.

     

    Your measurement of 10 ohms is a bit high. Many multimeters cannot accurately measure low resistances. So there usually is an offset on the order of a few tenths of an ohm near zero. You can calibrate your offset by measuring the resistance from the SAME PAD of the inductor. Both leads on the same side. When you end up measuring the actual resistance you subtract what you got when you had the leads on the same side. I have one multimeter that has a 0.3 Ohm offset, but another has something like 5 ohms.

     

    Now... Even that 10 ohms reading can be considered "almost zero". 10 ohms is a tad much, but if we factor in about 5 ohms of offset on your multimeter, it doesn't sound too bad. Of course, for efficiency's sake, you would rather have 0.1 Ohms or less, but if that is unobtainable in the formfactor and/or pricepoint, then you'll have to settle for something less than ideal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • unsagicois
    0 unsagicois over 9 years ago in reply to COMPACT

    Thanks very much to all of you. I hope I will get to next delicate step of formatting my questionably authentic Sandisk SD card and installing the Noobs. image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<