Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Memory mapped I/O?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 3514 views
  • Users 0 members are here
  • raspberry_pi
Related

Memory mapped I/O?

michael.vos
michael.vos over 9 years ago

Does the compiler have memory mapped I/O - at least  byte wide?

  • Sign in to reply
  • Cancel
  • rew
    0 rew over 9 years ago

    The compiler has nothing to do with "memory mapped IO".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michael.vos
    0 michael.vos over 9 years ago in reply to rew

    Then maybe I should asked: is memory mapped I/O available? And by memory mapped I mean can you read and write at least byte wise (at least 8 bits in one go as opposed to building up a word from individual GPIO bits) via the GPIO. I would want to setup an 8 bit bus structure to access external peripherals.

     

    Kind regards

    Michael Vos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago

    I'm not a Pi expert but I'll try to help.

     

    The Pi hardware (in common with all similar processors) does not support memory mapped IO in the way that, for example, an ARM Cortex M part does.  This is because it is designed to work with DDRAM which is hard enough to get to work in the very special case of a processor or FPGA to memory interface - as far as I know no one uses the DDRAM interface for IO. The usual solution is to provide some additional IO ports which will require some kind of drivers to operate them - they are rarely mapped into normal memory space.

    The PI has very limited IO (Beagles are much better) but it is supported by lots of low cost IO expanded boards from many sources but they are all slow.

    To be fair the PI is not alone in having this problem - the best way to get data in and out of most computers at high speed is often to use Ethernet or PCI but both require serious hardware.

     

    It's this (hardware) limitation which allows small Cortex M class  micros to beat the ****** out of GHz application processors like that on the PI when it comes to low latency fast IO. And even with Gbit Ethernet, although you can get 100Mbytes/s in and out of the processor the round trip latency will be measured in us  - perhaps 100x slower than an STM32F4xx can bit bang IO !!!

     

    Roger is correct in implying that it isn't a compiler issue - you'll have the same problem with Python, C or anything else.

     

    What are you trying to do - there are (almost) always ways round these problems.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michael.vos
    0 michael.vos over 9 years ago in reply to michaelkellett

    Thanks for your reply. I have been using a Crystalfonz SOM (CFA10036) which uses an ARM9 iMX287 but the software drivers for I/O are single bit at a time - rather slow for accessing an 8 bit bus. I also use the Silicon Labs ARM3 micros and the I/O is much better on these. In my naivety I assumed the BIGGER micros would be at least the same or better.

     

    Thank you both for your help.

     

    Kind regards

    Michael Vos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 9 years ago

    Hi Michael,

     

    As I recall, there was a way to group I/O pins so that you could treat them as a single port.

     

    That said, I have no idea on how to do this as my Pi experience is limited.

     

    Check with the Pi org, I will bet that someone has done what you want to do.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 9 years ago in reply to michaelkellett

    You're not a processor architecture expert either. The 8086 processor and some of its more modern variants had special instructions for I/O operations

    that separated them from memory space accesses using dedicated hardware I/O read/write signals (I assume that they still do, but for example the PCI bus

    is memory mapped !). ARM processors (and most other RISC processors) do not have these instructions and instead dedicate some of their memory

    space for I/O, this is what is known as memory-mapped I/O and accessing this "I/O space" uses the same instructions as normal memory reads and

    writes. When this I/O space is accessed it does not in any way affect DRAM because the memory address decoding of this I/O space prevents RAM

    access hardware signal pins from being activated.

     

    ARM SoCs use some of it's memory space for I/O registers built into the SoC to perform the various types of I/O supported by the chip. While in general

    these registers do use consecutive bits in each 32 bit word, unfortunately when they are connected to dedicated I/O pins on the SoC they do not always

    follow that bit order. Most of the time it is because some of the GPIO pins have multiple functions and when the "alternate" function (such as I2C, SPI, A/D, etc)

    is used it splits up the other I/O bits so that they are no longer 8 or 16 consecutive bits. Sometimes because of pin limitations they just don't run all of the bits

    to external pins. And just to make things worse, sometimes when laying out the PCB, it is just easier to route the SoC I/O pins to the PCB I/O when they are

    split up. This has always been a pet peeve to me for the reason that Michael Vos has stated, sometimes it would just be a whole lot better/easier to be able

    to do true byte-wide (or bigger !) accesses but it is physically impossible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to michaelkellett

    The pi has memory mapped IO just like any cortex-M does. Just like a cortex-M the processor on the pi has several peripherals. On the 'pi, because it runs Linux, there are usually drivers for these peripherals. These are mapped into normal memory space. Now, on Linux user-space processes get a virtual memory space that does not allow them access to the hardware (memory mapped IO). But a simple open(/dev/mem) + mmap system call will map the memory mapped peripherals into your process space.

    Especially on the pi, PCI or Ethernet is NOT the way to get data in or out the computer. The first because the pi  processor doesn't have PCI, and the second because the pi procesor doesn't have Ethernet, and ethernet was included by using and USB-ethernet chip on the board.

    If you program the pi at the right level, it can beat the *** out of a slower (e.g. 48MHz) embedded arm processor. First because it runs at 700MHz+, second because it has caches, and third because it has a GPU co-processor that can do enormous amounts of floating point operations....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to gdstew

    Gary, one little addition: the PCI bus allows IO accesses that the '8086 family of processors support. Most expansion cards no longer use such old fashioned stuff, but the PCI bus supports it. A reason could be that the address space on IO accesses is only 64k.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to michael.vos

    I don't know too much about that  Crystalfonz module, but it is most likely just like  the pi.

     

    The CPU has a bunch of GPIO pins. They are possibly grouped by eights, sixteens or thirty-two. For each group, you can "set all outputs with one write".

    GPIO->DATA_REGISER = values;

    I just checked the datasheet for you, and the broadcom processor surprises me in that it cannot do this.

    It has a register to SET and another register to RESET bits in the output register.  That on the one hand might slow you down a factor of two, but it also speeds you up more than a factor of two! Now to write your eight-bit bus to the value you want, you simply RESET all 8 bits of your 8 bit bus: GPIO->GPCLR0 = 0x003FC0000; and then write the 8 bits you want to the SET register: GPIO->GPSET0 = data << 22; (assuming your 8bit bus is on GPIO 22 through 29).

     

    The biggest problem is that on the first pi, routing of the PCB influenced which GPIOs came where on the GPIO connector. Thus it might prove difficult to find 8 free GPIOs that are contiguous. So you might need to assemble a few parts of the 8 bits of data into the 32-bit write to the GPSETx register.

     

    So on the GPIO connector we have access to: 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17, 18, 20, 21, 22, 23, 24, 25, 26, 27. So, you are in luck! There ARE 8-bit contiguous stretches of GPIO pins available that allow easy single-instruction access to that databus.

     

    One thing you might run into is that some of these have a "special function". So if you need the UART as well, that's on pin 14-15, so that creates a hole there. 2-3 is I2C, 7-11 is SPI. But 20-27 remains together as a byte. It's scattered around physically on the connector, but in software you can do it in one go.

     

    That said... the reason you're seeing things go slow is unlikely related to accessing separate bits in memory mapped IO. Suppose I chose to connect my 8-bit bus on GPIO4, 14, 15, 17, 18, 27, 22,23 because those are nicely together on the connector. then I'd write

    GPIO->GPSET0 = (data&0x01)<<(4-0) |

                               (data&0x02)<<(14-1) |

                               (data&0x04)<<(15-2) |

                               (data&0x08)<<(17-3) |

                               (data&0x10)<<(18-4) |

                               (data&0x20)<<(27-5) |

                               (data&0x40)<<(22-6) |

                               (data&0x80)<<(23-7);

    Because we have three "stretches" of contiguous bits, we can simplify this:

     

    GPIO->GPSET0 = (data&0x01)<<(4-0) |

                               (data&0x06)<<(14-1) |

                               (data&0x18)<<(17-3) |

                               (data&0x20)<<(27-5) |

                               (data&0xc0)<<(22-6);

    Now if you know this in advance, you can optimize this even further by choosing longer stretches of contiguous bits.  I have written and compiled this, and it turns into twelve instructions. So at 1.2MHz that would evaluate in 10ns! (assuming you're doing this often enough to load the code into cache).

     

    If you are complaining about bitwise access and slowness, then I suspect that you might be accessing the Linux GPIO driver through /sys or someting. THAT is going to be horribly slow no matter what.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to gdstew

    Gary, when someone start a reply with an "I'm not an X expert but I'll try to help" any rational person interprets this as a genuine attempt to set the context for their answer.

     

    To respond with an " You're not a Y expert either ..." is quite simply rude and unhelpful. No, I'm not a processor architecture expert and I never claimed to be.

     

    My reply was, perhaps, a bit of an over simplification and I had assumed that the OP wished to connect an external non-memory device to the PI and have it appear in the PI memory space - something which is easily done with ARM Cortex M (and similar) parts with external memory buses but not feasible on most application processors.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>