Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Wolfson modified Noobs raspbian zipped img  Cannot unzip new download
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 108 replies
  • Subscribers 714 subscribers
  • Views 20153 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Wolfson modified Noobs raspbian zipped img  Cannot unzip new download

superpat
superpat over 12 years ago

Hi,

 

I deleted my original zip download  and the img of the above file.   I have downloaded it again, but all the unzip programs I try will not unzip it, ( say no unzip sig).

 

I have painfully downloaded it again and still no joy with unzipping.

 

Have you changed the file recently?

 

Please, please  publish the md5 sum for this file!  (so I can eliminate download errors)

 

many thanks

 

regards

 

Patrick

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi all,

     

    I had the same problems from Debian with unzip and 7zr, but finally I got it installing the "p7zip-full" package and uncompressing with 7z:

    * apt-get install p7zip-full

    * 7z e wolfson_3.10_master.zip

     

    7-Zip 9.20  Copyright (c) 1999-2010 Igor Pavlov  2010-11-18

    p7zip Version 9.20 (locale=es_ES.UTF-8,Utf16=on,HugeFiles=on,2 CPUs)

     

    Processing archive: wolfson_3.10_master.zip

     

    Extracting  wolfson_3.10_master.img

     

    Everything is Ok

     

    Size:       7892631552

    Compressed: 4713117059

     

    Good luck!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    RuneAudio - Embedded Hi-Fi music player , a project similar to Volumio, with your kernel works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi,

     

    Squeezeplug works pretty well with the Wolfson card, but if you want to use the Volumio web-interface as your client, that works too. A guy over in the Volumio forums, Ebsy, has produced a tutorial on how to install Volumio on the PiBang distro. I wondered if it would work on Raspian, so I tried it, and it does! This is using Ragnar's version of the Wolfson image. The tutorial is at http://typingoutloud.org/raspberry-pi-installing-volumio-pibang/. I'm now happily using the Volumio web-interface with the Wolfson card. It may not have all the background tweaks of the full Volumio distribution, but it seems to work pretty well to me.

     

    Colin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for your efforts on this.  Like one of the other posters here my dmesg is just full of stack traces and the card is unrecognizable.

     

    I'm so utterly disappointed in this product.  It boggles my mind that I would have to use a custom pre-built OS to use an add-on hardware device.  I have spent too much time installing and configuring other aspects of my raspian OS (I use it as a print server, backup storage device, etc) to just blow it away and use a new OS image.

     

    So all I can do is sit and hope one day they can get their act together and get the drivers & libs in the official channels and we don't have to mess around with this kind of b.s.  Looks like someone pushed a product to market before it was ready.

     

    Blech.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    @Wayne Westlake what you need is this post - no need for a reinstall, just a kernel swap.  Why this isn't what they did officially I don't know!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    @Joe E.

    So from a "normal" noobs install It´s enough with just changing the kernel according to Ragnars post?

     

    I´m with Wayne here. It´s not working at all. The Wolfson NOOBS install can't be done because of discspace on the SD card ( 8 Gb)....

    For som reason Ragnars raspian.wheezy stop booting after half a minute.

    and so on.....

     

    Why didn´t they do it right from the beginning, now Ragnar and alike have to fix what they didn´t do.

     

    Disappointed, but thanks to all that is trying to help.


    Btw, forgot to say that the download of the image isn't working either.

     

    Rgds

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Ragnar's image worked right away for me, and the card is working fine too. Maybe a problem with your SD card?

     

    I think the intention is that the Wolfson drivers will be included into the standard Raspian distribution in due course. We are the early adopters, so we have to work with what is, I think, an interim solution. As I say, it does what I need it to (play music via the SPDIF ouput), and works better than my previous USB Dac set-up, so I'm not complaining.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Unfortunately like at least one other poster this doesn't work for me.  I think it's because I'm already on the latest kernel (3.10.36) and this is a backdated one.  I get all sorts of stack traces when viewing logs with dmesg as did another poster.  That's also the caveat with this method, you're stuck on his 3.10.25 kernel forever.

     

    Thanks for the suggestion though.

     

    Wayne

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I did a standard Raspbian install (not through NOOBS) then updated everything (not much) and changed the kernel and have had no problems, though I didn't look through any logs (it worked, why question it?)

     

    I've slightly downgraded kernels on other systems before without issues but you might be using something which is built against the newer one which objects to the downgrade.  Lets hope they get it integrated into the default kernel soon, then it will be a simple upgrade for everyone.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    It might be a problem with the Sd card, but everything else is working. Like the normal NOOBS.

     

    Early adopters and early days yes, but now it´s up to us (read you image) to fix it I think.

     

    Hoping and waiting for an official fix.

     

    Rgds

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>