Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi B+ wiith USB 3g/4g dongle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 676 subscribers
  • Views 1648 views
  • Users 0 members are here
  • 4g
  • raspberry_pi
  • raspberrypi
  • 3g
Related

Raspberry Pi B+ wiith USB 3g/4g dongle

Former Member
Former Member over 10 years ago

Hi,

 

I am trying to set up my rpi with its own internet usig a 4g USB Dongle: (ZTE Australia > Products > MF823).   I have read many articles about it but haven't found anything current so not sure if they apply to the B+.

 

Setting up the 4g dongle was very simple, I installed usb-modeswitch, switched form USB to ethernet, added some basic config to the interfaces file, rebooted and it worked....It was a nice surprise.

 

Here are the questions I have,:

 

1) Will the B+ have power issues with the 4g Dongle, specs say it draws 700mA, im using 2.1A power supply? (do I still need a powered hub)

2) I read in many places that ppp and wvdial although I believe my dingle has a built in dialer.  How do I confirm this?

3) If I send the device to a location that has 3g only, will everything still work the same ?

 

Thanks in advance.

  • Sign in to reply
  • Cancel
  • rew
    0 rew over 10 years ago

    1) There is a 1.2A "fuse" on the 'pi. This may lead to problems: if say you perform a remote update and you require a constant download of data for several minutes/hours, the fuse might overheat and you'll "lose" your pi. (it won't recover unless you unplug it by hand). Theory says you're too close to the limits for comfort. In practise the 'pi will usually not consume its full power, but for the dongle, the conditions where it might do so might be out of your control. If you're on 4G now, the power requirements might be lower than when you're on the edge of a 3G cell, and the module has to use "full transmit power" to make itself heard by the cell-tower.

     

    I have a powered-hub that powers up the 'pi when I connect it to the 'pi as a HUB. (i.e. nothing in the power connector of the 'pi). Such a construction would be ideal. Aim for at least 1.5A of REAL deliverable power. (A chinese 2A power adapter might run short of have short lifetime if loaded like this).

     

     

    2) Yeah, If it works like this, don't touch it. wvdialer would normally need a virtual com port to talk to so if you now just use the dongle as an ethernet adapter, then wvdial has no business talking to that thing. (it cant).

     

    3) I think so.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to rew

    Thanks Roger,

     

    From what you are saying a powered USB hub should put me in the clear with this solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to Former Member

    The raspberry has a fuse at the power-connector. Your total consumption is too much for that fuse. Even though your tests seem to indicate that right now it works, you cannot depend on it. It might fail at any inconvenient moment.

     

    A powered hub with a sufficient powersupply will work. (If backfeeding as described above works: fine, otherwise you need to run a micro-usb-cord-for-power to the power port of the 'pi)

     

    I saw a nice 7-port powered hub at a friend's place one day. As required: a 3.5A powersupply. So I got one too. THEN he tells me that he replaced the powersupply with a better one: it comes from the shop with a lowsy powersupply. So: Be careful: Get a proper powersupply even if on first look you think it should be enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to rew

    Do you have any links to the type of USB Hub / Power Supply you would recommend?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to Former Member

    Well, I like the 7-port one that my friend bought. However it comes with an insufficient power supply. My friend tells me he "grabbed a leftover powersupply from work", and I connected it to a big 650W PC powersuply here on my desk. I have a few 12V devices (occasionally up to 10A), and a few 5V things (two raspberries, charging my phone), so having "plenty" power makes sense here.

     

    But all that said, I haven't had the need for a "5V, 1.5A sustained" powersupply, so I haven't investigated.

     

    This one is "not too shabby" 2A EU US USB AC Wall Charger Power Adaptor For iPhone Smartphone Device - US$2.99

    claims 2A tested to work fine at 1.5A. MTTF unknown.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago

    Hi Mitbo,

     

    Post was from a while ago but I have the same usb modem but cannot get it to work. Can you remember how you set it up and the settings?