Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pico with HC-05 - how do you get it to work?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 702 subscribers
  • Views 4594 views
  • Users 0 members are here
Related

Pico with HC-05 - how do you get it to work?

gregaryb
gregaryb over 3 years ago

image

I am using GP17 and GP16 as Rx and Tx connected directly to the HC-05 Tx and Rx pins (cross connected)
I am powering the HC-05 with 5V from the Pico Vbus pin.

I have a voltage trimpot divider on the HC-05 pin Tx pin to make sure the voltage stays under 3.3V.
I am connecting to the HC-05 with Android SerialBluetooth app and sending "XXXXX" with carriage return and new line.

Code on my Pico running in Thony on Windows 10

But it just isn't working. There is not data received in Thonny.

With Arduino all this (with equivalent C) just works.

So what am I missing with Pico and micropython?

from MotorControllerLibrary import *
from machine import UART, Pin
import time

# enable     GP2
# in1         GP3
# in2        GP4
# enable    GP6
# in3        GP7
# in4        GP8
serial = UART(0, baudrate = 9600, tx = Pin(16), rx = Pin(17))

while True:
    if (serial.any == True):
        strCommand = serial.readline()
        print(strCommand)

  • Sign in to reply
  • Cancel
  • gregaryb
    0 gregaryb over 3 years ago in reply to dougw

    Absolutely positive. I set the baud rate myself via AT commands.
    serial = UART(0, baudrate = 9600, tx = Pin(16), rx = Pin(17), timeout = 10000)
    It needed a timeout. Otherwise readline() returns imediately before you can send any data.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to gregaryb

    The serial capability of MicroPython on Pico isn't great unfortunately. It's actually missing useful stuff like ability to flush the input too, I.e. clear any input buffer. Still, it's sometimes possible to work around that sometimes, so the existing functionality is still quite useful, but it could be better. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gregaryb
    0 gregaryb over 3 years ago in reply to shabaz

    This simple library solves the problem.
    It blocks until you send a token over bluetooth, delineated by \n
    It also expands on the rather unhelpful Python error message 'bad tx pin'

    from machine import UART, Pin

    class CSerial:
        
        uart = 0
        nUARTPort = -1
        
        def __init__(self, nBaudRate, nRxPin, nTxPin):
            if ((nRxPin == 5) and (nTxPin == 4)) or ((nRxPin == 9) and (nTxPin == 8)):
                self.nUARTPort = 1
            elif ((nRxPin == 13) and (nTxPin == 12)) or ((nRxPin == 17) and (nTxPin == 16)):
                self.nUARTPort = 0
            
            if (self.nUARTPort == -1):
                print("Tx = " + str(nTxPin) + " and Rx = " + str(nRxPin) + " are not a valid UART port!")
                print("UART 0")
                print("  Tx = 12, Rx = 13 or Tx = 16, Rx = 17")
                print("UART 1")
                print("  Tx = 4, Rx = 5 or Tx = 8, Rx = 9")
                self.uart = UART(0, baudrate = nBaudRate, tx = Pin(nTxPin), rx = Pin(nRxPin), timeout = 60000)
            else:
                self.uart = UART(self.nUARTPort, baudrate = nBaudRate, tx = Pin(nTxPin), rx = Pin(nRxPin), timeout = 60000)
                print("UART port " + str(self.nUARTPort) + ", Tx = " + str(nTxPin) + " and Rx = " + str(nRxPin))
                
        def WaitForToken(self):
            strToken = ""
            print("Waiting for token via UART port " + str(self.nUARTPort) + "...")
            while (True):
                strToken = self.uart.readline().decode("utf-8")
                if (strToken != ""):
                    break
            print("Token recieved: '" + strToken + "'")
            
            return strToken
                

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<