You don't have permission to edit metadata of this video.
Stable diffusion, A.I. LLM, video rendering, or gaming? Maybe VR? Would a more powerful GPU on the Pi benefit you?
Stable diffusion, A.I. LLM, video rendering, or gaming? Maybe VR? Would a more powerful GPU on the Pi benefit you?
I've sent you a message.
I've seen working with them are mostly focusing on the software, rather than the electronics side. Everything to them is code ... and this isn't the "forum" they would naturally gravitate towards.
I feel like that needs to be improved on this Community but I may be in the minority thinking that.
you can install TensorFlow and Pytorch and run pretty much anything that don't requires newer versions.
I've been meaning to get my head around these myself, do you know of any beginner resources?
Hardware decode for h.264 and VP9
And encode, that's a good point, depending on the graphics card you could even have hardware encode/decode for AV1.
Yay! Hardware decode for h.264 and VP9
As soon as I'm done with it, I can post it here.It's nothing fancy really - just read my license plate and open my garage door - this will be used - at least for a proof of concept - on my work place .
First I'm just learning how to use the NVIDIA specific functions for deep learning and ML.
NVIDIA has quite a number of tutorials for one to learn. They even offer free certification after you submit a project and be graded by them.
That's cool, I'd be interested in reading more about how people put it to use, I often see the end result or reference manuals, but not many blog examples of people actually using it.
hackster.io has many projects.
Since it's a Linux ( It runs Ubuntu 18.04 LTS) you can install TensorFlow and Pytorch and run pretty much anything that don't requires newer versions.
Newer Jetsons (and more expensive ) run more up to date versions.
I think if you're going at something "from scratch" it can be a valid question to ask "Why?", if you're going "but I already have these components lying around" or "I'm technically curious" then it can make sense. It also furthers support for hardware in the arm linux infrastructure that may not have been there before and that could open up possibilities.
That's an really good example (and I missed it on my original reply) of - "because I can" !
I remember one episode of the Big Bang Theory (really really excellent series) when they guys are turning the living room lights on and off (and the stereo) using Internet by bouncing the signal through several countries and Penny asks them why and they reply - "Because we can" .
Why ? Why run an external GPU ?
I think if you're going at something "from scratch" it can be a valid question to ask "Why?", if you're going "but I already have these components lying around" or "I'm technically curious" then it can make sense. It also furthers support for hardware in the arm linux infrastructure that may not have been there before and that could open up possibilities.
I have the Jetson Nano developer KIT and it's not the most up to date stuff. Python is 3.6 and because of that I'm limited on the TensorFlow, Pytorch versions that I can install.
That's cool, I'd be interested in reading more about how people put it to use, I often see the end result or reference manuals, but not many blog examples of people actually using it on the element14 Community.
I'm using it . Still learning how to use that (with the NVIDIA specific functions - the Jetson is basically a computer that runs Linux) stuff, but it's better and faster than a Raspberry PI.
I have the Jetson Nano developer KIT and it's not the most up to date stuff. Python is 3.6 and because of that I'm limited on the TensorFlow, Pytorch versions that I can install.
Because I still have to receive my PI5 (4GB) can't compare them yet, but as soon as I get my RPI5, I will definitely compare them.
Regarding the original post, my question goes - Why ? Why run an external GPU ? If I have the need to run something that requires a GPU, I will not use a Raspberry PI. A Jetson Orin or something else that is specific for that task.