Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi2 Model B v1.2 kernel issues
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 708 subscribers
  • Views 2997 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Pi2 Model B v1.2 kernel issues

pi2bv1.1
pi2bv1.1 over 9 years ago

The new Pi2 B v1.2 uses a new chip that functions differently from Pi2 B v1.1. I wish we were told this before ordering more Pi's. We are using custom kernel in our current products with Pi2 B v1.1 and cannot just upgrade to the latest kernel/firmware. Can you point me to documentation on how to change the kernel 3.18.14 to use the Pi2 B v1.2 hardware? If that is not possible, where can I buy Pi2 B v1.1?

  • Sign in to reply
  • Cancel
  • Dudley
    Dudley over 9 years ago

    That's odd - I wasn't aware of any significant hardware differences between the various versions of the pi2 B.

     

    Are you sure that what you have isn't a B+? The B+ does have different chip to the B, and the B+ also has a v1.2.

     

    On the pi silk screen, is it definitely labelled as a B, or is it a B+?

     

    We sell the B and the B+ separately as separate products, so confusion is possible

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 9 years ago in reply to Dudley

    Dudley Nelson wrote:

     

    That's odd - I wasn't aware of any significant hardware differences between the various versions of the pi2 B.

     

    Are you sure that what you have isn't a B+? The B+ does have different chip to the B, and the B+ also has a v1.2.

     

    On the pi silk screen, is it definitely labelled as a B, or is it a B+?

     

    We sell the B and the B+ separately as separate products, so confusion is possible

    It does look like the SOC has changed on the RPi 2  model B .   The v1.1 board that I have has a BCM2836

    The v1.2 that you now show on your site here Raspberry Pi  says the RPi 2 model B has the same SOC (BCM2837) as the RPi3  but running at 900MHz

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 9 years ago

    Could you be more specific as to what no longer works. The description of the problem, "functions differently" is way too broad to make any kind of

    recommendations on if or how it can be fixed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to gdstew

    With the v1.2 new chip, the SD card doesn't boot 95% of the time, and when it does boot, only 1 CPU of the BCM2837 comes up. This SD card works fine on the old BCM2836 chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Dudley
    Dudley over 9 years ago in reply to bwelsby

    Today I learned.

     

    I've just gone and had a chat with one of our pi people (a phrase that conjures a weird mental image!)

     

    So, everyone else is correct, and I was wrong. The chip * has * changed on the latest B model. This was because the BCM2836 was getting very difficult to source, so they used the BCM2837 chip in it instead. So it now has the same chip as the pi 3 and has been underclocked to run at 900MHz.

     

    This leaves you pi2bv1.1 in a difficult position, either you're going to have to source old 1.1 versions of the B, or you'll have to bite the bullet re your Kernel, and I don't think either is palatable for you :/

     

    There was someone here who had some ideas, so I'll get him to post. cstanton

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to bwelsby

    Brian can you ener

    cat /proc/cpuinfoto check what processors are there?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 9 years ago

    Hi pi2bv1.1 ,

     

    Yes it looks like the Raspberry Pi 2 Model B has changed its SoC (processor) from the v1.1 to the v1.2, it is now running the same 64bit Quad Core processor as the Raspberry Pi 3, however it is downclocked to 900mhz processor. This means that your custom kernel isn't going to work.

     

    Your choice will be to either find Raspberry Pi 2 v1.1 devices, or to recompile your linux kernel, and you will find the sources on git, so you may be able to 'diff' between your customisations for the kernel and the sources from the Pi Foundation. This may be made a bit easier for you now that Linux Kernel 4.8 has arrived with support for the new BCM SoC chip.

     

    The Pi Foundation only recently (this week) got Raspbian booting on the Pi 2 v1.2, so if you've already tried to do this, it would be a good idea to try again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to cstanton

    Has anybody successfully configured a HotSpot/SoftAP running on a Pi2B v1.2.

    It looks like there are driver errors for the RT5370

     

    This is becoming a serious issue trying to get this to work :-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to e14 Contributor

    the kernel outputs the following errors before disconnecting the clients

     

     

    Dec  9 17:41:34 raspberrypi kernel: [  593.401956] ieee80211 phy0: rt2800usb_tx_sta_fifo_read_completed: Warning - TX status read failed -71

    Dec  9 17:41:34 raspberrypi kernel: [  593.402335] ieee80211 phy0: rt2800usb_tx_sta_fifo_read_completed: Warning - TX status read failed -71

    ...

    Dec  9 17:41:36 raspberrypi kernel: [  595.508947] ieee80211 phy0: rt2x00usb_watchdog_tx_dma: Warning - TX queue 2 DMA timed out, invoke forced forced reset

    Dec  9 17:41:38 raspberrypi kernel: [  597.228951] ieee80211 phy0: rt2x00usb_watchdog_tx_dma: Warning - TX queue 2 DMA timed out, invoke forced forced reset

    ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • spannerspencer
    spannerspencer over 9 years ago

    I wonder if we might be able to solicit some advice from our resident Raspberry Pi experts from the Community if we move this conversation into the The specified item was not found. section?

     

    I'll move it across, and maybe one of our Top Members could kick things off?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>