Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog BP Classification & announcing Results over Voice Using Pi3
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Akarshcetech
  • Date Created: 3 Dec 2022 5:14 PM Date Created
  • Views 1645 views
  • Likes 3 likes
  • Comments 1 comment
  • SpO2 Monitor
  • Voice Broadcasting
  • raspberry pi
  • BP Monitor
  • ir sensor
Related
Recommended

BP Classification & announcing Results over Voice Using Pi3

Akarshcetech
Akarshcetech
3 Dec 2022
BP Classification & announcing Results over Voice Using Pi3

image

In this Upgrade Project, I Have provided the following parameters

1. SpO2

2. IR Temperature Sensor

3. LCD Display

4. Voice Broadcasting

5. Data Saving For Future ML Training

I added the basic details of different Classifications of blood pressure for adults (18 years and older). I will utilize the same chart to create this Project.

Block Diagram Of the Project

image

I will Explain How To Interface The Sensor With the Raspberry and How to Process to Display the Output. By following this blog You can find what are the libraries and Software settings need to configure for the project.

By using This project you can measure Blood Pressure, Non-Contact IR Temperature Measurement, and SpO2. All these results are displayed on LCD and the Results are Broadcast through Voice. Based on the Accent you required you can change your Voice Broadcast Accent.

Blood Pressure sensor Interfacing With Raspberry Pi

I have used Python 3 for writing code for this project. I have used Python Idle3 to write and Run The code. By default, Raspberry Pi Will have Thonny IDE. If you want to use the same IDE as mine you need to download it by typing the following command in the Raspberry Pi terminal.

sudo apt-get install idle3

The BP Sensor Exchanges the Data Over the UART Terminal in Half Duplex Mode. This sensor Communicates the Raspberry Pi by 9600 Baud Rate. To receive the data In the Raspberry Pi We need to Configure UART Channel in the Raspberry Pi.

Raspberry Pi UART

Raspberry Pi has two in-built UART which are as follows:

  • PL011 UART
  • mini UART

PL011 UART is an ARM-based UART. This UART has better throughput than mini UART. In Raspberry Pi 3, mini UART is used for Linux console output whereas PL011 is connected to the Onboard Bluetooth module. And in the other versions of Raspberry Pi, PL011 is used for Linux console output.

Mini UART uses the frequency which is linked to the core frequency of the GPU. So as the GPU core frequency changes, the frequency of UART will also change which in turn will change the baud rate for UART. This makes the mini UART unstable which may lead to data loss or corruption. To make mini UART stable, fix the core frequency. mini UART doesn’t have parity support.

The PL011 is a stable and high-performance UART. For better and more effective communication use PL011 UART instead of mini UART.

It is recommended to enable the UART of Raspberry Pi for serial communication. Otherwise, we cannot communicate serially as UART ports are used for Linux console output and Bluetooth module.

Raspberry Pi 3 UART Pins

image

Configure UART on Raspberry Pi

In Raspberry Pi, enter the following command in the Terminal window to enable UART,

sudo raspi-config

Select -> Interfacing Options

image

After selecting the Interfacing option, select the Serial option to enable UART

image

Then it will ask for the login shell to be accessible over Serial, select No shown as follows.

image

In the end, it will ask for enabling the Hardware Serial port, select Yes,

image

Finally, our UART is enabled for Serial Communication on the RX and TX pins of Raspberry Pi

image

Then, reboot the Raspberry Pi.

Serial Port for UART Communication

By default, mini UART is mapped to UART pins (TX and RX) while PL011 is connected to the onboard Bluetooth module on Raspberry Pi 3.

In the previous versions of Raspberry Pi models, PL011 is used for Linux Console output (mapped to UART pins) and no onboard Bluetooth module exists.

After making the above configuration, UART can be used at UART pins (GPIO14 and GPIO15).

To access mini UART in Raspberry Pi 3, the ttyS0 port is assigned. And to access PL011 in Raspberry Pi 3 ttyAMA0 port is assigned. But in other models of Raspberry Pi, there is only the ttyAMA0 port is accessible.

Hardware UART port i.e. GPIO14(TXD) and GPIO15 (RXD) is also known as serial0 while other UART port connected to the Bluetooth module is known as serial1. These names are created as serial aliases for Raspberry Pi version portability.

We can check which UART i.e. mini UART (ttyS0) or PL011 UART (ttyAMA0) is mapped to UART pins (GPIO14 and GPIO15). To check UART mapping, enter the following commands.

ls -l /dev

The UART mapping for /dev/ttyS0 and /dev/ttyAMA0 is shown below,

image

After Enabling the UART we need to activate The Audio output channel. Then we have to Install gTTS (Google Text-to-Speech) to announce the BP Status in voice-over.

gTTS (Google Text-to-Speech )

gTTS (Google Text-to-Speech), a Python library and CLI tool to interface with Google Translate's text-to-speech API. Write spoken mp3 data to a file, a file-like object (byte string) for further audio manipulation, or stdout. Or simply pre-generate Google Translate TTS request URLs to feed to an external program.

Run The Below command in the Raspberry Pi terminal To download the gTTS.

pip install gTTS

To Know More About the gTTS Follow the Link https://gtts.readthedocs.io/en/latest/

after the successful installation of gTTS, we need to add a Manipulate audio with a simple and easy high-level interface, To Manipulate audio In this project, I am using pydub.

Run The Below command in the Raspberry Pi terminal To download the pydub.

pip install pydub

To Know More About the pydub Follow the Link https://pydub.com/

Once all the Mentioned Configurations are made we can Run the BP Sensor Interfacing Code.

The Output Of the BP Sensor Is saved in the Text Format In Below Figure. You can see the Results Image.

image

IR Temperature (MLX90614)Sensor Interfacing With Raspberry Pi

To interface the IR temperature sensor we need to enable The I2C and we need to install a few modules.

Enter The command in the Raspberry pi Terminal

sudo apt-get install -y python-smbus 
sudo apt-get install -y i2c-tools

install i2c support for the ARM core and Linux kernel. To enable I2C support, We need to enter the configuration Mode of raspberry By Running The Below command in the Raspberry Pi terminal

sudo raspi-config

image

Select Interfacing Configurations

image
  • In the Interfacing option, Select-> I2C

image

image

Select Yes when it asks to Reboot.

Now, after booting Raspberry Pi, we can check the user-mode I2C port by entering the following command.

ls /dev/*i2c*

then Pi will respond with the name of the i2c port.

image

Test I2C device on Raspberry Pi

Once the configuration is done correctly Connect The MLX90614 IR Temperature sensor to the Raspberry Pi I2C Pins along with the power pins.

Now when you log in you can type the following command to see all the connected devices

sudo i2cdetect -y 1

image

Once all the Mentioned Configurations are made we can Run the IR Temperature Sensor Interfacing With Raspberry Pi Code.

The Output Of the Temperature Sensor Is saved in the Text Format In Below Figure. You can see the Results Image.

image

SpO2 Sensor Interfacing With Raspberry Pi

To interface the SpO2 With the raspberry pi we use I2C Communication, Since We already Installed All the Required Configuration For I2C, LCD There is no need to enable Them Again. You Just Need To add the Library Called max30102, This Library is modified for the Raspberry Pi based on My requirements. you just need To add those files to the Folder.

The main code is in SpO2 Sensor Interfacing With Raspberry Pi file You need to run this to view the result on the LCD. Before running the code You need to save the hrcalc.py and hrdump.py and max30102.py codes to the folder location as same as the SpO2 Sensor Interfacing With Raspberry Pi code location folder.

In this project, all the above codes run individually you can modify the code to run through a single code.

  • Sign in to reply
  • shabaz
    shabaz over 3 years ago

    Hi,

    None of your code links currently work. Also, you mention BP sensor, but nowhere do you mention what that is. What's the part number?

    There's a disadvantage in doing the UART modifications that you mention. If you do that, you've lost the last resort way of logging into the Pi. Sometimes unplugging the power without a powerdown results in corruption. Having the UART as a last-resort helps to provide a way out if/when problems occur.