Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Building a Render Farm with a Bitscope Blade Quatro - Setup of the controller
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 22 Jan 2017 12:09 AM Date Created
  • Views 3491 views
  • Likes 6 likes
  • Comments 13 comments
  • cluster
  • rpiexpert
  • raspberry_pi_projects
  • blender
Related
Recommended

Building a Render Farm with a Bitscope Blade Quatro - Setup of the controller

Workshopshed
Workshopshed
22 Jan 2017

Setup of the controller node

 

SSH

The latest raspbian disables SSH by default so I turned that on and changed the hostname and password.

 

External disk

As mentioned about this is a USB disk, so it was simply a case of plugging it in and it being detected. I had a problem detecting the old IDE disk so I swapped in a SATA disk I had spare.

 

I'm not much of a command line guru so I installed gparted a graphical disk utility that I'd used before for repairing problem disks. I formatted the disk with ext4 (as it won't be accessed outside the cluster) and gave it a suitable name. On reboot it was mounted automatically.

 

I did have to resort to a command prompt to make a new directory and grant permissions to all

 

sudo mkdir /mnt/external/images/
sudo chmod 777 /mnt/external/images

 

Sharing software

Samba Server

The software for sharing files on a LAN is called Samba. The setup is quite detailed so I followed the steps in Peter Legierski's blog post below. In summary the steps are, install, set password, configure samba and configure the firewall (iptables).

 

There are a few differences I needed:

 

  • the line "security = user" did not exist so had to be added
  • the path in the smb.conf file was changed to  /mnt/external/images
  • restarting the service requires service smbd restart not samba as in Pete's notes
  • iptables did not need configuring it defaults to all access

 

Samba Client

I checked that I could connect from my windows desktop.

image

I also configured the Pi to automatically mount the network share. The first step is to make a backup of the configuration.

 

sudo cp /etc/fstab /etc/fstab.bak

 

Add a mount point

sudo mkdir /mnt/network

 

Then edit the configuration file to contain the details of what to mount

sudo nano /etc/fstab

 

I added the following to connect my share to my mount point and to use an external file for credentials

//cluster0/shares /mnt/network cifs credentials=/etc/samba/user,noexec 0 0

 

Next create a file with the user account

sudo nano /etc/samba/user

Containing the username (pi) and password from when you setup the Samba share

username=pi
password=samba_user_password

 

And finally test it works with

sudo mount -a

 

I created a file in my folder and checked it could be read over the network with

ls /mnt/network

Network

The ethernet router I was using was configured to give out the same IP addresses as my wifi so I went with Niall McCarroll's suggestion of using static IP addresses. However, I found his suggestion of using /etc/network/interfaces does not work. You need to edit /etc/dhcpcd.conf

 

interface eth0
static ip_address=10.1.1.200/24
static domain_name_servers=192.168.1.254 8.8.8.8 4.2.2.1
metric 400

 

For my controller node, I needed to change the metric of the LAN connection so that it was higher than the default for the Wifi. Otherwise attempts to reach the internet were routed to the internal router. I also needed to add the DNS entry so that commands such as apt-get still work.

 

My /etc/hosts file was

10.1.1.200   cluster0
10.1.1.201   cluster1
10.1.1.202   cluster2
10.1.1.203   cluster3

 

Finally I tested the configuration with a reboot and

ping 10.1.1.200

 

What's next

The network and disk has taken me a bit longer than anticipated so there will be another part where I setup the nodes. This will likely follow the guidance of Niall McCarroll. I'll also need to get the nodes rendering from the shared drive.

 

Reference

GParted -- A free application for graphically managing disk device partitions

Mount an external hard disk on the Raspberry Pi

Building a Raspberry Pi mini cluster - part 1

Raspberry Pi [Part 2]: External drives, Samba and SFTP | self.li - blog by Peter Legierski

Cannot restart samba, samba.service is masked - Ask Ubuntu

Samba Guide

Samba Client Guide

PiHut - connecting to network storage at boot

Internal and External IP Addresses

  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Workshopshed

    True, Andy. Using a linux distro - or a Windows with linux mix - has become way easier for the users.

    What a great leap they took from expert-manageable only to plug-and-play in many situations.

    (let's hope that developing and packaging applications for all those linux distros becomes easier too)

     

    The only thing that I'm a little uncomfortable with in your (Peter's) steps is the file with user name and password in plain text (/etc/samba/user). Is there no way to have that encrypted?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to shabaz

    Yes, a lot of this is applicable to several scenarios. I've learnt quite a lot along the way. There seems to be quite a lot of things that happen automatically in modern distros around the network and disk.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago

    Hi Andy,

     

    This is a nice reference to setting up a system actually, even for those without the blade hardware.

    I always need to search around and double-check stuff like how to do the mount, I can never remember it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<