Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Catch Santa Challenge
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mcb1
  • Date Created: 29 Jan 2014 10:00 AM Date Created
  • Views 2637 views
  • Likes 0 likes
  • Comments 9 comments
  • rpiintermediate
  • ir_led
  • ir_camera
  • raspberry-pi
  • camera
  • noir
  • raspberry_pi_projects
Related
Recommended

Catch Santa Challenge

mcb1
mcb1
29 Jan 2014

I was fortunate to be selected to receive

The Bundle & the Challenge

image

For the purposes of this "RoadTest Plus", we have bundled the Pi NoIR camera with these other products:

  • Raspberry Pi 8 GB Bundle with NOOBS
  • Wi-Pi Wifi Networking Module
  • PiFace Control & Display
  • Carbon Fibre Enclosures for both the camera and PiFace Control & Display.

 

Due to foreseen problems the products didn't ship until Dec 27th, so some action was required.

 

You can read about it here

http://www.element14.com/community/roadTestReviews/1677

 

 

While this was coming, I was asked to do something using the RPi and NoIR camera for security to include in The Shed magazine

It provides a perfect solution to those expensive and very obvious security cameras.

 

I chose to use an outside floodlight and modified an outdoor movement sensor to run off 12v, as the trigger device.

image

These were mounted on a board for testing, but can be fitted seperately, along with lamps that never come on...

 

The text of the article has been generously provided by the publisher and is attached.

(and yes it uses the normal camera image rather than the black NOir camera, its called poetic licence)

 

The conclusion was the Piface CAD is a very useful addition to any RPi, and the NoIR camera allows images to be captured without a human being aware he can be seen.

As the article says, I (and others) had problems with the WiPi , but hopefully its now setup, although its not happy if it can't find the network and tends to go to sleep.

 

There is some fine tuning to be done on the IR light source to improve its output, and I can see some other uses for this, so this may not be the only entry.

Mark

Attachments:
imageRPi camera.pdf
  • Sign in to reply
  • mcb1
    mcb1 over 12 years ago in reply to Problemchild

    John

    Thanks.

     

    I ran out of time before the article had to go to print, so I didn't have a lot of time to play with the IR LEDs.

    These were driven at 100mA, but between pulsing and a diffuser, it should be capable of reducing the zones.

     

    I intend to keep playing, but sharing it means that someone else may work in parallel.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Thanks Laureen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi, Thanks so much for a great submission..

    How much fun are our members for participating with us!! Thanks Again...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago

    Hey Mark, good work I think that the IR picture is excellent considering that you have only 12 LEDs.

    It would of been nice to stage another shot on the back wall to see how recognisable the person's face was under this illumination as

    the Police tend to be very fussy on what they would prosecute on. Also with only a few LEDs you could see differing zones of illumination

    where the beams intersected etc.

    I also like the re-engineering of a commercially available lighting system this is really practical and stuff and cheaper too image

     

    Good work .. John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<