Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Game On! Raspberry Pi Video Game Arcade Machine
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 17 Sep 2015 1:05 PM Date Created
  • Views 5589 views
  • Likes 9 likes
  • Comments 33 comments
  • raspberry_pi_arcade
  • arcade_machine14
  • retro
  • raspberrypi
  • video_gaming
  • raspberrypi2
  • raspberry_pi_projects
Related
Recommended

Game On! Raspberry Pi Video Game Arcade Machine

spannerspencer
spannerspencer
17 Sep 2015

We've been cruelly teasing you all week about a project we're about to kick off here at element14, as we alluded to the brand new Raspberry Pi case we had delivered.

image image

image image

But you guys were too quick for us. Although there were a few wry suggestions about what was being delivered -- including a rather excellent notion about building a Raspberry Pi juke box (watch this space) -- most of you astute Pi eaters sussed out that we've bagged ourselves a classic, upright arcade cab that'll soon become the company's most effective time wasting tool to date.

 

Arcade Machine14

The facts are these:

  • With your (not insignificant) assistance, we're going to strip out the cab and retrofit it with a Raspberry Pi.
  • The RPi will be used to emulate a bunch of classic video games.
  • The cab will be installed here in the element14 offices for the staff and visitors to play.
  • Any money collected by the cab will be given to a community-selected charity each month.

 

Great plan eh? But there's no shortage of work to be done before the pixels can be set free.

 

Retro Revival

There are a few factors we're endeavouring to accomplish in this project. Firstly, we want to keep the whole thing under the £500 mark, thereby making the build comparable to buying a contemporary games console. So anyone who builds along with us can divert any funds they might have allocated to an Xbox or PlayStation, and have themselves an arcade cab instead. It's a gift to yourself that keeps on giving.

 

We also want to re-use as much of the cab as possible. It's got a power supply in there already, and it still has its old 15KHz arcade monitor, which you can't beat for that authentic look. Hooking it up to a Raspberry Pi isn't going to be any small task, of course, and we're not even sure if it's working right now.

 

And then there's the controls. We'll need to interface the joysticks and buttons with the Raspberry Pi, which in itself isn't a particularly difficult task. At least, it wouldn't be, if the RPi had enough GPIO inputs for eight joystick directions (four for each stick), 12 game buttons, two game start buttons, a working coin mechanism, and however many controls we need to operate the OS front end and emulators. Hmm.

 

So we'll be calling on the element14 community for input and assistance at most every turn, and would love to hear any hints, tips or ideas you might have about putting together a Raspberry Pi arcade machine. In the meantime, we'll bring you regular blogs and discussions about how the project's going, and how you can help.

 

For now though, here's a look inside and outside the cabinet. I'll be downstairs, cleaning it for the first time in 30 years...

imageimageimageimageimageimage

  • Sign in to reply

Top Comments

  • screamingtiger
    screamingtiger over 10 years ago +2
    IMO throw the main circuit board away, as well as the monitor. Get a cheap LCD and just use a Pi. You may be able to use the power supply but its overkill. Just my .02. Gut the whole thing and put a Pi…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    It's a great project Spanner! Also interesting the charity aspect. Thinking to what are the parts to interface, I have no idea on how to do the video part (but maybe simple and cheap as far as what I know…
  • spannerspencer
    spannerspencer over 10 years ago in reply to balearicdynamics +1
    Yo Enrico! We've been kicking around a couple of ideas about hooking up the controls to the Raspberry Pi, but haven't made any decisions yet. Your solution sounds like a solid starting point! If you have…
  • e14 Contributor
    e14 Contributor over 10 years ago

    Awe that... that is beauty right there! I am trying to make something like this but maybe after christmas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    For completness though, typically the RGB signals and H/V sync are 1V ptp and about 50-75ohm impedence ish. the Monitor will be at best 640*500 or so lines in interlaced mode so quite low res for a PI but in line with many smaller LCD screens

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to spannerspencer

    Yes, but I thought you where wanting to keep the monitor for accuracy and staying true to the origional, but really I agree with the others, replaceing it with a low cost HDMI 1080P screen or even 720P and your life will be so much easier as you may spend way too much time trying to interface it than it is worth, and the LCD screen will probably be no more $$$ than the interface hardware, though the aspect ratio may be off a bit from the original.

     

    Also dont forget the monitors in most of those arcade games are mounted in Portrate not landscape

     

    As for the switches, I also agree with the general opinion that it is also overkill to try to optimise the switches in a matrix, take a leaf from Ben Heck and his pinball machine projects and use a 8 bit to Serial convertor, you could use his interface exactly  the same way so nothing to really design either, just build one on vero board or get him to send you one image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to spannerspencer

    My answer is yes. I was just thinking that a bare LCD is too "modern" instead an old TV maybe the good compromise.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 10 years ago in reply to balearicdynamics

    Yep, you guys aren't wrong -- in many respects we're making it hard for ourselves using the old monitor image

     

    When we were shopping around for an old cab, 97% of them didn't have their original monitors, or if they did they were burnt to hell. But as this one happened to still have it, we thought it was worth a bit of effort to try and get some life from it before we scrapped it image

     

    But if it becomes a huge obstacle or winds up adding a load of money to the budget, it'll probably get replaced. Maybe an old TV would simplify things, while still giving it a more authentic look?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>