Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Ground station idea for Raspberry Pi + GPS kit
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bobalexander
  • Date Created: 11 Aug 2015 2:53 AM Date Created
  • Views 931 views
  • Likes 1 like
  • Comments 3 comments
  • raspberry_pi_gps_kit
  • raspberry-pi
  • gps
  • raspberry_pi_geocaching
  • raspberry_pi_projects
Related
Recommended

Ground station idea for Raspberry Pi + GPS kit

bobalexander
bobalexander
11 Aug 2015

I was thinking this little kit might make an excellent ground station for my model aircraft.

I have a little 900MHz telemetry system that could be connected over serial to the Pi and I should be able to use the Pi to send commands to the UAV...

 

What kind of features could I add with this? Maybe a GPS based antenna tracker, or a simplified control system for changing way points?

Simple things like reporting distance to current (or last known) position would be helpful, especially in locating a crashed craft.

 

Some possible roadblocks:

Does the Pi have more than one serial port?

Can it handle processing high speed input from two GPS sources?

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago +2
    Here is a detailled connection and operation of Rasberry Pi with Pixhawk Autopilot and Mission Planner Groud Control Software (That can do Antenna tracking Using Gps signal coming from Plane Telemetry…
  • cstanton
    cstanton over 11 years ago +1
    The Pi only has one directly accessible serial port on the GPIO pins, however it also has i2c. You can get GPS devices that connect via USB, which would work. The Pi 2 should be capable of handling input…
  • bobalexander
    bobalexander over 10 years ago in reply to e14 Contributor

    That's pretty good. I should be able to write up roughly the same thing for Cleanflight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Here is a detailled connection and operation of Rasberry Pi with Pixhawk Autopilot and Mission Planner Groud Control Software (That can do Antenna tracking Using Gps signal coming from Plane Telemetry):

     

    Communicating with Raspberry Pi via MAVLink | Developer

     

    Have Fun

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 11 years ago

    The Pi only has one directly accessible serial port on the GPIO pins, however it also has i2c. You can get GPS devices that connect via USB, which would work.

     

    The Pi 2 should be capable of handling input from two GPS sources.