Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog How I Built a Raspberry Pi 3 SDR Radio Ground Station with OpenWebRX
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: afernandez
  • Date Created: 11 Jul 2026 9:20 AM Date Created
  • Views 505 views
  • Likes 4 likes
  • Comments 11 comments
  • raspberry
  • project
  • rpi3
  • raspberry pi
  • raspberrypi
Related
Recommended

How I Built a Raspberry Pi 3 SDR Radio Ground Station with OpenWebRX

afernandez
afernandez
11 Jul 2026
How I Built a Raspberry Pi 3 SDR Radio Ground Station with OpenWebRX

Hi, community!

I’m writing this post because I’d like to share my radio ground station project, built using an old Raspberry Pi 3 that I found in a box at home.

First, I’d like to give you some context. A few months ago, I started learning about a new hobby: radio! I don’t have my Spanish amateur radio licence yet, so I’m not authorised to transmit, although I’m currently working towards getting it. In the meantime, I wanted to build a ground station that would allow me to explore and listen to different radio frequencies.

One of the most important parts of the project is the antenna. Since I don’t have much available space, I decided to buy a Diamond X50. It is a compact, dual-band VHF/UHF antenna that is approximately 1.7 metres long. I installed it on a standard TV antenna mast.

image

Lightning and surge protection are also very important, so I connected the antenna mast to a grounding point and installed a Diamond SP1000PW coaxial surge protector.

image

In the future, I would also like to transmit using this antenna. For that reason, I added a coaxial switch that allows me to select either the SDR receiver or the TX/RX radio.

image

I had to modify the coaxial switch by adding some internal insulation. By default, the inactive port was shorted to ground, which could potentially damage the transmitter if I accidentally tried to transmit while the SDR position was selected.

Once the installation was complete, I used my NanoVNA to measure the antenna system, check its resonant frequencies and analyse the SWR across the supported bands. These were the results.

imageimageimage

For SDR reception, I chose a Nooelec NESDR Smart v5. I also added a Nooelec Flamingo FM filter to reduce interference from powerful commercial FM broadcast stations.

Finally, I installed the required SDR drivers on the Raspberry Pi 3 and set up OpenWebRX, allowing me to access the receiver remotely through a web browser and listen to different frequencies.

imageimage

There are still many things I would like to improve, but I’m very happy with the results so far. I hope you find the project interesting, and I’d love to hear your suggestions and feedback!

  • Sign in to reply

Top Comments

  • afernandez
    afernandez 1 month ago in reply to kmikemoo +1
    hahaha kmikemoo I have the same problem now , I spend more time tinkering than talking
  • DAB
    DAB 1 month ago in reply to afernandez

    I have played with a cheap SDR.

    Many years back I was the Independent Software Verification engineer for an Integrated Communications Navigation Identification Avionics system.

    The prime contractor built a common set of hardware that could be programmed to receive and transmit any of the CNI signals.

    My background proved very useful in assessing how well the resulting hardware and software worked. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • afernandez
    afernandez 1 month ago in reply to kmikemoo

    hahaha kmikemoo  I have the same problem now Joy, I spend more time tinkering than talking

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo 1 month ago in reply to afernandez

    afernandez I am WI9MMM.  I am a builder ham more than a talker ham.  Almost all of my on-air time is on 2m.  I really only do HF on ARRL Field Day.  I thought I would radio more, but there are just so many bright shiny things out there. Joy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Qbit
    Qbit 1 month ago

    This is a fantastic write-up! OpenWebRX is such a powerful tool for making SDR setups accessible over a local network or the internet without clunky desktop software client dependencies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • afernandez
    afernandez 1 month ago in reply to kmikemoo

    I have the same problem with my current projects, haha. My ultimate goal is to add a Ku-band antenna to monitor weather satellites, but I don’t have any space left on my roof because of the solar panels. However, I think it might be possible to build the setup in my garden.

    For now, I’m really excited to start making contacts on the 2-metre band! Hopefully, in the future, I’ll also be able to get some HF equipment and make contacts over much longer distances.

    Do you have a radio callsign?

    Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>