Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog How I Built a Raspberry Pi 3 SDR Radio Ground Station with OpenWebRX
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: afernandez
  • Date Created: 11 Jul 2026 9:20 AM Date Created
  • Views 478 views
  • Likes 4 likes
  • Comments 11 comments
  • raspberry
  • project
  • rpi3
  • raspberry pi
  • raspberrypi
Related
Recommended

How I Built a Raspberry Pi 3 SDR Radio Ground Station with OpenWebRX

afernandez
afernandez
11 Jul 2026
How I Built a Raspberry Pi 3 SDR Radio Ground Station with OpenWebRX

Hi, community!

I’m writing this post because I’d like to share my radio ground station project, built using an old Raspberry Pi 3 that I found in a box at home.

First, I’d like to give you some context. A few months ago, I started learning about a new hobby: radio! I don’t have my Spanish amateur radio licence yet, so I’m not authorised to transmit, although I’m currently working towards getting it. In the meantime, I wanted to build a ground station that would allow me to explore and listen to different radio frequencies.

One of the most important parts of the project is the antenna. Since I don’t have much available space, I decided to buy a Diamond X50. It is a compact, dual-band VHF/UHF antenna that is approximately 1.7 metres long. I installed it on a standard TV antenna mast.

image

Lightning and surge protection are also very important, so I connected the antenna mast to a grounding point and installed a Diamond SP1000PW coaxial surge protector.

image

In the future, I would also like to transmit using this antenna. For that reason, I added a coaxial switch that allows me to select either the SDR receiver or the TX/RX radio.

image

I had to modify the coaxial switch by adding some internal insulation. By default, the inactive port was shorted to ground, which could potentially damage the transmitter if I accidentally tried to transmit while the SDR position was selected.

Once the installation was complete, I used my NanoVNA to measure the antenna system, check its resonant frequencies and analyse the SWR across the supported bands. These were the results.

imageimageimage

For SDR reception, I chose a Nooelec NESDR Smart v5. I also added a Nooelec Flamingo FM filter to reduce interference from powerful commercial FM broadcast stations.

Finally, I installed the required SDR drivers on the Raspberry Pi 3 and set up OpenWebRX, allowing me to access the receiver remotely through a web browser and listen to different frequencies.

imageimage

There are still many things I would like to improve, but I’m very happy with the results so far. I hope you find the project interesting, and I’d love to hear your suggestions and feedback!

  • Sign in to reply

Top Comments

  • afernandez
    afernandez 1 month ago in reply to kmikemoo +1
    hahaha kmikemoo I have the same problem now , I spend more time tinkering than talking
  • kmikemoo
    kmikemoo 1 month ago in reply to afernandez

     afernandez When I first got in the hobby, I wondered why so many Hams had multiple radios and antennas.  This may be why.
    Maybe the SDR gets its own wide band (receive) antenna - like a discone - and your regular radio uses the Diamond.  It's just a thought.
    I am still using a 4-position switch for the 2m band.  I have many 2m antennas - but only one of them is mounted to the house right now. Joy
    I have a satellite dish slot antenna that I want to mount and try out.  I just have too many projects going on right now.  It will probably get tested on a tripod and then stored with the other antennas until... someday. Sweat smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo 1 month ago in reply to DAB

     DAB I got into the hobby late in life.  It was/is my first adult hobby that wasn't directly related to my job.  I was intrigued by doing email over radio - which I learned about while in the service.  I'm really in the hobby for the electronics and to build stuff. Joy  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • afernandez
    afernandez 1 month ago in reply to DAB

    Uooo! This sounds good! If you have interest in this hobby, there are a lot of public SDR radio servers public Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • afernandez
    afernandez 1 month ago in reply to kmikemoo

    Thanks kmikemoo !!! I'm now make some test in the setup, and final idea is that you say, but i'm currently not found a solution to ensure that the radio trasminter can't operate if the rf conector is switched to ground jajajaja I not have any solution for this now.... but i thinking arround

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 1 month ago

    Well done.

    I never got into amateur radio, but in Tech School I did get a 2nd class FCC license, which got me an A for the class.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>