Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Hydrogen Fuel Cell Bench Test Rig
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 22 Aug 2014 10:24 AM Date Created
  • Views 1335 views
  • Likes 1 like
  • Comments 3 comments
  • hydrogen
  • UAV
  • raspberrypi
  • rpiexpert
  • fuel-cell
  • raspberry_pi_projects
Related
Recommended

Hydrogen Fuel Cell Bench Test Rig

e14 Contributor
e14 Contributor
22 Aug 2014

Hydrogen Fuel Cell Bench Test Rig

 

Background:

Hydrogen Fuel Cells!

Hydrogen Fuel Cell Controller Demonstration

Hydrogen Fuel Cell Polarisation Curve

You may have seen some previous posts (above) about my developmental test rig for hydrogen fuel cells.  Well I am pleased to say it has now finished the final stage of prototyping!

 

I have released the code on github and have tried to make it as user friendly as possible, however I would really appreciate some feedback! Even if you do not have a fuel cell, you can still run the code with an AdcPiV2 and a PiFaceDigitalIO; although it won't do a lot but you can check out the user interface!!  All code is in Python3 so pretty easy to work with.

 

Obviously this is a very specific project which many people cannot replicate however I thought it would be cool to show the hobbyist community that the rPi is being used in research as such an awesome solution to the rapid prototyping of electronics and control. In my opinion, the reason that the rPi is more popular in my area that BB and the like is the community support. If we can't figure out how to do something then the forums are awash with people wanting to help.  Many thanks to all of you!

 

Graphs:

Among the millions of graphs I have, here are a couple of ones that illustrate some stuff you may find interesting:

1. On the left, the profile is the "power demand." As you can see the fuel cell is slow to respond to demand, which is expected. More interestingly, the green "Raspi" line is the attopilot90 current and voltage sensor hooked up to an AdcPiV2, and the load bank is a `mucho expensivo' calibrated research device.  Looking pretty good for the rPi!

2. On the right is a similar graph but with mass flow rate of hydrogen.  This is calculated from a 0-5v analogue signal from a sensor, being fed into an Arduino 2560, which is then connected to the rPi over I2C.  I have also included a dynamic purge controller, hence the quicker reaction time. image

imageimage

 

Rig:

Here is the messy entanglement of wires which is the prototype rig.  Soon to be condensed down into a single rPi board which will plop straight onto the GPIO header.

imageimage

 

 

Hope you found this interesting and a bit different!

 

Simon

________________________________

Low Carbon Technologies Group

Aeronautical & Automotive Engineering

Loughborough University

United Kingdom

  • Sign in to reply
  • mcb1
    mcb1 over 12 years ago

    Nice to see.

     

    For the uninitiated here ...

    Your graph suggests a water flow rate of 2.5 Litres/min at 100w.

    If that's the figure this would equate to 150 litres for 1 hr at 100w (100wH), which is 150kg weight.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago

    Referring to your first picture - it looks like a really complicated way to make a cup of tea !!

     

    What's the fancy rack box with all the buttons ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago

    Hi Simon,

     

    It is good to hear from you again.

    It looks like you are making some good progress with your device and testing.

     

    Look forward to seeing how well this technology pans out.

    DAB