Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog PIK3A Retro Gaming Table Mk II
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 22 Mar 2016 10:45 AM Date Created
  • Views 18256 views
  • Likes 12 likes
  • Comments 44 comments
  • retro gaming
  • rpibeginner
  • retro
  • pi3
  • pik3a
  • raspberry pi
  • raspberry_pi_projects
Related
Recommended

PIK3A Retro Gaming Table Mk II

spannerspencer
spannerspencer
22 Mar 2016

I'm not a fan of Ikea. In fact, it's a place I usually try to avoid, until I discovered that you can hack it's ultra-cheap tables into retro video game systems! You know the one I mean: PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table.

 

You guys have been busy making your own versions, which I'm thrilled to be reading about. Keep those photos and top tips coming.

 

But in the meantime, meet PIK3A Mark II.

image

Hackin' the LACK

This is, in many respects, the same build as the PIK3A Mk I. The idea came about when I initially bought the square LACK tables that we mounted a monitor in, and added controls to. I was casually keeping an eye out for a table that'd accommodate two players, with six buttons each. You know. A Street Fighter II machine!image

 

There were definitely options, but the table size makes them prohibitively intrusive for the average living room. So I needed a way to reduce it, while maintaining the full control set.

 

The answer presented itself in the LACK TV stand; a narrow, 90cm by 26cm table that boasts a shelf and a table top deep enough to accept the joysticks and buttons. By dispensing with the monitor and going straight into the TV, the unit is easily accommodated in your average (well, as average as us element14 types ever really are) front room.

 

There isn't much to explain about the build that isn't already covered in the PIK3A Mk I. I cut two access holes in the bottom so I could get to the joystick and buttons for each player, and drilled start and coin buttons into the edge as before.

image

I kept the Raspberry Pi 3 external, mounting it in a case underneath the table top, in the centre. It's still nicely hidden, and there's only a short length of USB cable from the controls into the RPi. The benefits of this are that you don't need any extensions or panel mount connectors for the micro USB input or HDMI output. It also makes it easy to get to the SD card, should you need to.

 

There's no need for any acrylic or polycarbonate sheeting over the top either, given that there's no screen, making this a quick, simple yet highly effective variation on the PIK3A.

 

That said, one nice tweak might be coming up with a way to eliminate the HDMI cable and send the video to the TV wirelessly. Any thoughts on that?

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • bwelsby
    bwelsby over 10 years ago in reply to shabaz +2
    Hm yes 12 inputs may not be enough, how about another hack... as in hack a genuine bluetooth keyboard
  • e14 Contributor
    e14 Contributor over 10 years ago +2
    You can hack a LG an-wl100 to wireless transmit HDMI and you can buy them for around 15 bucks on eBay. Directions for hacking Hacking the LG Wireless Media Kit AN-WL100W . Not a compact solution but it…
  • ipv1
    ipv1 over 10 years ago +1
    Awesome man!
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to spannerspencer

    Hi there - do you have the leonardo code you used for each controller?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 10 years ago in reply to e14 Contributor

    Hi there David! I can't remember exactly, but I think this is the layout I used for the joystick and buttons when building this table.

     

    image

     

    As you say, I just drilled through from above, and cut out the bottom of the table from underneath to mount them, and wire them up. Exactly the same as when building the PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi there.  My son and I are trying to build this as a little project.  I've got all the parts I need and was wondering if someone could help me with a template for the joystick and buttons for the layout shown in the picture.  Also is there a need to cutout the underside of the table for the buttons and joystick or could you simply drill through the table top and attach the joystick below and also the buttons?

     

    Thanks in advance,

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tonyboubady
    tonyboubady over 10 years ago in reply to e14 Contributor

    I can answer your 2nd question... and i have never tried this before but just a suggestion...

    You need to buy bluetooth module with HID(Human Interface Design) profile...

    Here is one https://www.adafruit.com/product/1535

     

    it has 12 input, so it's enough for you to design your buttons with this one...as well you don't need that serial bluetooth profile with Arduino...Rpi 3 has bluetooth so you can pair it directly...

     

    Hope the Rpi 3 linux distro works with this module...again not sure as I am not owning raspberry pi...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi!,

     

    Congrats on your project, its very inspiring! I am planning on building a table like yours, with the exception of having the rapsberry on the tv and trying to connect the arduino wirelessly via bluetooth and powering it with a powerbank or something.

    Having no prior experience with electronics and this kinda projects i have a few questions.

    1) What kind of wires and approximately how long, do i need for connecting the arcade buttons with the controller? Male to Male Jumper wire? Do i have to smolder it?

    2) Its 1 bluetooth adapter for each controller, right? Can you point out a suitable one to buy?

    3) All the holes are 28mm wide for the buttons as i figured out, is there a fixed size for the joystick too, or you cut the wood manually?

     

    Thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>