Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Pilolu - 3D controller for Raspberry Pi.
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 28 Aug 2015 6:23 AM Date Created
  • Views 396 views
  • Likes 0 likes
  • Comments 0 comments
  • 3d
  • printing
  • raspberry_pi_projects
Related
Recommended

Pilolu - 3D controller for Raspberry Pi.

e14 Contributor
e14 Contributor
28 Aug 2015

I'm working on a 3D controller hat for a Raspberry Pi. This is a glimpse of the hardware prototype. You can see the USB and ethernet ports of the Pi on the left side.

 

image

 

Features:

 

4 motor control channels

  - compatible with A4988 and DRV8825 Stepstick motor drivers

  - Motor supply voltage up to 45V

 

3 High power (15A Max) 12v/24v discrete switch channels to drive fans, heaters, extruders, spindles etc.

 

6 Digital switch inputs for limit switches. Can also be used as 3.3V digital outputs

 

4 Thermistor input channels

 

4 Unassigned analogue inputs.

 

SPI port for expansion.

 

The board provides power to the Pi, and can run from 7-12V DC. It has separate supplies for the bed and motors.

 

The software is the hard bit (for me at least).  I'm looking at a real-time raspbian kernel at the moment.  The Pi will probably have to run a kernel device driver to drive the motors, but will probably be able to use the BCM2835 GPIO library for everything else.