Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Punch It Up: RPi Arcade Game Proposal
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ipv1
  • Date Created: 6 Apr 2016 1:47 PM Date Created
  • Views 1287 views
  • Likes 5 likes
  • Comments 5 comments
  • global_arcade
  • punch_it_up
  • ip_iot
  • raspberry_pi_projects
Related
Recommended

Punch It Up: RPi Arcade Game Proposal

ipv1
ipv1
6 Apr 2016

Introduction

 

New age gaming is all about new technology and advanced peripherals or toys and has given rise to things such as motion gaming. The old arcade games with a big machine with large buttons and 8 bit graphics and sounds brings backs so many memories of childhoods passed which need to be relived sometimes. The proposed project is about breathing life into the old and bulk arcade machine which was a great source of entertainment (with a bit of nostalgia). “Punch it up” is an arcade based game with a lot of physical exercise included and is more or less a fighting game. With the help of large punchable buttons, you get to fight your opponent while standing right besides him in a virtual fighting game. This concept roots from the classical “big game” form factor but takes advantage of the programming capabilities offered by the Raspberry Pi 3 as well as the extensive processing power to make things more new age.

 

How it works

 

image

Figure 1. Basic Game Layout

 

The game is designed with each player having one joystick and a set of 4 buttons arranged as shown in figure 1,  that can be punched to activate in-game functions which gives the player a physical feeling of the game. There are button pads which are designed with a cushion to protect your hand when you punch them and they stand on top of regular arcade buttons. The pads are removable if you want to revert back to the original arcade game button feel. When playing the game, the joystick function just like  your avatar move around and dodge the attack while the punching buttons are to land punches and kicks on your opponent. Synchronise the punches/kicks and the position of your avatar for a successful ‘KO’ of your opponent.

 

Implementation

 

image

There are two plans of action for this project. The first involves using retro pi to play the classic arcade games like street fighter. Only this time, instead of a gamepad, you get to literally such buttons to make the characters punch in game. Buttons 5 and 6 however will be made a part of a wired joystick which the user will hold in the hand. For combos, the user can keep a button pressed while punching the second button thereby executing more advanced moves.

 

 

As shown in the diagram above, we can use a wired soft stick with two buttons conveniently placed near the thumb.

 

image

For the second phase of implementation, now of out team members will try and implement a game of our own where we take pictures of our opponent and use it in the game. The total screen is split into 8 columns and 2 rows with a 2x2 matrix available to each player. The user image is displayed to the opponents screen in one of the 4 squares. The opponent can punch one of the 4 buttons to punch in one of the 4 squares. If you are able to punch the right square you get a point. The user can move his image within the 4 squares using the joystick to avoid getting punched. The game is to punch the opponent while avoid getting punched yourself.

 

 

Risks and challenges

The only challenge here is getting the enclosure sturdy enough to take the punches. We will be taking the help of a carpenter to fabricate something that can really take it.

 

Summary

We are proposing a twist to the original arcade game form factor while adding a new arcade game of our own. Its our first experience with such a project and once we finish this one, we can really kick things up a notch

 

 

Thanks,

Punch It Up Team

 

g++, shubhamsharda, shwetankv007 ipv1

  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 10 years ago in reply to clem57 +3
    This one is a team proposal. The enlisted few are students at the university where I teach...
  • jkutzsch
    jkutzsch over 10 years ago in reply to ipv1 +2
    I like it! I could see where you could even add a 3rd phase, once you were able to get another device created, and maybe even link for remote beat downs! Throw a camera on there and enjoy the Global interaction…
  • clem57
    clem57 over 10 years ago +1
    ipv1 Nice Idea. Was this a joint decision? Or group think? Clem
  • ipv1
    ipv1 over 10 years ago in reply to e14 Contributor

    Thats a good idea and can be implemented. Though its a portable system I would not call it a handheld. Its designed to be sturdy and a fixed system infact.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Cool idea!

     

    The game can include a bit of control switching too to avoid the monotonous gameplay just to have an efficient use of the device.

    Since, it's handheld, putting the entire play on punches only might become repulsive.

     

    But it's a unique idea as such.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 10 years ago in reply to ipv1

    I like it!  I could see where you could even add a 3rd phase, once you were able to get another device created, and maybe even link for remote beat downs!  Throw a camera on there and enjoy the Global interaction of video gaming! 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 10 years ago in reply to clem57

    This one is a team proposal. The enlisted few are students at the university where I teach...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago

    ipv1

         Nice Idea. image Was this a joint decision? Or group think?

    Clem