Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry Pi 2in1 Gaming Tablet
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tobiassmullet
  • Date Created: 17 Jan 2017 11:50 AM Date Created
  • Views 978 views
  • Likes 3 likes
  • Comments 3 comments
  • raspberry_pi_projects
Related
Recommended

Raspberry Pi 2in1 Gaming Tablet

tobiassmullet
tobiassmullet
17 Jan 2017

Morning all!

 

I'm working on a little Pi Project, and I'd like to get your input on logistics or and ideas you might have to make it easier/better.

 

Basically, I'd like to have a device that can run Retropie with dedicated gaming buttons, and also run an Andrid like tablet operating system.

 

The idea is that I have a custom Tablet case with a touchscreen, and inside there will be 2 Raspberry Pi units, one of them running RetroPie, and one running Android or an alternative. I'd like it to have one Power button, with a toggle switch to choose between the two systems.

 

The RetroPie system will be hooked up to some buttons/joysticks for gaming, and the Android tablet will be hooked up to a home button. Ideally there would be a shared Battery for both units in the middle behind the screen, or 2 separate ones if that's easier to set up. I'd like to have a USB port for both units for file transfer, and for multiplayer on the Retropie, and ideally an HDMI out for use with a monitor.

 

I've made a little mockup to demonstrate what I mean, or roughly what I'd like it to look like, if you can see any problems or potential issues with the design, features, or the concept as a whole, let me know! I'm interested to see what you guys think!

 

image

 

 

CHEERS

  • Sign in to reply
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to e14 Contributor

    Lucie I think this can be a good tird option. What if I have battery powering a second - unised - Pi ?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago

    Nice concept, rather than having a power button that selects one Pi being on or the other maybe there could be an option to have both powered at the same time and a way to switch the screen between one or the other so you can switch between them without having turn one off first.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • inghernandez
    inghernandez over 9 years ago

    That´s a nice job, congratulations friend