Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry Pi B+ can do double duty and more
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 31 Oct 2015 12:34 AM Date Created
  • Views 789 views
  • Likes 2 likes
  • Comments 0 comments
  • raspberry_pi_projects
  • pumpkinpi2015
Related
Recommended

Raspberry Pi B+ can do double duty and more

e14 Contributor
e14 Contributor
31 Oct 2015

  As I mentioned last time, I added a Raspberry Pi B+ to the project, basically to take advantage of its GPIO pins.  Today, I was going to start interfacing the Arduino , which is driving the Neopixel stick.  I had read that there was a nice library for letting ArmV6 Raspberry Pis Raspberry Pis drive NeoPixels.  So, I movel the NeoPixel stick over to the secondary Raspberry Pi in thes project, which is a Raspberry Pi B+.  I tried out the library and it works quite well so far.  So, now this Pi is detecting people walking up with the PIR sensor, and driving the NeoPixe stick.  I expect it will have no problem controlling the relay board.  That is really simple, and timing is not crucial.  I thought I might be keepingthe B+ busy enough that the NeoPixels might not look good, but the Raspberry Pi is doing just fine.  Here is a picture of the B+ with the PIR module, and NeoPixel stick connected.

image

 

The Raspberry Pi B+ is in a nice case I printed from a design on thingiverse.  I am still experimenting with how to mount the Raspberry Pi 2 B with the Sense Hat.  It may justget mounted on a spare VESA plate I laser cut.  The HAT gets in the way for most cases and I can'y getto the laser cutter to design a custom case at the moment.  Let me give you a close up on the breadboard showing the connection a little better.

image

 

I will also add a short video showing the NeoPixel stick running from the B+/  The B+ is running the PIR detection script at the same time and is commanding the Raspberry Pi 2 B to scroll fog messages across the Sense Hat.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

  The final assembly blog entries by the project designer(Charles Gantt)have not shown up yet, so I am going to  improvise.  I'll probably mount things in a box and tie them down with twine. I'll show more on that next time.