Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry Pi Connected Picture Frame
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 28 Aug 2017 7:34 PM Date Created
  • Views 13237 views
  • Likes 20 likes
  • Comments 50 comments
  • rpibeginner
  • raspberrypi
  • display
  • resin.io
  • iot
  • raspberry_pi_projects
  • resinos
  • picture frame
Related
Recommended

Raspberry Pi Connected Picture Frame

fvan
fvan
28 Aug 2017

This project is about a digital picture frame aimed at family members, such as grandparents.

 

The idea is that parents taking pictures of their children, can easily share those pictures with the children's grandparents by making them appear on the picture frame automatically. In turn, the grandparents can "like" the pictures, letting the children's parents know which pictures are their favourites.

 

By making use of a specific software platform called resin.io, multiple instances of this picture frame can be deployed for various family members, without hassle.

 

  • Features
  • Hardware
  • Software
    • resin.io
      • Application Creation
      • Flashing SD Card
      • Configuration & Environment Variables
      • Application Deployment
    • IFTTT
  • Demo

image

 

Features

 

The project makes use of different services. Here's an overview:

 

image

 

The picture frame offers following features:

  • simple user interface to navigate the pictures, start a slideshow or like a picture
  • periodically download pictures from a shared Dropbox folder
  • send push notifications whenever a picture is liked
  • Turn the picture frame's display off every evening, and back on every morning

 

Let's take a closer look at the software and hardware for this project, and how you can build your own connected picture frame.

 

Hardware

 

The following hardware components are used in this project:

  • Raspberry Pi 3 with 16GB MicroSD cardRaspberry Pi 3 with 16GB MicroSD card
  • Official Raspberry Pi 7" Touch ScreenOfficial Raspberry Pi 7" Touch Screen
  • Official Raspberry Pi 5.1V/2.5A Power SupplyOfficial Raspberry Pi 5.1V/2.5A Power Supply
  • Raspberry Pi Touch Screen EnclosureRaspberry Pi Touch Screen Enclosure

 

Assembly is super easy, following these steps:

  1. Mount the Raspberry Pi 3 to the Raspberry Pi Touchscreen
  2. Connect the jumper wires from the screen's board to the Pi for power
  3. Slide the Touchscreen assembly through the enclosure's front bezel
  4. Screw everything in place

Do not insert the microSD card or power on the frame yet, as the software needs to be

image

 

Software

 

The complexity of the project is in the software. Let's break it down.

 

resin.io

 

Resin.io makes it simple to deploy, update, and maintain code running on remote devices. Bringing the web development and deployment workflow to hardware, using tools like git and Docker to allow users to seamlessly update all their embedded linux devices in the wild.

Resin.io's ResinOS, an operating system optimised for use with Docker containers, focuses on reliability over long periods of operation and easy portability to multiple device types.

To know more details about how resin.io works, be sure to check out this page: How It Works

Sign up for a free account and go through the detailed Getting Started guide. From there, you can create your first application.

 

Application Creation

 

Setting up a project requires two things:

  • application name: ConnectedFrame
  • device type: Raspberry Pi 3

 

image

 

After completing both fields and creating the application, a software image can be downloaded for the devices to boot from. The useful part is that the same image can be used for every device involved in the project. Select the .zip format, which will result in a file of about 400MB, as opposed to 1.8GB for the regular .img file.

image

Before downloading the image, connectivity settings can be specified, allowing the device to automatically connect to the network once booted. Enter the desired SSID and matching passphrase.

 

Flashing SD Card

 

Once the image specific to the application is downloaded, it needs to be flashed to a microSD card for the Raspberry Pi to boot from.

 

There is a tool available for doing just that, by the same people from resion.io, called Etcher. It works on mac, Linux and Windows, is simple to use and gets the job done.

image

 

Launch Etcher, select the downloaded image file. Etcher should automatically detect the SD card, all that remains is to click the "Flash" button.

 

The SD card is ready to be inserted in the Raspberry Pi.

 

Configuration & Environment Variables

 

Some raspberry Pi configuration changes are typically made by editing the /boot/config.txt file. Resin.io allows users to do this via the user interface, by defining Device (single device) or Application (all devices) Configuration Variables.

 

In config.txt, pairs of variables and values are defined as follows: variable=value

 

Using the Device/Fleet Configuration, the variable becomes RESIN_HOST_CONFIG_variable and is assigned the desired value.

 

For example, rotating the LCD touch screen is normally done by appending lcd_rotate=2 to /boot/config.txt. As a configuration variable, this becomes RESIN_HOST_CONFIG_lcd_rotate with value 2.

image

 

Another type of variables, are Environment Variables, which can again be defined at application or device level.

 

image

 

These environment variables can be used by the operating system, such as "TZ" which is used to set the correct timezone, but also by scripts.

 

Following environment variables are used by the connected frame Python script:

  • DISPLAY: display to use for the Tkinter user interface
  • DROPBOX_LINK: link to dropbox shared folder
  • IFTTT_KEY: personal IFTTT webhooks key to trigger notifications
  • DOWNLOAD_INTERVAL_HOURS: interval in hours to download photos from the dropbox folder
  • CAROUSEL_INTERVAL_SECONDS: interval in seconds to automatically switch to the next photo
  • FRAME_OWNER: the name of the person the frame belongs to, used to personalise the "like" notification

 

Most are to be set at application level, though some variables such as FRAME_OWNER are specific to the device.

The link to the shared dropbox folder ends with "?dl=0" by default. This has to be changed to "?dl=1" in the environment variable, to allow the application to download the pictures.

 

Application Deployment

 

I've been developing a Python application using Tkinter to create the graphical interface for the picture frame.

The layout is simple: four interactive buttons (two on each side), with the picture centralised.

 

Deploying an application with resin.io requires some additional files, defining which actions to perform during deployment and which command to use to start it. The full code and accompanying files for this project can be found on GitHub.

 

You can clone the repository for use in your resion.io application, reproducing the exact same project, or fork it and modify it as you desire!

 

git clone https://github.com/fvdbosch/ConnectedFrame 
cd ConnectedFrame/

 

In the top right corner of your resin application dashboard, you should find a git command. Execute it in the cloned repository.

 

git remote add resin gh_fvdbosch@git.resin.io:gh_fvdbosch/connectedframe.git

 

Finally, push the files to your resin project:

 

git push resin master

 

If all went well, a unicorn should appear!

image

 

In case of problems, a clear error message will appear, telling you what exactly went wrong.

 

IFTTT

 

"IFTTT" stands for "If this, then that" and is an online platform that enables users to connect triggers and actions for a plethora of services.

 

For this particular project, the webhooks service is used to trigger notifications to the IFTTT app on a smartphone.

image

 

The trigger is part of the code and needs to remain as is, though the action could be modified to suit your own personal needs.

 

Demo

 

Enough with the theory, let's see the frame in action!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What do you think? Is this something you could see family members use? Let me know in the comments! image

  • Sign in to reply
  • fvan
    fvan over 8 years ago in reply to nickuk77

    Can you try changing the extension of your images to lower case "jpg" and see if that helps?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nickuk77
    nickuk77 over 8 years ago

    Hi everyone. Not sure if this thread is still active but I just discovered this project and after I setup everything I get following error:

     

    20.05.18 19:06:53 (+0100)  maininflating: /usr/src/app/images/#www.dropbox.com.url20.05.18 19:06:53 (+0100)  maininflating: /usr/src/app/images/DSCN0017.JPG20.05.18 19:06:54 (+0100)  maininflating: /usr/src/app/images/DSCN0018.JPG20.05.18 19:06:54 (+0100)  maininflating: /usr/src/app/images/DSCN0019.JPG20.05.18 19:06:54 (+0100)  maininflating: /usr/src/app/images/DSCN0020.JPG20.05.18 19:06:54 (+0100)  maininflating: /usr/src/app/images/DSCN0021.JPG20.05.18 19:06:55 (+0100)  maininflating: /usr/src/app/images/DSCN0026.JPG20.05.18 19:06:55 (+0100)  maininflating: /usr/src/app/images/DSCN0027.JPG20.05.18 19:06:55 (+0100)  maininflating: /usr/src/app/images/DSCN0028.JPG20.05.18 19:06:55 (+0100)  maininflating: /usr/src/app/images/DSCN0029.JPG20.05.18 19:06:56 (+0100)  maininflating: /usr/src/app/images/DSCN0032.JPG20.05.18 19:06:56 (+0100)  maininflating: /usr/src/app/images/DSCN0033.JPG20.05.18 19:06:56 (+0100)  maininflating: /usr/src/app/images/DSCN0034.JPG20.05.18 19:06:57 (+0100)  maininflating: /usr/src/app/images/DSCN0035.JPG20.05.18 19:06:57 (+0100)  maininflating: /usr/src/app/images/DSCN0036.JPG20.05.18 19:06:57 (+0100)  maininflating: /usr/src/app/images/DSCN0037.JPG

    20.05.18 19:07:09 (+0100)  main  Traceback (most recent call last):

    20.05.18 19:07:09 (+0100)  main    File "/usr/src/app/connectedframe.py", line 154, in <module>

    20.05.18 19:07:09 (+0100)  main      center_image = Image.open(image_list[0])

    20.05.18 19:07:09 (+0100)  main  IndexError: list index out of range

    20.05.18 19:07:09 (+0100)  main  xinit: connection to X server lost

    20.05.18 19:07:09 (+0100)  main

    20.05.18 19:07:09 (+0100)  main  waiting for X server to shut down (II) Server terminated successfully (0). Closing log file.

    20.05.18 19:07:10 (+0100)  main

    20.05.18 19:07:10 (+0100)  main  xauth: (argv):1:  bad display name "45e2263:0" in "remove" command

     

    If anyone know why I am getting "list index out of range", can you please reply?

     

    Thank you very much!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bishely
    bishely over 8 years ago in reply to salmanslim

    Hi Salman

     

    Sorry if this seems patronising, but are you aware that the crontab message you tested should turn the display off at 6:30 AM every day? Remember that crontab's hours column is in 24hr format, so 6 PM is 18. Also, make sure that you're using the correct value for off/on as they're a little odd (to me, at least) - 1 is off, and 0 is on.

     

    So if you want it to turn off at 6AM, use the line you tested:

    30 6 * * * echo 1 > /sys/class/backlight/rpi_backlight/bl_power

    but if you want it to turn off at 6 PM you'd use:

    30 18 * * * echo 1 > /sys/class/backlight/rpi_backlight/bl_power

     

    I'd also check that your TZ environment variable is working properly - in the resin.io terminal for your frame, type 'date' (no quotes), hit enter and check that you get your correct local time. Oh, and I'm not sure why it wouldn't be, but check cron is actually running, with the command:

    systemctl status cron

    It should show up as 'active (running)'.

     

    If cron is running, and both the cron job and the timezone are set correctly, and it's still not working properly, I'm afraid that I'm out of ideas, and if no one else here can help you, your best option is probably to reflash your SD card and start again, just in case something messed up the first time around. I hope you get to the bottom of it!

     

    Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • salmanslim
    salmanslim over 8 years ago in reply to bishely

    Thank you Tom , i have made the following changes to reflect the on off feature.

     

    # Turn off display every evening @ 11PM

    0 23 * * * echo 1 > /sys/class/backlight/rpi_backlight/bl_power

    # Turn on display every morning @ 8AM

    0 8 * * * echo 0 > /sys/class/backlight/rpi_backlight/bl_power

     

    Under resin io dashboard ENV variables TZ is set to America/Los_Angeles but jobs.txt is not turning on and off the display. i have rebooted and checked my settings once again and they are all correct. i tested this out by changing turn off display to

    30 6 * * * echo 1 > /sys/class/backlight/rpi_backlight/bl_power

    i have also verified the settings in crontab -l

    but it kept running. Do you if i am missing anything?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bishely
    bishely over 8 years ago in reply to salmanslim

    There's a few things going wrong there - as far as I know (I'm no expert) cron always and only uses the local timezone, so you can't specify a time zone on your cron jobs.

     

    On an ordinary Linux OS, you'd probably need to explore your locale settings, but with this project, you should be able to login to resin.io, open your connected frame project, click Env Vars (environment variables) and add (or edit) a variable with the name TZ and the value of your locale/timezone (I'm not sure what your setting should be, but if it helps, mine is 'Europe/London' without quotes).

     

    Once you've set your timezone, your cron jobs should be a little less confusing to setup. That said, cron can still be slightly counterintuitive if you've not used it before, so I'd recommend using crontab.guru to help make sure your timings are set the way you want them to be.

     

    Lastly, check that your rules do what you want them to do. For instance, if you wanted to set the backlight brightness to 40 at 5am every day, your rule should look like:

     

    0 5 * * * echo 40 > /sys/class/backlight/rpi_backlight/brightness

     

    Hope that's enough for you to figure out the rest yourself!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>