Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog RPi Haunted Foginator turned to RPi Haunted Halloween.  :-)
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jkutzsch
  • Date Created: 2 Nov 2015 3:20 AM Date Created
  • Views 1165 views
  • Likes 3 likes
  • Comments 3 comments
  • raspberry_pi_projects
  • pumpkinpi2015
Related
Recommended

RPi Haunted Foginator turned to RPi Haunted Halloween.  :-)

jkutzsch
jkutzsch
2 Nov 2015

image

Wrap up time!

 

Sadly after cleaning, and testing and checking everything with my old foginator, it started having intermittent problems.  Sometimes it would work, sometimes, nothing.

Not having enough time to get a new one I changed over the idea of a relay just for firing the Foginator and built an outlet Relay inside a 4 gang box similar to https://youtu.be/8cPK8lh6oLI , I had seen this video while waiting for parts and liked the idea of being able to remotely power the relay as well as having the PIR sensor flip the relay.  Plus being able to use the box to wrap everything up inside was a nice tie in.

 

Hating the idea of the Foginator not being consistent I set up 2 masked heads capable of movement, 2 masked heads static, and a cool Electric Plasma Glass Skull head.

All 4 masked heads are illuminated from within by solar led and one is lit from below by modified solar led that I swapped a UV led into.

The 2 moving heads are provided mobility by taking oscillating fans and attaching the heads to the top with drop cloths on the front to billow when the fan spins up and the head unit moves.  Side note, this drop cloth was not UV reflective, next year test before assuming.  :-)

 

As you can see in the above picture Static is pretty cool, but in the bottom video the creepiness went WAY up as the PIR was activated and things started moving!

 

 

 

I have to admit I had been working on this guy for a bit before adding it into the RPi display.  Had to keep busy while waiting for parts and pieces to come in!

 

imageimage

This was going to be a static display with the coolness to be how the recessed eyes are glowing and will "follow" you as you move past.  But after a bit of creative thought the idea of working it on a standing oscillating fan seemed to be even more creepy since it would only move when the PIR sensor was activated it.  The billowing plastic below and UV led were extra steps to the overall feel.

 

imageimage

 

This head was based on a glow in the dark trick or treat pail and was illuminated by a Solar LED from the top and unseen in these pictures a Solar UV LED underneath.  The pail did not illuminate near as well as the balloons I tried on the others.  But it was helpful for me to be able to put in the recessed eyes for the "following".

 

image

 

Once I decided to move forward with the full display I thought having a couple of non-moving simple heads would be nice.  These are on white balloons illuminated from within by solar LEDs so always lit when dark.

 

image

 

This was the second moving head, Not as complex as the other but still with enough creepy to it that my little ones didn't want to go near the "trolls".  :-)

Also based on a white balloon, illuminated from within by Solar LED.  The wire was needed to keep it to the fan and was not obvious from farther away.

 

image

 

Plasma skull!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Final implementation in Video Format!

 

This was an awesome project to work on and I want to give a huge THANK YOU to Element14 for letting me participate!

 

Very eager to do more, and can't wait to see how everyone else did with their projects.  The element of limited timeline helped the creative process!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Nice build. I would have gone with red eyes for the masks, but that is just me. Scary on its own though. How did the kids react when they saw it? DAB
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    Scary and well included in the entire scenography
  • jkutzsch
    jkutzsch over 10 years ago in reply to DAB

    The blue eyes were from the basic mask I saw implemented.  They used just a standard face mask and it made it appear pretty human.  But after I did all of the eye work I couldn't find a standard face mask, but the Dollar store had these cool Space Masks that I went with.  The cloth for the head, the balloons, the pail, the solar lights all from the Dollar store so it made it easy to put together.  :-)  The eye itself is made from an egg carton, with glow in the dark paint for the whites.

     

    The kids loved it!  My little kids kept clear of the area.  The downside is that someone loved it so much that when I took the kids out for a Halloween Party someone swiped most of it.  I didn't think anyone would be so bold that early with so many people walking around but now I know.

     

    It was a great learning experience!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago

    Scary and well included in the entire scenography

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Nice build.

     

    I would have gone with red eyes for the masks, but that is just me.

     

    Scary on its own though.  How did the kids react when they saw it?

     

    DAB