Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Setting up the system
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: pvalyk
  • Date Created: 15 Oct 2015 8:54 AM Date Created
  • Views 1189 views
  • Likes 1 like
  • Comments 3 comments
  • geocaching
  • geocache
  • rasberry
  • raspberry_pi_2_kit
  • gps
  • raspberry_pi_geocaching
  • microstack
  • raspberry_pi_projects
Related
Recommended

Setting up the system

pvalyk
pvalyk
15 Oct 2015

     First off, let say thanks for being part of this project. Sorry for the late post.

     A couple of weeks ago I started assembling my project. For starters I choose to setup just the GPS module. The LCD display will come after. I put the system on my fridge, right near the wifi router.

 

image

     When I first booted into latest version of Raspbian I ran the Configuration menu . In Advanced Options>Serial  set disable serial. I rebooted, and the ran:

image

sudo apt-get update && sudo apt-get upgrade


     and

image

sudo apt-get install python3-microstacknode

 

     and

 sudo apt-get install gpsd gpsd-clients python-gps

image

     Then I comment out the following line in /etc/inittab by putting # in front of it so that it goes from this:

#T0:23:respawn:/sbin/getty -L ttyAMA0 115200 vt100

 

     And remove all references to ttyAMA0 in /boot/cmdline.txt so that it goes from this:

 

dwc_otg.lpm_enable=0 console=ttyAMA0,115200 console=tty1 root=/dev/mmcblk0p2

 

     I removed console = tty1 too.

     Now I configured GPSD:

 sudo dpkg-reconfigure gpsd

 

     -Choose Yes for automatically start gpsd.

     -Choose No for “should gpsd handle attached USB GPS receivers automatically”

     -Enter /dev/ttyAMA0 when asked “Device the GPS receiver is attached to”

     -Choose default for the other options.

sudo poweroff

 

     I unplugged the Raspberry Pi and attached the GPS module.

     My first mistake was that I replaced the GPS antenna with a wifi antenna or did not attached an antenna at all. That didn’t got any fix on satellite.

     I attached the antenna from the kit and got gps location.

     Now I ran

sudo gpsd /dev/ttyAMA0 -F /var/run/gpsd.sock

     and

cgps –s

 

     and got the latitude and longitude of my location.

 

     Use this as a great resource:

     https://github.com/microstack-IoT/python3-microstacknode

 

     To follow: load saved locations and display on the screen. I got a problem with module's switch. It came broken. Any Ideas?

image

  • Sign in to reply

Top Comments

  • gadget.iom
    gadget.iom over 10 years ago +1
    Good start. Which module has lost the switch, and what is the switches function?
  • gadget.iom
    gadget.iom over 10 years ago in reply to pvalyk +1
    It looks like an SMD device. Might be possible to hand-solder it back on. Are the pads intact?
  • gadget.iom
    gadget.iom over 10 years ago in reply to pvalyk

    It looks like an SMD device. Might be possible to hand-solder it back on. Are the pads intact?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • pvalyk
    pvalyk over 10 years ago

    PiFace's 3-position navigation switch. It's in the last picture. I tried to put it back and tighten it but it keeps falling.

    I haven't found any use for it so perhaps it's not important for this project.

     

    Also, i found this link for customizing the characters on the display.

     

    PiFace – Custom character on PiFace Control And Display – Generating custom characters

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago

    Good start. image

    Which module has lost the switch, and what is the switches function?