Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Trick or Trivia Halloween Candy Dispenser #002 - Building The Trivia Interface
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: CharlesGantt
  • Date Created: 15 Sep 2015 8:09 AM Date Created
  • Views 1722 views
  • Likes 6 likes
  • Comments 4 comments
  • pi2candydispenser
  • raspberry
  • python
  • halloween
  • touch
  • pi
  • trivia
  • trick
  • 2
  • tkinter
  • screen
  • raspberry_pi_projects
  • or
Related
Recommended

Trick or Trivia Halloween Candy Dispenser #002 - Building The Trivia Interface

CharlesGantt
CharlesGantt
15 Sep 2015

image

 

Hello everyone! It’s been a week and I have been working hard at designing and writing the trivia interface for this project, and I am proud to say that after an absence of more than five years from Python, I was successful in getting a decent looking GUI built. Unfortunately I have yet to figure out how I will be randomizing the questions that the device ask trick-or-treaters, but that is something I can work on later in the project. So let’s jump in and take a look at how I created the trivia interface.

 

In my first post, I mentioned that I had planned on using the Drupal CMS to build the trivia interface. After some conversation with another Drupal developer, I came to the conclusion that using a PHP-based framework and building a database was way overkill when I wanted to just display a few questions on a screen. So I decided to just write the whole trivia interface in Python, a language I have not touched in more than five years. Unfortunately my entire Python experience was in the command line, and I had never tried writing a GUI before.

 

image

 

After some research I found out that it is extremely easy to create a simple, low-level user interface in Python by using a GUI library named Tkinter. For those of you who have never heard of Tkinter (like me), it’s Python's de-facto standard GUI (Graphical User Interface) package. It is a thin object-oriented layer on top of Tcl/Tk. Using Tkinter I was easily able to create a nice full-screen application that would clearly present the question and its answer buttons to the user.

 

 

Installing The Raspberry Pi 7-InchTouch Screen

 

 

image

Before I show you the interface and the code that created it, let’s take a look at what we will be displaying the code on. Element14 sent me the brand new Raspberry Pi 7-inch touch-screen LCDRaspberry Pi 7-inch touch-screen LCD to use in this project, and after spending a couple of weeks with this screen, all I can say is WOW. I have used several different screens with the Raspberry PiRaspberry Pi, and Beaglebone BlackBeaglebone Black boards, and none has been as easy as this screen was to use.

 

 

image

Getting the Raspberry Pi 7-inch Touch Screen up and running is as simple as connecting the large ribbon cable to the back of the driver board, and then securing the driver board to the screen with the provided hardware.

 

 

image

With the driver board mounted to the LCD screen, connect the smaller ribbon cable to the driver board. I found it was easier to do it this way since I have larger fingers.

 

 

image

With thetwo LCD ribbon cables connected, mount the Raspberry Pi to the stand-offs, and then connect the DSI cable to both boards.

 

 

image

Now connect the two power jumper wires to both boards as shown in the above image. You will also want to insert the SD card into the Raspberry Pi. If you are running the latest version of raspbian, you can now plug a 5V 2A power source into the LCD screen’s driver board. If you do not have a 5V 2A power source, you can remove the power wires that connect the two boards, and then connect a single 5V 1A power source to the Raspberry Pi and One to the LCD screen’s driver board.

 

You will have to connect your Raspberry Pi to video source via the HDMI port for this process, or SSH into the Pi if you know it’s IP address. If you are using the NOOBs SD card that comes with the kit for this tutorial, you will have to update to the latest Raspbian, as the one installed on it is out of date.

 

To see which version of Raspbian your Pi is running, use the following command in the terminal:

 

uname -a

 

Which should return something that looks like this.

 

 

Linux raspberrypi 4.1.6-v7+ #810 SMP PREEMPT Tue Aug 18 15:32:12 BST 2015 armv7l GNU/Linux

 

 

If your version of Raspbian is out of date, run the following commands in the terminal:

 

sudo apt-get update

 

Then

 

sudo apt-get upgrade -y

 

 

With the update and upgrades ran, you can now restart your Raspberry Pi, and the LCD screen should now work and display the login screen.

 

image

 

 

Enter the desktop GUI by typing the following command after logging in.

 

startx

 

 

 

 

image

 

Now that you are on the desktop, let’s look at how I built the trivia GUI.

 

 

GUI Build UsingTkinter

 

image

As I mentioned above, I decided to write my own GUI instead of using a heavy framework like Drupal to create a simple quiz interface. I looked at a few options and finally decided on a GUI solution that was already built into Python called Tkinter. I chose this because it was very lightweight which would save loading times, and because it seemed very simple to use.

 

The Knowledge

 

One of the biggest sellers for me on Tkinter was the sheer amount of documentation that is available online. New Mexico Tech has a great Tkinter reference on their website which was very helpful when troubleshooting, but the best resource I found was a series of Videos on YouTube from a user named TheNewBoston. I would highly recommend heading to his channel and watching his tutorial series on using Tkinter.

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

TheNewBoston's first Tkinter Tutorial

 

 

I ended up watching the entire series, but if you only have time to watch a few, everything up to video six will give you the knowledge needed to complete this project. Watch the videos if you are following along at home, and check out my code below which I have broken out to better explain what each section does.

 

The Code

 

We need to import Tkinter, the Raspberry Pi GPIO as GPIO, Time, and system libraries.

 

from Tkinter import *
import RPi.GPIO as GPIO
import time
import sys
                              

 

 

Here we set up the GPIO pins. For the purpose of this tutorial I turn GPIO warnings to off. Then we need to set the GPIO Pinout to the BCM layout. Finally we need to define two output pins that will turn on a pair of LEDs.

 

GPIO.setwarnings(False)
GPIO.setmode(GPIO.BCM)
GPIO.setup(26, GPIO.OUT)
GPIO.setup(19, GPIO.OUT)
                              

 

 

For those of you who do not know, the Raspberry PI’s GPIO sins can be configured two different ways, GPIO.board and GPIO.bcm.  When setting the GPIO pins mode, you are telling it what numbering scheme your code will be adhering too. Unfortunately the pin numbering between each of the different modes changes on various models and revisions of the Raspberry PI. So if you are not running a Model B+ or Raspberry Pi 2, you will need to search the internet for the proper pinouts for the mode you select.

 

  • The GPIO.BOARD option specifies that you are referring to the pins by the number of the pin the the plug - i.e the numbers printed on the board (e.g. P1) and in the middle of the diagram below.
  • The GPIO.BCM option means that you are referring to the pins by the "Broadcom SOC channel" number, these are the numbers after "GPIO" in the green rectangles around the outside of the diagram below.

image

Raspberry Pi B+ and Raspberry Pi 2 GPIO Pinout.

 

 

We need to set the state to True

 

state = True
                           

 

 

This section defines a function called blink_led. At the end of this script I add a sys.exit line that is executed three seconds after I turn off the GPIO pin for the last time. This exits out of the quiz script, allowing us to reset for the next trick-or-treater.

 

def blink_led():
# endless loop, on/off for 1 second
    while True:
        GPIO.output(26,True)
        time.sleep(1)
        GPIO.output(26,False)
        time.sleep(1)
        GPIO.output(26,True)
        time.sleep(1)
        GPIO.output(26,False)
        time.sleep(1)
        GPIO.output(26,True)
        time.sleep(1)
        GPIO.output(26,False)
        time.sleep(1)
        GPIO.cleanup()
        time.sleep(3)
        sys.exit()
                           

 

 

This section sets up another function that blinks the same pattern, but this time we name the function blink_led_2.

 

def blink_led_2():
# endless loop, on/off for 1 second
    while True:
        GPIO.output(19, True)
        time.sleep(1)
        GPIO.output(19, False)
        time.sleep(1)
        GPIO.output(19, True)
        time.sleep(1)
        GPIO.output(19, False)
        time.sleep(1)
        GPIO.output(19, True)
        time.sleep(1)
        GPIO.output(19, False)
        time.sleep(1)
        GPIO.cleanup()
        time.sleep(3)
        sys.exit()
                           

 

 

Now we need to set up Tkinter. The first thing we need to do is set up a basic box that will hold the elements of our GUI. We do this by telling the program that root=Tk().

 

root = Tk()
                           

 

 

Now we need to set the window to not have a border, title, or any of the normal minimize, maximize, and close buttons.

 

root.overrideredirect(True)
                           

 

 

This line tells the program to set the window to full screen and auto size it to the screens resolution.

 

root.geometry("{0}x{1}+0+0".format(root.winfo_screenwidth(), root.winfo_screenheight()))
                           

 

 

Now we need to tell the program to set the focused window to this one.

 

root.focus_set()
                           

 

 

We also need to set the window’s background to black.

 

root.configure(background='black')
                           

 

 

With the basic GUI window setup we can move on to setting up the elements that will appear in the z. This consist of three labels on top that span three rows of a grid, followed by two answer buttons on the next row spaced apart by two columns, and another row with two buttons and the same spacing below it. Finally we need to add two more labels to the bottom that describe what the rewards are for correct and incorrect answers. You will see that I have styled the elements inline with basic styling options, and placed the elements using Tkinter's .grid Geometry Manager.

 

 

Setting up the Labels.

 

 

In each of these three labels you can see that I have placed them in the root box, and included font, font size, background color, and foreground color attributes. and the set each of the labels to display using the .grid method followed by some placement style and padding attributes.

 

 

label_1 = Label(root, text="Welcome to Trick or Trivia", font=("Helvetica", 36), bg="black", fg="white")
label_1.grid(columnspan=6,padx=(100, 10))
label_2 = Label(root, text="Answer the question for candy!", font=("Helvetica", 28), bg="black", fg="red")
label_2.grid(columnspan=6, pady=5, padx=(100, 10))
label_3 = Label(root, text="Casper is a friendly ____!", font=("Helvetica", 32), bg="black", fg="green")
label_3.grid(columnspan=6, pady=5, padx=(100, 10))
                           

 

 

Setting up the Buttons

 

Just like the Label elements, I defined the buttons by placing them into the root window, adding text, and including attributes for font type and font size. Here is a reference (http://effbot.org/tkinterbook/button.htm). What makes the buttons special is the “command” attribute I included at the end of the button setup line. This calls the function it names, which in our case is one of the two blink_led functions we wrote earlier. Finally I displayed the button using the .grid method with some styling attributes.

 

button_1 = Button(root, text="Ghost", font=("Helvetica", 36), command=blink_led)
button_1.grid(row=4, column=2, pady=5, padx=(100, 10))
button_2 = Button(root, text="Ghast", font=("Helvetica", 36), command=blink_led_2)
button_2.grid(row=4, column=4, sticky=W, padx=(100, 10))
button_3 = Button(root, text="Ghoul", font=("Helvetica", 36), command=blink_led_2)
button_3.grid(row=5, column=2, pady=5, padx=(100, 10))
button_4 = Button(root, text="Gremlin", font=("Helvetica", 36), command=blink_led_2)
button_4.grid(row=5, column=4, sticky=W, padx=(100, 10))
                           

 

 

Finally I added two more labels with the same styling and placement attributes as before.

 

label_4 = Label(root, text="Correct Answer = 3 Pieces", font=("Helvetica", 20), bg="black", fg="green")
label_4.grid(columnspan=6, padx=(100, 10))
label_5 = Label(root, text="Incorrect Answer = 1 Piece", font=("Helvetica", 20), bg="black", fg="red")
label_5.grid(columnspan=6, padx=(100, 10))
                           

 

 

Finally we need to tell the program to stay in the event loop until we close the window.

 

root.mainloop()
                           

 

 

Putting It All Together

 

Here is what the code looks like as a whole. You can download this code from my Github repo for this project or by clicking here.

 

 

from Tkinter import *
import RPi.GPIO as GPIO
import time
import sys


GPIO.setwarnings(False)
GPIO.setmode(GPIO.BCM)
GPIO.setup(26, GPIO.OUT)
GPIO.setup(19, GPIO.OUT)


state = True


def blink_led():
# endless loop, on/off for 1 second
    while True:
        GPIO.output(26,True)
        time.sleep(1)
        GPIO.output(26,False)
        time.sleep(1)
        GPIO.output(26,True)
        time.sleep(1)
        GPIO.output(26,False)
        time.sleep(1)
        GPIO.output(26,True)
        time.sleep(1)
        GPIO.output(26,False)
        time.sleep(1)
        GPIO.cleanup()
        time.sleep(3)
        sys.exit()


def blink_led_2():
# endless loop, on/off for 1 second
    while True:
        GPIO.output(19, True)
        time.sleep(1)
        GPIO.output(19, False)
        time.sleep(1)
        GPIO.output(19, True)
        time.sleep(1)
        GPIO.output(19, False)
        time.sleep(1)
        GPIO.output(19, True)
        time.sleep(1)
        GPIO.output(19, False)
        time.sleep(1)
        GPIO.cleanup()
        time.sleep(3)
        sys.exit()


root = Tk()
root.overrideredirect(True)
root.geometry("{0}x{1}+0+0".format(root.winfo_screenwidth(), root.winfo_screenheight()))
root.focus_set()  # <-- move focus to this widget
root.configure(background='black')
root.config(cursor="none")


label_1 = Label(root, text="Welcome to Trick or Trivia", font=("Helvetica", 36), bg="black", fg="white")
label_1.grid(columnspan=6,padx=(100, 10))
label_2 = Label(root, text="Answer the question for candy!", font=("Helvetica", 28), bg="black", fg="red")
label_2.grid(columnspan=6, pady=5, padx=(100, 10))


label_3 = Label(root, text="Casper is a friendly ____!", font=("Helvetica", 32), bg="black", fg="green")
label_3.grid(columnspan=6, pady=5, padx=(100, 10))


button_1 = Button(root, text="Ghost", font=("Helvetica", 36), command=blink_led)
button_1.grid(row=4, column=2, pady=5, padx=(100, 10))


button_2 = Button(root, text="Ghast", font=("Helvetica", 36), command=blink_led_2)
button_2.grid(row=4, column=4, sticky=W, padx=(100, 10))


button_3 = Button(root, text="Ghoul", font=("Helvetica", 36), command=blink_led_2)
button_3.grid(row=5, column=2, pady=5, padx=(100, 10))


button_4 = Button(root, text="Gremlin", font=("Helvetica", 36), command=blink_led_2)
button_4.grid(row=5, column=4, sticky=W, padx=(100, 10))


label_4 = Label(root, text="Correct Answer = 3 Pieces", font=("Helvetica", 20), bg="black", fg="green")
label_4.grid(columnspan=6, padx=(100, 10))


label_5 = Label(root, text="Incorrect Answer = 1 Piece", font=("Helvetica", 20), bg="black", fg="red")
label_5.grid(columnspan=6, padx=(100, 10))




root.mainloop()
                           

 

Copy and paste this code into a new file on your Raspberry Pi’s desktop, or from the command line enter the following commands.

 

cd Desktop

sudo nano TrickorTriviaQuiz.py

 

 

 

 

Then right click to paste the copied code into the new file, and exit nano.

 

 

Setting up the LEDs

 

image

 

Follow the diagram above and wire up your LEDs to GPIO pins 19 and 26 . Since the Pi’s GPIO pins output a 3.3v signal, you do not need resistors if you are using a single red, green LEDs.

 

 

Running the program

 

image

 

Now from the desktop, open the terminal (if you were not in the GUI or pasting the code remotely. With the terminal open, navigate to the desktop directory and enter the following command to run your new quiz program.

 

sudo nano TrickorTrivia.py

 

The trivia screen should pop up like in the video below. If you select a correct answer, then the green LED will illuminate and flash three times. If an incorrect answer is selected, then the red LED will illuminate and flash three times.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The LEDs used in this tutorial are just for troubleshooting purposes, and are not part of the kit. You can use any LEDs you have laying around, or two of the red 10mm LEDs included in the kit. In a future update, I will show you how to write a function that rotates a servo via the GPIO pins and we will replace the blink_led calls with this. For now this proves that the quiz script works, and that we are okay moving forward with the next step in the project. Check back next week for another update, and until then, Hack the World and Make Awesome!

 

 

Win this Kit and Build-A-Long

 

  1. Project Introduction

  2. Building The Trivia Interface

  3. Interfacing Ambient and Triggered Audio Events
  4. Building The Candy Dispenser & Servo Coding
  5. Carve Foam Tombstone
  6. October 24th -  Assembly and Testing
  7. October 28th - Project Wrap-up
  • Sign in to reply
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to CharlesGantt

    Hi Charles,

     

    you can not start a Tkinter script without starting it on the machine that is running the script directly

    Sorry, I am not sure I have understood what do you mean image


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • CharlesGantt
    CharlesGantt over 10 years ago in reply to cmelement14

    Yes, you can not start a Tkinter script without starting it on the machine that is running the script directly. You also have to be within a GUI

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cmelement14
    cmelement14 over 10 years ago

    Hi Charles,

     

    First of all, thank you very much for this great series of blogs. I am following this blog, but a few things came up:

    1. GPIO.setup(26, GPIO.OUT) statement failed if I don't start Python with root privilege. I have to start Python interpreter using sudo python

    2. If I started python in privilege, root=Tk() statement would fail. Therefore, I cannot successfully run the whole TrickorTriviaQuiz.py with or without privileged Python interpreter.

    3. The command run quiz program should not be sudo nano TrickorTrivia.py, instead, it should be python TrickorTriviaQuiz.py


    I have to mention that I am doing things a little bit different. Since I don't have keyboard to connect Pi directly, so I am using VNC remote desktop. Could this be the reason giving me troubles?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Very interesting Blog.

     

    I like the 7 inch display and your UI for the trivia questions.

     

    Nice simple and clean design.

     

    DAB