Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog What's a PiJack?
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rctho
  • Date Created: 21 Nov 2017 9:21 PM Date Created
  • Views 4302 views
  • Likes 9 likes
  • Comments 15 comments
  • rpiintermediate
  • raspberry_pi_projects
Related
Recommended

What's a PiJack?

rctho
rctho
21 Nov 2017

I needed to extend the wifi range of my router with a minimal footprint in my apt. I didn't want more peripherals plugged in all over my apt. I used a RPi0w for the wifi repeater and jammed it into a two gang receptacle box. Two usb ports (one is for console connection) and kill switch, or reset button in case the computer hangs. The console connection will also power the Pi in case the power goes out.

 

image

First i had to attach the antenna. I found tutorials online that looked easy enough at first but the pics were scaled about 1000% of the pi's actual size. When i looked at the board and the size of the components i had to re-solder on, i was quickly discouraged. It doesn't look the greatest, but it got it done and it works. That's what matters.

 

image

 

Next i cut all the cords to size then soldered on the usb, micro usb, and pinout thingy. I used shrink tube and hot glue so that no wires are exposed. I used the internal circuit from a standard 5v transformer/ regulator commonly used to recharge a cell phone to hardwire the pi to my apt. it will act the same as if i plugged it in.

 

image

I used Leviton Qickports for the wall plate. two ports i drilled holes in for both the external antenna and reset button. Got all my components together. Time to assemble.

 

image

The transformer/regulator fit in perfect. All of the pre soldering was done so at this point, it was pretty much plug and play. I taped the pi to the side, then connected all the components.

 

image

Got it all in there. Easy street!

 

image

image

 

I had to disable the bluetooth to use the uart console gpio pins. console, usb, antenna, and reset switch all work great. I'm now configuring the wifi repeater. I'm going to make sure everything works before i put it in the wall.

 

Other than a wifi repeater, this device doesn't have much purpose. I could connect a usb camera, or I could swap out the usb for hdmi to connect it to a tv.. i wanted to make it more than i knew what i would do with it. Does anyone have any suggestions for what else this can be used for?

  • Sign in to reply

Top Comments

  • rachaelp
    rachaelp over 8 years ago +3
    Nice first blog post Craig! Keep practicing with soldering the tiny components and you’ll get the hang of it. Get a decent soldering station, tweezers, solder, flux, solder wick etc and a reasonable illuminated…
  • ninjatrent
    ninjatrent over 8 years ago in reply to rctho +3
    Hi Craig, Really great post! Thanks for sharing it with the community. The Pi Zero W seems like it would be a good candidate for Onion Pi router. Thanks again. It is a very inspiring project. Trent
  • rctho
    rctho over 8 years ago in reply to ninjatrent +2
    Hi Trent, I followed this tutorial: Raspberry Pi Zero W external antenna mod | BrianDorey.com I bypassed the onboard antenna to the external antenna connection pad on the board. To my knowledge, the external…
  • ninjatrent
    ninjatrent over 8 years ago in reply to rctho

    Hi Craig,

     

    Try listening to music that you enjoy when you are soldering.

    Also try resting your elbow and forearm on the bench while soldering.

    Try not to do any work with your arms before you solder.

    Relax and enjoy. Soldering is fun.

     

     

    Trent

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rctho
    rctho over 8 years ago in reply to ninjatrent

    Thanks Trent. Sure np. Onion Pi router is a good idea. With a nice lil' battery pack for mobility.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rctho
    rctho over 8 years ago in reply to rachaelp

    Thanks Rachel. I have access to everything you mentioned. flux is amazing when soldering but unfortunately is always out because of it. It's my shaky hands though image I'll keep at it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago in reply to rachaelp

    Would like to add adequate ventilation to your excellent list of soldering equipment.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago in reply to rctho

    Hi Craig,

     

    Really great post!

     

    Thanks for sharing it with the community. 

     

    The Pi Zero W seems like it would be a good candidate for Onion Pi router.

     

    Thanks again. It is a very inspiring project.

     

    Trent

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>