Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents New Pi Camera and Pi Camera NoIR V2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 21 Apr 2016 1:23 PM Date Created
  • Last Updated Last Updated: 10 May 2021 8:50 PM
  • Views 8780 views
  • Likes 12 likes
  • Comments 18 comments
Related
Recommended

New Pi Camera and Pi Camera NoIR V2

Given that the Raspberry Pi 3 is now probably firmly in your hands, and in your projects, the timing is spot on for an update to some of its accessories, and today we're happy to announce that the Pi Camera V2 and Pi Camera NoIR V2 are yours to buy.

 

New Look

image

First, of course, you'll be wanting to know what's changed in Pi Camera V2.

 

I don't mind openly admitting that the update is an incremental one, because I'm already a big fan of the original Pi Camera. Apologies for resorting to a cliche here, but I'm a big believer that if it ain't broke, don't fix it, and Pi Camera V2 upholds that valuable adage admirably.

 

There are some changes, of course, primarily in its CCD resolution. Both models now boast an 8 megapixel Sony IMX219 CCD (as opposed to its predecessor's 5 megapixels), and there's a new lens in place to beam a crystal-clear image onto it. From this you can expect the following resolutions:

  • Photos up to 3280 px by 2464 px.
  • Video at 1080p at 30fps; 720p at 60 fps; and 640 by 480p at 90 fps, offering a bit of slow-mo fun.

 

As before, the NoIR version of the Pi Camera dispenses with the infra-red filter, giving you a great response in low light applications. Between the two, you've got all bases covered when it comes to a video solution for the Raspberry Pi. And it's worth noting that these V2 cameras are also backwards compatible, should you want to swap out a Pi Camera on an existing project or use an older model of Raspberry Pi. Just make sure you're version of Raspbian is up to date.

 

And that's the basics of the Pi Camera V2 done and dusted. Nice and simple, eh?

 

Pi Camera V2Pi Camera NoIR V2

image

BUY NOW

image

BUY NOW

 

Eyeballs on New Projects

As with any new product launch, the first thing I want to know about (even before the product's specs, if I'm honest!) is about the project ideas that immediately come to mind for you guys when you see them.image

 

As we've already discussed, the Pi Camera V2 is a product improvement as much as a complete revamp, but I've no doubt that you have projects that could use enhanced detail, extra image clarity or improved night vision, so tell us all about them in the comments section below. The project idea that gets the most likes by the end of the week (Friday 29th) can have the two product samples that are sat on my desk (one of each camera model).

 

So be generous and fair as you read through each other's ideas, and let's see if we can come up with some cunning new ways to put eyeballs on a Pi!

  • pi camera noir v2
  • pi camera v2
  • pi camera project
  • raspberry_pi
  • pi noir
  • raspberry pi accessories
  • pi camera
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • clem57
    clem57 over 10 years ago +3
    I live near a creek with more activity at night rather than the day (except for the humans of course). If I had the NOIR, I could capture the animal life at night and see the other side of the non sleeping…
  • e14 Contributor
    e14 Contributor over 10 years ago +3
    Hi, My name is Alyssa from Quebec Canada, I team with my fhather to realize a scool projet to participate in scence fair ( http://exposciencess.qc.ca ). my gool is to compare twoo technologies, I want…
  • jwatson
    jwatson over 10 years ago +2
    Hi Everyone Enter our Pi@Night Photography Competition! For 2 weeks only! Get snapping for your chance to win a Raspberry Pi 3 Camera Bundle Kit including the NEW Raspberry Pi Camera v2 launched today…
  • e14 Contributor
    e14 Contributor over 10 years ago

    I am working on the design of a Wireless Sensor Network-based water quality monitoring system to be deployed in Ghana, Africa, where a large percentage of the population does not have access to safe drinking water, and hence suffers from frequent occurrences of water-borne diseases. The system will be comprised of several wireless sensor nodes (to collect water parameters such as dissolved oxygen, oxidation-reduction potential, pH, conductivity, and temperature), a base station, and a remote monitoring center. I am experimenting with different low cost devices and, among others, I am considering to use a Raspberry Pi. Adding the Pi Camera would allow to get real time access to the monitoring site thus adding an additional level of security to the system, and potentially prevent acts of vandalism. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oliverhbailey
    oliverhbailey over 10 years ago

    I've started working with a group of visually impaired people who would like to be able to enjoy target practice. The camera would be mounted on a scope and broadcast via WiFi to a tablet for focus and adjustment.

    It would be detachable so it can be used to communicate via the Internet by using a braille keyboard and text to voice. A visually impaired type of Skype.

     

    These are people who have been legally blind for 20+ years but all had perfect sight at one time. They are so excited and fun to work with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    A TV/Display Calibrator

     

    I would like to see a project where we could use the camera and Pi to do calibration of TV's and Monitors. Typically it takes a fairly expense photometer and software (I like the open source HCFR software).

    Using this camera and the fact that the Pi has an HDMI port would make this doable. Here is an overview:

     

    1) Store the various screen patterns (10 step grey scale and primary/secondary colors) as jpg's on the Pi. These calibrated patterns are available from a variety of sources.

    2) Initial scan. Place the camera as close to the screen as possible.

         Have the Pi display each pattern and then take a reading using the Sony camera. All done automatically.

    3) Show the results and also what the target readings should be. Likely there will need to be some tuning done. If so...

    4) Perform tuning/calibration

         Pi outputs each pattern, step by step with user control, and reads the screen/display. It shows the R G B values it is reading, updating every second or so. Using controls for your monitor/TV, adjust settings while watching the updates and try to get close to the target.

         When each step is done, advance to the next. Each of the 10 Grey Scales and each of the 5 Primary/Seconday colors

    5) Perform a post-calibrate scan and show the new results

     

    The Pi could be controlled over ssh or possible over Wifi. Another challenge is the accuracy of the Sony camera. I would be willing to run a comparison against a know calibration device (I have an Xrite i1D3) and supply a correction matrix. Granted, this should/could be done for each Sony camera, but I would think a correction matrix for one would be close enough for all the cameras.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago

    I live near a creek with more activity at night rather than the day (except for the humans of course). If I had the NOIR, I could capture the animal life at night and see the other side of the non sleeping world at that time. I would use a microphone to sense the animal and snap pictures in the IR range of the heat signature of these nocturnal creatures. If you like this can happen. Thanks.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    I'm working on a multimedia project for Burning Man with a RPi 3 and an RPi 2. The lights and sound coming through can be manipulated by people from the  7" touch screen, while onscreen instructions will guide people though a set of ridiculous but fun instructions on how to get the installation to play music and flash light.

    By using the NoIR camera I will position it to capture video of people completing the instructions at night time, each making their own dance video and I hope to record the elated joy of people enjoying interactive art on the playa in Black Rock Desert Nevada.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    I would like to have the NOIR camera.

     

    I could use it in my spectral microscope to view materials in the IR range.

     

    The full capabilities of the silicon sensor should support imaging from UV, about 400 nm to about 1.2 microns in the IR.

     

    Who knows what I might find.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sjlyons50
    sjlyons50 over 10 years ago

    As a project idea, I'd like to use the new NoIR camera to take pictures through a telescope. If I had a decent computer controlled mount, I'd incorporate the control of it and also focusing, so I can aim, focus and take pictures of the various planets and our Moon while sitting in comfort. I currently have the V1.3 version of the camera, but until this weekend I didn't have a long enough ribbon cable to use it. Now I have a 30cm cable, but the nights have been cloudy! Just need to sort it out with my 7" touchscreen equipped Pi 2 now.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jwatson
    jwatson over 10 years ago
    Hi Everyone
    Enter our Pi@Night Photography Competition! For 2 weeks only!
    Get snapping for your chance to win a Raspberry Pi 3 Camera Bundle Kit including the NEW Raspberry Pi Camera v2 launched today for just £20.75 from farnell.com
    5 lucky members will win fantastic camera bundles & a very special bumper prize bundle for the best photo voted by you - our members!
    Ts & Cs @ https://www.element14.com/community/community/raspberry-pi/raspberry-pi-accessories/blog/2016/04/25/pinight-competition
    Good luck!

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<