RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Converting 5v LCDs to 3.3v and tweaking a MakeCode extension
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: stevesmythe
  • Date Created: 15 Jun 2019 10:58 AM Date Created
  • Views 8972 views
  • Likes 7 likes
  • Comments 12 comments
Related
Recommended
  • micro:bit
  • lcd
  • smd
  • makecode
  • charge pump

Converting 5v LCDs to 3.3v and tweaking a MakeCode extension

stevesmythe
stevesmythe
15 Jun 2019

When I RoadTested the Kitronik Klimate board recently and made a wireless weather station with it, I needed to display four values (temperature, humidity, atmospheric pressure and windspeed) plus some text, on a display.

image

 

As you can see in the photo above, it's hard to fit all the information onto a 16 x 2 display. I knew that a 20 x 4 display would be perfect for this, but there were two problems:

  1. The micro:bit uses 3.3v logic levels but 3.3v 20 x 4 LCD displays are hard to find - and expensive.
  2. I needed to program the micro:bit with Microsoft MakeCode because the Micropython driver for the Klimate board's BME280 completely uses up the limited micro:bit memory space once Micropython is loaded but nobody appears to have written a MakeCode extension for a 20 x 4 LCD display (2004A). However, there is a nice extension for the 16 x 2 LCD (1602A).

 

I decided to see if I could solve both problems.

 

1. Converting 5v LCD to 3.3v

I have previously converted 5v 16 x 2 LCDs to 3.3v, so why not do the same with a 20 x 4 display? I bought a 5v "2004A" display wih I2C backpack from a "favourite online auction site" for about £5. You can buy one without a backpack; I just bought this one because I wanted to use I2C to talk to the micro:bit.

 

image

 

These LCDs (and their 1602A equivalents) have unused pads on them including space for an 8-pin voltage convertor chip. This is designed to allow a 3.3v version of the display to be made by adding a charge pump negative voltage generator to the LCD module.

 

Converting the module to 3.3v is simply a matter of soldering the correct voltage converter chip (ICL7660ICL7660) onto the space provided (U6), plus two 10µF capacitors across pads marked C3 and C4 and a 2.2k Ohm resistor across pad R6.

 

The ICL7660 voltage convertor can be obtained for around £1. From the datasheet, you can see the minimum circuit to provide the necessary voltage reduction.

 

image

 

Finding the correct capacitors in small quantities was a bit more tricky. Unless you have access to some already, you'll probably have to buy 100. HereHere are some suitable ones. Actually, they were slightly too large for this display, but they were perfect for the 1602A LCDs and I had already bought 100, but they just about fitted onto the pads, so I used them anyway. The resistorresistor was a better size for this display and I only had to buy 10.

 

It can be seen that the voltage converter and additional capacitors are surface-mounted. Although they are more fiddly to solder than "through the hole" components, a normal soldering iron is fine (preferably with a fine tip). The technique I used is to melt some solder onto one of the pads for the 7660 chip then, holding the chip down against the pads, apply the soldering iron briefly to the relevant leg of the chip to remelt it and "fix" the chip in position. At this stage it is important to ensure that the chip is correctly aligned with all of the pads. If not, repeat this procedure until it is. Now, the other 7 legs of the chip can be soldered in place by heating each leg in turn and then dabbing the solder onto the leg. Miraculously, the solder will flow onto the pad and over the leg! Once you have soldered all 8 legs, check that there are no "bridges" between adjacent legs. If there are, a quick dab with the soldering iron should sort it out - if not, hold some solder wick between the affected bridge and the soldering iron and that should suck up the excess.

 

image

 

Now use a similar process for each of the capacitors and the resistor; melt some solder onto one of the pads, hold the capacitor in place on top of it, then reapply the soldering iron to melt it into position. Check the alignment, and repeat.

 

image

 

Job done!

 

2. Tweaking the 1602A MakeCode extension to support 20 columns and 4 lines

Microsoft MakeCode extensions for the micro:bit are written in TypeScript (an enhancement to JavaScript). These extensions add MakeCode blocks to support different devices and functions. The "official" extensions can be browsed within the MakeCode online compiler but you can upload your own extensions from a web address (such as GitHub). I had already used the excellent 1602A MakeCode extension for a 16 column, 2 row I2C LCD display and I asked the author if he had written one for the 20 column, 2 row equivalent. He said that he hadn't because he didn't have a device to test it on, so I decided to have a go at tweaking his code myself. It turned out to be remarkably easy. All the TypeScript code is in the file LCD1602_I2C.ts.

 

In the snippet below, I just added a couple of "else if"s to include the correct LCD commands to put the data onto the two extra rows.

 

1602A code

 

export function ShowString(s: string, x: number, y: number): void {
        let a: number

        if (y > 0)
            a = 0xC0
        else
            a = 0x80
        a += x
        cmd(a)

        for (let i = 0; i < s.length; i++) {
            dat(s.charCodeAt(i))
        }
    }

 

2004A code

 

export function ShowString(s: string, x: number, y: number): void {
        let a: number

        if (y > 2)
            a = 0xD4
        else if (y > 1)
            a = 0x94
        else if (y > 0)
            a = 0xC0
        else
            a = 0x80
        a += x
        cmd(a)

        for (let i = 0; i < s.length; i++) {
            dat(s.charCodeAt(i))
        }
    }

 

There were only a handful of other minor changes to the code needed (e.g. to allow data to be put on the display up to column 19 and row 3 (starting from column 0 and row 0)). If you would like to look at the whole code (or indeed use it), you're more than welcome. It's on my GitHub and it works well, but I need to tidy it up, to give it a different name and also to add the image that appears in the simulator (you'll see that it still shows the 16 x 2 version).

 

Here is the result!

 

image

 

image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +3
    Hi Steve, Great info! I've been meaning to do the exact same mod with some 16x2 screens, and purchased the bits but not got around to it yet. Nice to see the mod will work.
  • stevesmythe
    stevesmythe over 7 years ago in reply to shabaz +3
    Thanks Shabaz There is a "jumper" that needs to be moved on the 1602A version that doesn't seem to be the case for the 2004A size. I wrote up the process for the 1602A on my own blog (just before I discovered…
  • neilk
    neilk over 7 years ago +2
    Hi Steve Nice mod to the display board and I like the custom block for MakeCode. Neil
  • hugohu
    hugohu over 5 years ago in reply to svdp

    Thank you for the clarification, Stefan!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • svdp
    svdp over 5 years ago

    Hi Hugo,

     

    I think there is a difference between the blue and the green lcd screens. For the blue LCD's and active pixel is transparent and a background pixel opaque. The back light is seen through the transparent (active)  pixel. For the green LCD it is just the other way around the active pixel is opaque and shows as "black" both require a different contrast voltage. So the points I want to make are:

    -hack does not work for a green display

    -value of R6 is not justified, if you take 0 Ohm its also fine for a blue display

    -no distinction made between display types

     

    Yes, you can you a pot but the proper values for R6/R7 are also handy ;-)

     

    Kind regards,

     

    Stefan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 5 years ago in reply to svdp

    Not quite an expert-

     

    Can't you use a pot? I think that's what you use to control contrast.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • svdp
    svdp over 5 years ago

    Hi Steve,

     

    The patch you suggest does not work for a green display. The reason is quite obvious. The output of the charge pump is connected via voltage R6/R7 to Vo.

    You just take 2.2k for R6 without any reasoning which means that the full -3.3V is on Vo. Which leads to way too much contrast.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    Here are the articles :

     

    https://www.hackster.io/jancumps/hitachi-lcd-driver-example-for-the-hercules-launchpad-7d56f8

     

    https://www.hackster.io/jancumps/rolling-material-monitoring-51b6fc#toc-lcd-display-8

     

    Looking back - I see that I drive the data lines with 3V3, but used 5V for both VDD (contrast) and backlight.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>