RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Keithley 2450  Zener diode test
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: robrenz
  • Date Created: 30 Oct 2013 1:12 PM Date Created
  • Views 2060 views
  • Likes 3 likes
  • Comments 11 comments
Related
Recommended
  • 2450
  • 12v
  • zener
  • vs

Keithley 2450  Zener diode test

robrenz
robrenz
30 Oct 2013

I just had to try out the sweep functionality of the 2450 on a 12V zener.  Very easy to set up and the graph mode is very functional.The pan and zoom is a little slow and seems to have a glitch if you zoom in too far. Still very awesome.

 

As graphed with auto on X and Y axis Y is in linear mode

image

 

As graphed with auto on X and Y axis Y is in Logarithmic mode. Notice Amperage is shown as all positive ??????

image

 

Zoomed on the knee of the Linear Y graph

image

 

Zoomed on the knee of the Logarithmic Y graph

image

 

Zoomed on the forward conduction of the Logarithmic Y graph

image

Time to get back to getting used to this unit and doing the review.

  • Sign in to reply
  • shabaz
    shabaz over 12 years ago

    Hi Rob,

     

    Nice graphs! It is showing an incredible amount of detail. Clearly some very nice analog circuitry in the box. The log one is correct, without having an unusual/ fake y-axis - the easiest way to see this is to notice that as the values get smaller, it would need a very long axis (infinitely long) to reach zero amps.

    When I initially saw the roadtest, I was wondering if the built-in screen could do sufficient justice to the information it could capture, or if it would need to be permanently tethered to a PC. At first glance these screenshots show that the built-in display and graphing routines are highly competent.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<