RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Keysight U1461A Insulation Resistance Meter (part 2)
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: mcb1
  • Date Created: 22 Mar 2015 4:58 AM Date Created
  • Views 2048 views
  • Likes 6 likes
  • Comments 8 comments
Related
Recommended
  • u1461a
  • keysight
  • thermocouple
  • insulation_resistance

Keysight U1461A Insulation Resistance Meter (part 2)

mcb1
mcb1
22 Mar 2015

This is a follow-on from the initial review which can be found here

Software Upgrade

When we were checking the Keysight website documentation, it was noted there was a firmware upgrade available.

As shipped the meter had ver 1.09, and the new version is 3.02.

The changes are here (it's not a lot)

Firmware revision updates:-

 

2015-02-02:

Version 3.02

- Change Identity to Keysight

- Add alert message in EBR and mA

 

Version 1.00

- Initial release version



The software installer was downloaded and installed, and the driver for the USB to serial adaptor installed itself without problems.

The software was unable to find the meter, and checking the Com port showed it only went to 15.


Since my laptop has seen many USB devices, it had allocated port 30.

So for anyone thinking of using the lead, make sure you set the com port to something less that 15.

 

 

 

Port Setting

In Win7 ... Open Control Panel, Hardware and Sound

image

Then click on Device Manager

image

This opens up another window, and select the Ports tree, which should show the USB adapter.

image

Right click on the adapter and choose propertie

image

then select Advanced

image

In the bottom left corner you should have a drop down to select what ports are free.

 

image

 

I simply chose COM9 (port 9) despite it having something else previously using it.

 

 

Software Update process

The software updater checks to see it can see the meter, and verify the version.

image

(version number removed by me)


For some reason while the software was able to read the model, serial number and version, when I clicked on Upload Firmware it brought up a window that said "Meter Disconnected".

Now this was strange as it was showing that it was talking to the meter. image

 

I repowered the meter, disconnected the lead and repeated the process and strangely when I clicked Upload Firmware it worked.



image


          Image of the Firmware Update on both the computer and meter.




What are some of the other features? image

As I eluded in the review, this meter is more than just an Insulation Resistance meter.


Included in the kit are a J Type Thermocouple and K Type thermocouple.

Both are for measuring temperature, and the difference had me wondering.


When I need information I usually resort to either :-


1. The manual (that's usually the paperwork that you left in the box)

2. A little known search engine called Google.


Surprisingly we find many community members are unsure about this Google search thing, but it's very easy to use, and more importantly FREE.


So after checking with Google and a little cutting and pasting I sorted out this chart and information.


image

          source  Thermocouple - Wikipedia, the free encyclopedia


So the answer comes down to a different range and sensitivity.



Adapter

The thermocouples come with a polarised plug where the two pins are different sizes.

This is to ensure they get plugged in the right way around (correct polarity).

HOWEVER the adapter can be plugged in either way around, and worse still you do get a temperature reading.


I sort of missed that when I plugged it in and was wondering why the temperature was 11 deg when it should have been 21 or 22 deg C.


So do pay attention and you'll be rewarded with the right reading.



 

Logging Software

I have another Agilent/Keysight meter I purchased for Logging, and haven't needed to use it ....yet.


It uses the same optical connector which ensures total electrical isolation.

I'm not going to go very deeply into this, as it is secondary to the meter, but is a real benefit.


I logged the temperature as I warmed the thermocouple and it cooled down.

image

While the time on the graph shows as relative, the table view records the actual time based on the PC

 

 

You can elect to view the data as a graph (above) or table, and even as a virtual meter showing the current figure on the meter.

 

image

Once the data is plotted you can zoom in and drag it around, and it's very intuitive.

 

Full data capture below

image

 

Zoomed in section.

image

 

One other very useful feature is the remote control of the settings.

 

In this case it shows where the control knob is set, and allows the choices for that position.

image

 

 

Why bother with temperature? image

The temperature of the device under test can make the difference between a pass or fail.

 

With apologies to Keysight I extracted this explanantion

image

     source http://www.biddlemegger.com/biddle/Stitch-new.pdf

 

 

If the last test you did on a motor was just after it had been running, then it's likely to have a much lower Insulation Resistance than when it's cold.

 

 

What about Dampness? image

Moisture always condenses on surfaces below the dew point.

For those of us who live in more temperate climates, winter tends to damp and cold, rather than dry and cold, and the windows are often the coldest condensing surface.

 

Combine this moisture with dust and dirt, and you suddenly have increased leakage paths and reduced Insulation Resistance.

 

So the temperature probe ensures you can make proper recordings.

The logging software ensures that you can record and retrieve it easily.



I'll cover some of the other features in the next blog, and see if I can't find a faulty motor or transformer.


Mark

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    Excellent work Mark, good job so far Peter
  • mcb1
    mcb1 over 11 years ago in reply to Robert Peter Oakes +1
    Thanks Peter. It's an impressive meter. Mark
  • shabaz
    shabaz over 11 years ago +1
    Hi Mark, Thanks for this information! It looks from the screenshots that it logged temperature every second which is good. Temperature logging capability is a major need for us in handheld multi-meters…
  • jw0752
    jw0752 over 11 years ago

    Hi Mark, Thanks for the follow up on this interesting meter.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to mcb1

    I will also be looking into logging over the next week and and a performance comparison (The logging I will be doing is more on the other DMM features as Gough  is covering the IRT Logging )

     

    My meter is stripped to the bone right now as I take pictures of the boards and compare to the U1273A image (I freeze it in ice, I drown it then I skin it alive...  muuuhaaaaa  )

     

    btw You can also increase the sample rate by selecting the lesser number of digits if you ok with sacrificing resolution, available in the setup menu

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    Thanks guys

    shabaz

    I'll check tomorrow but I think it logs at less than 1 sec rate.

    It could be the update setting so I'll do some digging.

     

    Gough is going to look at the software and I'm sure he'll cover the logging in much more detail.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Nice detailed post.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago

    Never would I have guessed how to use this meter. Thanks for the heads up mcb1,

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>