RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Philips MASTER LEDspot Teardown
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: shabaz
  • Date Created: 7 Oct 2018 12:22 AM Date Created
  • Views 3226 views
  • Likes 17 likes
  • Comments 18 comments
Related
Recommended
  • philips_lumileds
  • leds
  • led lighting
  • philips
  • dialog semiconductor
  • teardown

Philips MASTER LEDspot Teardown

shabaz
shabaz
7 Oct 2018

Introduction

I recently ordered various LED home lighting from a UK supplier (theledspecialist.co.uk), and unfortunately one arrived smashed : ( They kindly sent a replacement very quickly, but before I threw out the damaged one, I couldn't resist a teardown : )

 

Details
NamePhilips MAS LEDspot CLA D 9.5-75W 830 PAR30S 25D
EAN Code8718696713907
UPC Code929001342902

 

It is a 9.5W, 760 lumen LED bulb, warm white, with an Edison E27 fitting. It has a 25,000 hour life (longer than the usual 15,000 hour rating), intended for lobbies, walkways and so on according to the datasheet at the Philips Lighting website. As its name suggests, the beam is fairly tight (about 25 degrees overall). I'm using it in the workshop as some temporary lighting (it replaced a bulb that I needed elsewhere, and I was curious to find out what this new-ish model Philips bulb was like!).

 

Teardown

Opening the box, I saw the bulb was smashed : ( Rarely for an LED bulb, it actually has a lot of glass! Definitely not one to drop! Despite all the glass that front lens is plastic, and there are more detailed photos further below.

image

The glass body is extremely thick (about 4mm). I couldn't understand why there was so much glass used, but I'm wondering if it was needed for producing the inner mirror reflective surface, or for strength. Perhaps the inner surface is intended to reflect out heat as well as lots of light. The inner surface was extremely reflective, just like a first-surface optical mirror, but with the dimple pattern that you can see from the outside in the photo below (and in some of the fragments in photos further below). I get the feeling that the entire enclosure forms a large part of the cost of this lamp!

image

The front lens was quite interesting. I could not guess what plastic, it could be polycarbonate or something more exotic, since it needs to withstand heat and be highly transparent. But the part was stunning. It is extremely intricate.

image

Here's a side view. It looks like a fairly complex shape!

image

Inside the bulb, the LED was mounted on an metal-core PCB (MCPCB), held in place by a clip (removed for the photo below). The connecting wires appear to have a silicone-like insulation, and there is heat-proof sheathing around that too, where the cable passes through to the other side of the aluminium heatsink.

 

I could not identify the LED manufacturer, I'd initially assumed it was a Lumileds part, but it is not a shape that I could see in their online catalog. The heatsink is actually not that thick! Given the shape of it, and how it is attached at its sides to the glass, I'm wondering if the glass plays a role in the heat sinking too. The LED is clearly very efficient though, just from the sums - the bulb offers 760 lumens at 9.5W, so even at 85% efficiency from the driver, that's close to 95 lumens per watt, and it could be higher still. I'm tempted to do further measurements : ) but there are plenty other projects to do too image

image

The circuitry was potted, but it didn't look overly crushed together; the E27 fitting shape has more than enough room for this circuit. It looks about the level of quality to be expected I think, not bad at all. There are a few inductors, and a MOSFET in an unusual package (i.e. small!) next to the yellow square inductor.

image

The underside contained more semiconductors. The main IC is iW3689 from Dialog Semiconductor (PDF brief datasheet).

image

The brief datasheet circuit looks similar to the implementation on the circuit board, although I didn't inspect closely.

image

Summary

I was quite impressed at the design of this LED bulb. It's definitely a more involved design than I would have expected! By the way its un-smashed sibling has a nice warm-white and powerful light output too, as expected.

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 7 years ago +5
    Hi Shabaz, It is always good to see what is inside things, and you seem to constantly deliver on that for E14 - thank you. The PCB does look well made and populated, which is good to see. I doubt some…
  • DAB
    DAB over 7 years ago +5
    One man's trash is another man's opportunity for adventure. It would be interesting to see what the IR emission is compared to the visible light emission. Was there a spectral plot in the datasheet for…
  • shabaz
    shabaz over 7 years ago in reply to 14rhb +5
    Hi Rod, Thanks! You're right, it looks great. I believe that LED lighting is an interesting challenge for manufacturers, even moving from one fitting to another could change the design a lot. Unfortunately…
  • shabaz
    shabaz over 7 years ago in reply to mcb1

    Hehe I was wondering that too, if they were re-using glass production capability : ) I couldn't come up with a good conclusion : (

    Maybe the existing lamps by the bed are no bad thing, since the small bit of heat could be nice nearby (but I'm only saying that because it is freezing here for the past week : (

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 7 years ago
    Rarely for an LED bulb, it actually has a lot of glass!

    I wonder if they aren't reusing the existing bodies that would be used for other lamps.

    Obviously they've had to fit a new front cover and the lens is probably to narrow the beam width down.

     

    The beam width of LED's has been another problem as we have some 50mm Dycrohics mounted beside the bed, and they are 10 deg lamps to reduce light spill.

    Trying to find LED alternatives is impossible.

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to Jan Cumps

    Hmm. I'd say it was a boost converter...

     

    The switch in the chip can't take the rectified mains voltage, so it's isolated by running the coil current through the external MOSFET which is biased in the appropriate place by the zener on the gate.

    It ramps the coil current to the sense limit and then lets it go. The coil then moves above the positive supply rail and supplies the cap and LED (which both sit on the positive rail) through the diode.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago

    I suspect that the right upper part of the schematics can be redrawn to look like a traditional Buck converter layout ...

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to DAB

    Hi DAB,

     

    Unfortunately I could not identify the LED component of it, but the Philips datasheet of the lamp/bulb does have this diagram:

    image

    There's a fair amount of data (although I've seen more in some bulb datasheets, I've also seen a lot less in many!), here is some of the high-level specs on the light output:

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>