RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs POST 7 I'm really done this time… Red Pitaya STEMlab 125-14 PRO Gen 2 Starter Kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: colporteur
  • Date Created: 26 Sep 2026 6:52 PM Date Created
  • Views 41 views
  • Likes 6 likes
  • Comments 9 comments
Related
Recommended
  • RoadTest
  • test equipment
  • red pitaya

POST 7 I'm really done this time… Red Pitaya STEMlab 125-14 PRO Gen 2 Starter Kit

colporteur
colporteur
26 Sep 2026

SPOILER ALERT: The Red Pitaya powers down if the USB-micro connection on the module is used.

On of my troubleshooting attributes that can be either a blessing or a curse depending on the horse, is that I am persistent. In a previous post I used the term beating a dead horse. I did not like the outcome (failed) when I attempted to load the operating system on the QSPI & eMCC module. I figured, I would take up the switch and beat that horse some more.

I was set to look at SDR. That changed after reading a post. I had made a post on the Red Pitaya forum regarding some the issues I have faced, looking for some guidance. The replies left me thinking the problem was between the keyboard and chair.

A cruel step mother convinces their weak father to abandon Hansel and Gretel in the forest during a famine. Hansel uses white pebbles and later breadcrumbs to mark their path back home.

My breadcrumbs for this Red Pitaya fairy tale are the links to two vendor documents. The forum post suggested that Red Pitaya documentation is regularly updated every 30 days. I wanted to stay on the right path so vendor documents it is. The first link describes the full process. The second link deals with how to stop the watchdog timer.

Stopping the board during the U-boot autoboot countdown will cause the QSPI eMMC module to reboot Red Pitaya. At this point in the boot sequence, the Zynq processor has not yet started the Red Pitaya OS, so the watchdog kick signal on the E3 connector is absent. The E3 module firmware treats a missing watchdog signal as a system failure and triggers a power reset. The watchdog must be disabled before attempting to stop autoboot and enter the U-boot console.

My plan is to use USB-A to USB-micro cable for DFU programming details for this are found in the document.

https://redpitaya.readthedocs.io/en/latest/quickStart/E3_board/emmc_flash.html#important-watchdog-behaviour-during-u-boot-autoboot-stop

https://redpitaya.readthedocs.io/en/latest/developerGuide/software/system_development/e3_software/QSPI_eMMC_sw/QSPI_eMMC_software.html#e3-qspi-emmc-module-sw

Here is a summary of the steps:

STEP 1. Prepare an SD card with Red Pitaya OS 2.00 or later. Using version 3.00-57

STEP 2.Establish serial console access to Red Pitaya

STEP 3.Disable watchdog timer.

STEP 4.Boot the board, stop at U-boot autoboot.

STEP 5.From console run ums 0 mmc 0.

STEP 6.Flash the OS image to the eMMC from the PC.

STEP 7.Reboot into the full OS from the SD card.

STEP 8. Write boot.bin to QSPI flash with flashcp /opt/redpitaya/boot.bin /dev/mtd0.

STEP 9. Power off, remove the SD card, enable eMMC boot, and power on.

The procedure failed at STEP 3. When I plugged a USB-A from the Linux computer to USB-micro on the Red Pitaya the device immediately powered down.

In order to restore power to the Red Pitaya, I had to remove the USB-micro cable and remove the power cord to the Red Pitaya. A second attempted at using the USB-micros gave the same results. A different cable, a different combination of plugging cables in and trying it with no cables attached except for the USB-C power all ended with the power turning off on the Red Pitaya. Unless power and micro cable are removed, the board would not reboot.

The horse, that I refer to as loading the OS on the QSPI & eMCC module and not booting from the SD card, is down. I am unable to get it up, on the device I have.

I would ask the other RoadTest members to try plugging a USB-micro to USB-A cable into the module and see if they get the same results. There is nothing special you need to do other than plug the cable in between two devices. If other do not have a problem then the issue is with my board.

I'm moving on to examining SDR.

  • Sign in to reply
  • colporteur
    colporteur 17 days ago in reply to beacon_dave

    The power on/off feature provided through the module is one luxury. Not a have to have but a nice to have.

    I haven't issued a shutdown command since I completed the install.

    I expect it will get some focus along it life cyce.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave 17 days ago in reply to shabaz
    [quote userid="123345" url="~/products/roadtest/f/forum/57306/post-7-i-m-really-done-this-time-red-pitaya-stemlab-125-14-pro-gen-2-starter-kit/238390"]What's the reason for the eMMC module? Is it just a rugged alternative to the SD card?[/quote]

    "...Upgrade your Red Pitaya PRO Gen 2 board with the QSPI eMMC module Gen 2—a compact E3 add-on that enables secure, reliable power control and flexible boot options. Designed for the STEMlab 125-14 PRO Gen 2 and Z7020 PRO Gen 2, this module features single-button power on/off, safe shutdown, and booting from a microSD card or eMMC. It includes an onboard STM microcontroller, watchdog timer, and 16 high-speed FPGA-connected GPIOs, making it ideal for advanced applications requiring robust control and automation..."

    https://redpitaya.com/product/qspi-emmc-module-gen2/

    [quote userid="123345" url="~/products/roadtest/f/forum/57306/post-7-i-m-really-done-this-time-red-pitaya-stemlab-125-14-pro-gen-2-starter-kit/238390"]Since by step 2, the OS is already on the card, could that not be used as-is, i.e. ignore the eMMC module.[/quote]

    I'm guessing that as the module was supplied as part of the RoadTest hardware, then some of these features should be at least checked out ?

    I can see the single-button power on/off + safe shutdown being a useful feature to make use of.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 17 days ago

    What's the reason for the eMMC module? Is it just a rugged alternative to the SD card? Since by step 2, the OS is already on the card, could that not be used as-is, i.e. ignore the eMMC module. Performance difference is likely near-negligible, since the OS (well, parts of it) will be running from RAM.

    I remember on the good old BeagleBone Black, that had eMMC, but the only time I used it was to install the micro SD, that eMMC was a waste of money as far as I was concerned (granted it is more rugged, as mentioned, but not good for development, since space was so limited with it).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave 18 days ago

    Can't the QSPI & eMCC module be programmed while unplugged from the main RP board ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<