RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Review of the Freedom KL25z Board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: e14 Contributor
  • Date Created: 26 Jul 2013 5:25 AM Date Created
  • Views 3117 views
  • Likes 2 likes
  • Comments 14 comments
Related
Recommended
  • RoadTest
  • freescale
  • frdm_kl25z

Review of the Freedom KL25z Board

e14 Contributor
e14 Contributor
26 Jul 2013

image

 

At first glance, this board seems a little complex, to say the least: it has two USB ports, a million pads to solder headers on, a touch slider, an accelerometer and a large TQFP-80 ARM microcontroller. This is different to what most people coming from an Arduino background will be familiar with (a board that has just enough to program and run the microcontroller, no more). However, this is a 32-bit ARM we are talking about, a significant step up from the 8-bit AVR microcontrollers. Still, Freescale has really thought of everything when designing this board - the little things like the rubber standoffs and space to solder a coin cell holder allow this board to be used anywhere and everywhere. Plus, the beautiful black soldermask with ENIG plating makes this something you'd want to have hanging up somewhere in your house, on a project you can show off!

 

The board came with one of those mini CDs, which I promptly disregarded; it's completely unnecessary. Instead, I went over to the Freescale product page for the board, and was presented with a huge wall of text, much of which was a string of letters and numbers. Heading to the training/support tab, I found a training video I thought I'd try. However, this required the use of the CodeWarrior IDE. This was the low point of my experience; in order to download a trial version of the software, I had to create a full account with Freescale (giving out all sorts of details such as what the end product is), only to be presented with a message saying that my request will be processed, instead of a download link. Forget it!

 

Unable to bear the information overload on the Freescale site, I went to the element14 product pageelement14 product page, and found a really useful mbed quick start guide. It's dead easy to set up - as easy as getting an Arduino up and running. All you have to do is:

 

  1. Plug in the board using the SDA USB port with the reset button held (it'll appear as a usb storage device)
  2. Go to the mbed website and download a bootloader
  3. Place the bootloader in the root folder of the board
  4. Restart the board

 

Then, you create an account with MBED, and you can compile! You can also import demo programs with just a couple of clicks, and when you hit compile, you get a .bin file, which you place in the root folder of the board (which is now titled MBED), and voilà - your program will run! And MBED has a much more comprehensive list of demo programs than what I found on the Freescale website. The beauty of using an online compiler is that you can get up and running on any machine with an internet connection, and still have all your previous programs and projects, thanks to the miracle of cloud storage!

 

Now, the cherry on top of the board is its price. It costs roughly $15, as much as a meal at a café! I would definitely recommend this board to anybody wanting to go further with their embedded electronics projects. Perhaps this isn't the product of choice for people new to electronics and programming, but hey, that's what Arduino is for. A suggestion to element14 however: ship these boards with the headers as well, as you can then solder them on and get started quickly, instead of waiting around for another order to come in!

 

More high-resolution images and example code here:

http://zapterra.com/systems/2013/07/26/testing-the-freedom-board/

 

*UPDATE*

I've had some more time to play around with this board using mbed (still no reply from Freescale regarding the CodeWarrior IDE), and I can say this board is nothing short of amazing. Being new to ARM in general, I was afraid of a steep learning curve, but the documentation on mbed.org regarding this board is great. There are explained examples on using various parts of the board such as the touch slider, and since the whole platform is online, importing libraries and examples is really simple. Just be warned that if you don't have much background in C/C++ or microcontroller programming in general, then you will likely get a few headaches before you get any interesting code of your own running. That being said, the libraries and mbed framework in general is extremely well designed and not hard to work with at all.

 

*UPDATE 2*

Well, Freescale has replied to me directly in the comments, and even posted direct download links to the codewarrior IDE. Shows great customer care and support; better late than never!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 13 years ago in reply to mcb1 +3
    Update that WILL be of interest. I ordered another KL25Z (Australia/NZ) and was surprised that it was packaged in its own bag. Included are the Header and Jumpers to fit to the board. Part Numbers 2215580…
  • mcb1
    mcb1 over 13 years ago +1
    Rahul Nice review I would agree with your comment about headers. The very least is the ability to add them to the order. Mark
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1 +1
    Thanks! Yeah, I don't thing there's anybody out there who wouldn't add the headers to their order, as it really does save time and effort.
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Free Trials and downloads are always a mixed bag.

     

    The TI site always makes me laugh "...are you going to use it in a guided missle application ..."  duh as if I'd answer that correctly..

     

    re

    you can download all the stuff online anyway

    Believe it or not some people don't have 100mB unlimited bandwidth internet.

    Its not just the third world, we're talking about relatively developed countries (we in NZ have running water now).

    Unless you live in the big cities or are not rural, then you may have very limited internet access.

     

    but if you don't have an internet connection, what are you doing with a 32-bit ARM

     

    I can think of a few uses that don't actually require internet to make it do things.

     

    It's a powerful and very affordable platform.

     

    It would be great if they offered headers see below for update, and when you buy the MEMs Sensor board they fit enough to allow it to be plugged in ....

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to phoenixcomm

    Most trial software is downloadable without registration, the only catch being that it expires after a while or it's limited somehow (take CadSoft Eagle for example). I don't see why Freescale has to gather so many details for you to download a trial version. That process is standard for ordering free IC samples, but it doesn't make sense for software. BTW, they still haven't replied to me...

     

    I agree that I should have at least loaded up the CD. However, there's really no need to send one because:

    • you can download all the stuff online anyway
    • online you can find the latest/updated versions
    • it's not very environmentally friendly to make thousands of CDs to send with the product (some people don't care about this but it still stands true)

    The only advantage I can see of having a CD is being able to access stuff offline, but if you don't have an internet connection, what are you doing with a 32-bit ARM? I'd much rather they just printed out the links to support.

     

    And Steve, I'm definitely going to try out "digital paper weight" next time (or perhaps "32-bit moustache trimmer")!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dragonstyne
    dragonstyne over 13 years ago in reply to phoenixcomm

    Christina,

     

    I agree with you, It's really none of their business what your are going to build. Besides, if the product is good you would hade multiple projects.

     

    I think a great answer would be...

    Digital Paper Weight  (Joke, I actually like the product)

     

    I think that would get their attention.

     

    Steve

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dragonstyne
    dragonstyne over 13 years ago

    Greetings,

     

    I agree, the headers should be included. I would rather pay a little more for the product with the header.

     

    As it is, I had to drive 70+ miles to get them and, still had to cut them down to fit.  I could have ordered them but...

     

    I did not want to wait. I wanted to play now

     

    I bought extra. Like Nico, just in case.

     

    The problem I see is, if you are not careful at soldering you can destroy the board.

     

    I like the option of using the IDE or MBED. if your prototyping or learning provides a lot of resources.

     

    Rahul,

     

    Good review.

     

    Regards,

     

    Steve

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 13 years ago in reply to e14 Contributor

    I wonder if they're expecting people to already have the headers in stock. I also had to wait a few weeks before I could add any external bits to it. But now I have enough of them for 4 more boards image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>