RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Here's Why I think You Should Consider Applying for the MAX32650 EV Kit RoadTest
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 2755 subscribers
  • Views 2234 views
  • Users 0 members are here
  • maxim integrated
Related

Here's Why I think You Should Consider Applying for the MAX32650 EV Kit RoadTest

rscasny
rscasny over 6 years ago

I know I have been getting a lot of fantastic products lately to roadtest. It's kind of pre-Holiday wishlist!

 

But there's one roadtest, I'd like you to take another loook at: Maxim MAX32650-EVKIT

 

The Ev kit is from Maximum Integrated. this kit is for the MAX32650.image

 

The MAX32650 ultra-low power memory scalable microcontroller designed specifically for high performance battery powered applications. It is often used with industrial sensors, IoT, sports watches, fitness monitors, wearable medical patches and portable medical devices.

 

Here's some more information on the MAX32650.

 

The MAX32650 is part of Maxim Integrated's DARMAN Series of low-power microcontrollers. They are smart, with the biggest memories in their class and a massively scalable memory architecture. They run forever, thanks to wearable-grade power technology. They are also tough enough to withstand the most advanced cyberattacks.

 

These ultra low-power microcontrollers are designed to handle the complex applications demanded by today’s advanced battery-powered devices and wireless sensors.They are based on ArmRegistered CortexRegistered-M4 with FPU CPU with 3MB flash and 1MB SRAM. Memory scalability is supported with multiple memory-expansion interfaces, including a HyperBusTm/XccelaTm DDR interface and two SPI execute in place (SPIX) interfaces. A secure digital interface supports external high-speed memory cards, including SD, SDIO, MMC, SDHC, and microSDTm

 

Here's some tech specs:

  • 120MHz Arm Cortex-M4 with FPU
  • SmartDMA Provides Background Memory Transfers with Programmable Data Processing
  • 120MHz High-Speed and 40MHz Low-Power Oscillators
  • 7.3728MHz Low Power Oscillators
  • 32.768kHz and RTC Clock (Requires External Crystal)
  • 8kHz Always-on Ultra-Low Power Oscillator
  • 3MB Internal Flash, 1MB Internal SRAM
  • 104µW/MHz Executing from Cache at 1.1V
  • Five Low Power Modes: Active, Sleep, Background, Deep-Sleep, and Backup
  • 1.8V and 3.3V I/O with No Level Translators

 

Here's some documentation: https://datasheets.maximintegrated.com/en/ds/MAX32650-EVKIT.pdf

 

 

If you do have the time, fill out an application here:  Maxim MAX32650-EVKIT

  • Sign in to reply
  • Cancel
Parents
  • crisdeodates
    crisdeodates over 6 years ago

    rscasny , This is a nice module to roadtest. But it takes some time to understand this item and its developing environment to learn to use it better. I usually fit the products I roadtest into one of my ongoing projects or at least try to use them to upgrade a former one. I really could not find a place for this product in any of my projects yet. Once I find something, I would definitely apply, provided I am sure that I could complete it before its deadline without affecting my current or future roadtests image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • crisdeodates
    crisdeodates over 6 years ago

    rscasny , This is a nice module to roadtest. But it takes some time to understand this item and its developing environment to learn to use it better. I usually fit the products I roadtest into one of my ongoing projects or at least try to use them to upgrade a former one. I really could not find a place for this product in any of my projects yet. Once I find something, I would definitely apply, provided I am sure that I could complete it before its deadline without affecting my current or future roadtests image

    • Cancel
    • Vote Up +3 Vote Down