RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Some Special Roadtesters for the UltraZed-EV
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 2759 subscribers
  • Views 3589 views
  • Users 0 members are here
  • ultrazed-ev
  • scasny
  • avnet
  • xilinx
Related

Seeking Some Special Roadtesters for the UltraZed-EV

rscasny
rscasny over 6 years ago

I am considering to roadtest the UltraZed-EV board. The UltraZed-EV is a highly flexible, rugged, System-On-Module based on the Xilinx Zynq UltraScale+ MPSoC. It's ideal for embedded video processing system development.image

 

In order to roadtest this board, I've discussed with the sponsor what kind of roadtester he needs and any specific requirements as well. Out of those discussions, I've come to the conclusion I need a special roadtester -- someone who has video experience and has the ability to write a quality technical report.

 

Specifically, these are the things the sponsor is looking for in a roadtester:

 

  1. Video Centric (preference to designs using interfaces without an Avnet reference design)
  2. External pieces (Video/PCIe/SATA/SFP+/etc.) should be COTS and readily available
  3. Utilize VCU (optional)
  4. Prefer staying within bounds of VCU TRD (see point 1)
  5. Have fun, show something exciting and new! (AI/ML?)

 

If you are interested and have these requirements, please leave a comment and I'll get back to you. Or, you can message me at rscasny

 

 

(BTW: If you are new to roadtesting, and are selected, you would receive the UltraZed-EV at no charge to you. I'll give you more info later.)

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • kk99
    kk99 over 6 years ago

    I think that will be perfect platform to make an example of adaptive bitrate streaming device. Below there be possible flow:
    1. As input source we could use camera connected via HDMI or 3G-SDI.

    2. Then will be required to encode input source in few variants (e.g. 4K, FHD, HD, SD and different bitrates) with given codec e.g. H265

    3. In PS this variants will be segmented and created single content source in given technology e.g. master playlist in HLS, media presentation in MPEG-DASH or manifest in SmoothStreaming.

    4. There will be HTTP server (e.g. Apache or Nginx). Playlists with segments could be stored in external hard drive connected via SATA. This allow us to create longer DVR window for content, so client player could has timeshift feature. It is possible to create some example of request caching in case of simulation of more client players.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kk99
    kk99 over 6 years ago

    I think that will be perfect platform to make an example of adaptive bitrate streaming device. Below there be possible flow:
    1. As input source we could use camera connected via HDMI or 3G-SDI.

    2. Then will be required to encode input source in few variants (e.g. 4K, FHD, HD, SD and different bitrates) with given codec e.g. H265

    3. In PS this variants will be segmented and created single content source in given technology e.g. master playlist in HLS, media presentation in MPEG-DASH or manifest in SmoothStreaming.

    4. There will be HTTP server (e.g. Apache or Nginx). Playlists with segments could be stored in external hard drive connected via SATA. This allow us to create longer DVR window for content, so client player could has timeshift feature. It is possible to create some example of request caching in case of simulation of more client players.