RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum My Brief Thoughts on Roadtesting
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 2756 subscribers
  • Views 4811 views
  • Users 0 members are here
Related

My Brief Thoughts on Roadtesting

14rhb
14rhb over 5 years ago

To make a point on Renesas RX72N Envision Kit | element14 |without detracting from the subject matter of compilers, GUI or board capability I have broken my thoughts out here regarding who is attracted to roadtesting such embedded development boards and hence the licensing of software.

 

I believe more roadtesters are keen hobbyists or students and therefore have a limited budget preventing them purchasing the niche software required to continue using these products. Instead they rely on the free or time limited software available from the vendor. Once the roadtest is complete that software can expire quite quickly and the board gets little use afterwards. This is a pity as the board never appears again in future projects or blog posts. The board's roadtest also often consists of showing the demo software only, perhaps with a few changes.

 

Conversely, professional developers will likely buy development boards as part of their companies work plan and the boss would also likely agree to paying for the software, supporting license agreements over the period of the project. All the testing and development is undertaken in that team and the end goal is to make money by selling a product, and such people have less time available to come onto E14 to roadtest and review.

 

I'd like to see more open source support for such embedded boards with manufacturers perhaps issuing licenses to their software to allow the 'hobbyist' end of the roadtesters to continue using the product. Should they create something appealing then the manufacturer would likely benefit from the increased orders for the hardware itself? However being able to identify useful open source solutions that roadtesters can use and build skills in should be encouraged.

 

Just in case this post reads as a case to stop roadtests or for manufacturers to stop sponsoring them, please read on ! I'm confident the roadtests are read by professional developers when picking out new products for their development - so very useful still. I also need to add, IMO many of the keen hobbyists and students take the knowledge gained from roadtesting back into companies, maybe as their day job or when they start a career. Regardless of which end of that skills and application scale the member is at, all the comments in roadtests etc are invaluable, available for all to see/learn from and action accordingly. My last point is that I have actually bought several pieces of test equipment and dev boards for colleagues at my work following roadtests by other members on E14, although I class myself as a hobbyist  image.

  • Sign in to reply
  • Cancel
Parents
  • misaz
    misaz over 5 years ago

    I agree that license for compiler should be included with roadtest or provided for free for everyone developing non-commercial projects. For example Segger Emebeded Studio (which I am using now as part of Arduino Nano 33 BLE Roadtest) is free for non-commerical projects and MCU manufacturer negotiated that when used with their (but only their) devices it is free even for commerical projects.

     

    Also note that GCC for RX72N is avalaible. It is part of installer but it is less supported than their proprietary compiler and provided examples contains some compiler specific stuff which makes hard to compile some examples using GCC (you must do appropriate modifications. Then it also should be compilable using GCC).

     

    I do not think that board become useless when license expire, but it will be more hard to use it.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • misaz
    misaz over 5 years ago

    I agree that license for compiler should be included with roadtest or provided for free for everyone developing non-commercial projects. For example Segger Emebeded Studio (which I am using now as part of Arduino Nano 33 BLE Roadtest) is free for non-commerical projects and MCU manufacturer negotiated that when used with their (but only their) devices it is free even for commerical projects.

     

    Also note that GCC for RX72N is avalaible. It is part of installer but it is less supported than their proprietary compiler and provided examples contains some compiler specific stuff which makes hard to compile some examples using GCC (you must do appropriate modifications. Then it also should be compilable using GCC).

     

    I do not think that board become useless when license expire, but it will be more hard to use it.

    • Cancel
    • Vote Up +7 Vote Down