RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum My Brief Thoughts on Roadtesting
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 2752 subscribers
  • Views 4870 views
  • Users 0 members are here
Related

My Brief Thoughts on Roadtesting

14rhb
14rhb over 5 years ago

To make a point on Renesas RX72N Envision Kit | element14 |without detracting from the subject matter of compilers, GUI or board capability I have broken my thoughts out here regarding who is attracted to roadtesting such embedded development boards and hence the licensing of software.

 

I believe more roadtesters are keen hobbyists or students and therefore have a limited budget preventing them purchasing the niche software required to continue using these products. Instead they rely on the free or time limited software available from the vendor. Once the roadtest is complete that software can expire quite quickly and the board gets little use afterwards. This is a pity as the board never appears again in future projects or blog posts. The board's roadtest also often consists of showing the demo software only, perhaps with a few changes.

 

Conversely, professional developers will likely buy development boards as part of their companies work plan and the boss would also likely agree to paying for the software, supporting license agreements over the period of the project. All the testing and development is undertaken in that team and the end goal is to make money by selling a product, and such people have less time available to come onto E14 to roadtest and review.

 

I'd like to see more open source support for such embedded boards with manufacturers perhaps issuing licenses to their software to allow the 'hobbyist' end of the roadtesters to continue using the product. Should they create something appealing then the manufacturer would likely benefit from the increased orders for the hardware itself? However being able to identify useful open source solutions that roadtesters can use and build skills in should be encouraged.

 

Just in case this post reads as a case to stop roadtests or for manufacturers to stop sponsoring them, please read on ! I'm confident the roadtests are read by professional developers when picking out new products for their development - so very useful still. I also need to add, IMO many of the keen hobbyists and students take the knowledge gained from roadtesting back into companies, maybe as their day job or when they start a career. Regardless of which end of that skills and application scale the member is at, all the comments in roadtests etc are invaluable, available for all to see/learn from and action accordingly. My last point is that I have actually bought several pieces of test equipment and dev boards for colleagues at my work following roadtests by other members on E14, although I class myself as a hobbyist  image.

  • Sign in to reply
  • Cancel
Parents
  • cstanton
    cstanton over 5 years ago

    I'd like to see more open source support for such embedded boards with manufacturers perhaps issuing licenses to their software to allow the 'hobbyist' end of the roadtesters to continue using the product. Should they create something appealing then the manufacturer would likely benefit from the increased orders for the hardware itself? However being able to identify useful open source solutions that roadtesters can use and build skills in should be encouraged.

    I'd love people who have the capability to roadtest products to see it as an opportunity to support the hardware with open source in mind as well, however what ends up happening, even with hardware that is designed with open source in mind (beagleboard?) is that people expect some level of "I don't want to have to work this out myself" but that fundamentally ends up being the situation when something is open source - because, no-one wants to do it for free, or give something away for free, and it only tends to come to fruition when someone has a devout interest or dedication in bringing it to everyone for the altruism for it.

     

    I believe we also have a side difficulty when we're given products to roadtest in that we look at it and go... "you realise you can't only give us the microcontroller/hardware board for this right? you can't expect roadtesters to have everything necessary to test this properly?" and it's likely software support is overlooked in some cases, or the supplier realises having an engineer test the kit is a bit more involved and needs the infrastructure.

     

    What was the term coined these days? Software as a service or similar?

     

    I personally find it frustrating either way, and maybe I went off on a tangent image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 5 years ago in reply to cstanton

    Well, I suppose it's nice for them to realise what's needed and provide it ...

     

    ... but if they don't, my pet peeve is when the licensing itself restricts the possibility of building a compatible "open-source" solution through clauses that prohibit reverse engineering altogether (and I don't mean the sort that involves decompiling, disassembly, but even observing or inferring what their code does or monitoring its operation). I know some companies feel their code offers a great competitive advantage and they may fear that their "innovation" is somehow recreated and/or ported to a rival platform or device, but at the same point in time, if they can't be reasonable about providing the license then more often than not, a tinkerer will probably find their own way around it.

     

    I've also done some RoadTests where I knowingly broke the license (which prohibited taking screenshots, or comparing the software to others). While nothing untoward has happened as a result of it, when you send a product for legitimate independent review, comparison and screenshots are supposed to be a fact of life.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 5 years ago in reply to cstanton

    Well, I suppose it's nice for them to realise what's needed and provide it ...

     

    ... but if they don't, my pet peeve is when the licensing itself restricts the possibility of building a compatible "open-source" solution through clauses that prohibit reverse engineering altogether (and I don't mean the sort that involves decompiling, disassembly, but even observing or inferring what their code does or monitoring its operation). I know some companies feel their code offers a great competitive advantage and they may fear that their "innovation" is somehow recreated and/or ported to a rival platform or device, but at the same point in time, if they can't be reasonable about providing the license then more often than not, a tinkerer will probably find their own way around it.

     

    I've also done some RoadTests where I knowingly broke the license (which prohibited taking screenshots, or comparing the software to others). While nothing untoward has happened as a result of it, when you send a product for legitimate independent review, comparison and screenshots are supposed to be a fact of life.

     

    - Gough