RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum My Brief Thoughts on Roadtesting
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 2756 subscribers
  • Views 4810 views
  • Users 0 members are here
Related

My Brief Thoughts on Roadtesting

14rhb
14rhb over 5 years ago

To make a point on Renesas RX72N Envision Kit | element14 |without detracting from the subject matter of compilers, GUI or board capability I have broken my thoughts out here regarding who is attracted to roadtesting such embedded development boards and hence the licensing of software.

 

I believe more roadtesters are keen hobbyists or students and therefore have a limited budget preventing them purchasing the niche software required to continue using these products. Instead they rely on the free or time limited software available from the vendor. Once the roadtest is complete that software can expire quite quickly and the board gets little use afterwards. This is a pity as the board never appears again in future projects or blog posts. The board's roadtest also often consists of showing the demo software only, perhaps with a few changes.

 

Conversely, professional developers will likely buy development boards as part of their companies work plan and the boss would also likely agree to paying for the software, supporting license agreements over the period of the project. All the testing and development is undertaken in that team and the end goal is to make money by selling a product, and such people have less time available to come onto E14 to roadtest and review.

 

I'd like to see more open source support for such embedded boards with manufacturers perhaps issuing licenses to their software to allow the 'hobbyist' end of the roadtesters to continue using the product. Should they create something appealing then the manufacturer would likely benefit from the increased orders for the hardware itself? However being able to identify useful open source solutions that roadtesters can use and build skills in should be encouraged.

 

Just in case this post reads as a case to stop roadtests or for manufacturers to stop sponsoring them, please read on ! I'm confident the roadtests are read by professional developers when picking out new products for their development - so very useful still. I also need to add, IMO many of the keen hobbyists and students take the knowledge gained from roadtesting back into companies, maybe as their day job or when they start a career. Regardless of which end of that skills and application scale the member is at, all the comments in roadtests etc are invaluable, available for all to see/learn from and action accordingly. My last point is that I have actually bought several pieces of test equipment and dev boards for colleagues at my work following roadtests by other members on E14, although I class myself as a hobbyist  image.

  • Sign in to reply
  • Cancel
  • cstanton
    cstanton over 5 years ago

    I'd like to see more open source support for such embedded boards with manufacturers perhaps issuing licenses to their software to allow the 'hobbyist' end of the roadtesters to continue using the product. Should they create something appealing then the manufacturer would likely benefit from the increased orders for the hardware itself? However being able to identify useful open source solutions that roadtesters can use and build skills in should be encouraged.

    I'd love people who have the capability to roadtest products to see it as an opportunity to support the hardware with open source in mind as well, however what ends up happening, even with hardware that is designed with open source in mind (beagleboard?) is that people expect some level of "I don't want to have to work this out myself" but that fundamentally ends up being the situation when something is open source - because, no-one wants to do it for free, or give something away for free, and it only tends to come to fruition when someone has a devout interest or dedication in bringing it to everyone for the altruism for it.

     

    I believe we also have a side difficulty when we're given products to roadtest in that we look at it and go... "you realise you can't only give us the microcontroller/hardware board for this right? you can't expect roadtesters to have everything necessary to test this properly?" and it's likely software support is overlooked in some cases, or the supplier realises having an engineer test the kit is a bit more involved and needs the infrastructure.

     

    What was the term coined these days? Software as a service or similar?

     

    I personally find it frustrating either way, and maybe I went off on a tangent image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 5 years ago

    I agree that license for compiler should be included with roadtest or provided for free for everyone developing non-commercial projects. For example Segger Emebeded Studio (which I am using now as part of Arduino Nano 33 BLE Roadtest) is free for non-commerical projects and MCU manufacturer negotiated that when used with their (but only their) devices it is free even for commerical projects.

     

    Also note that GCC for RX72N is avalaible. It is part of installer but it is less supported than their proprietary compiler and provided examples contains some compiler specific stuff which makes hard to compile some examples using GCC (you must do appropriate modifications. Then it also should be compilable using GCC).

     

    I do not think that board become useless when license expire, but it will be more hard to use it.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    ... I do find it very puzzling that some vendors offer Roadtest stuff with short time limited licenses - not just dev boards but instruments as well. Some Roadtests go on giving product exposure long, long after the official test is done.

    ...

    Indeed. It also hampers with the ability to answer questions.

    When there's someone trying to replicate or use things you've described in the test, and they are stuck, you can't help.

    The vendor could have profited from the support of an already convinced believer, for no extra investment.

     

    I'm a fan of ever-lasting evaluation licenses.

    I think it is fair to say: the license can only be used for evaluation and test purposes.

    But by giving the license an end-date, it results in the kit that will never be used again (as already told above) and that the new fanboy is rendered powerless image.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 5 years ago in reply to michaelkellett

    Thanks for your valuable words of wisdom. Sounds like your approach of Keil/ARM MDK works well for you, balancing your investment with ability to use something that works well.

     

    I know several companies where the boss isn't that keen on buying software (or hardware) tools.

    That resistance is a boss thing image. Once they see some costs showing extra income they tend to be more happy to hand over the company credit card !

     

    I'll be watching out for Bridgetek Eve products now as I hadn't heard of them before, sounds like they might be easy to use if much of the GUI code is embedded already.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago

    Here's a few random thoughts on the subject:

     

    Some companies have always tried hard to lock you in to their own tools although most seem to be trying to reduce the cost of development. In some product areas (like FPGA) they don't really have any options other than provide part specific tools.

     

    I know several companies where the boss isn't that keen on buying software (or hardware) tools.

     

    I don't mind (too much) paying for general purpose tools but I don't like paying for vendor specific tools - so I do all my embedded C development with Keil/ARM MDK - not cheap but supports multiple vendors.

     

    It's all part of the big picture you need to look at when choosing parts - unless your volumes are big then the cost of development is usually more significant than the cost of parts.

     

    I do find it very puzzling that some vendors offer Roadtest stuff with short time limited licenses - not just dev boards but instruments as well. Some Roadtests go on giving product exposure long, long after the official test is done.

     

    On a very specific point, the Bridgetek Eve family of graphics controller chips embedd a lot of graphics library stuff in the hardware  - you can buy displays with these chips built in. There are free tools.

     

    MK

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • Cancel
<