RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum White boarding a RoadTest Review of The Microchip PoE to USB-C®︎ adapter
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2754 subscribers
  • Views 5678 views
  • Users 0 members are here
Related

White boarding a RoadTest Review of The Microchip PoE to USB-C®︎ adapter

colporteur
colporteur over 5 years ago

image

What are your expectations at connection point C?

 

I am considering pitching an application for the Microchip PoE to USB-CRegistered Power and Data Adapter RoadTest review. I completed a review of a PoE device, Raspberry Pi4B (4GB) plus POE Hat - Review and figured why not leverage the knowledge into another PoE review.

 

The drawing shows my preferred setup for the RoadTest, a Linux laptop interfacing through a PoE Injector communicating with a Raspberry Pi4B. The injector is a device I acquired to resolve an issue I discovered during the RoadTest Review The Road to Raspberry Pi4B/ PoE Hat RoadTest Review (PoE insight needed) . I want to avoid more purchases.

 

After reviewing the documentation I'm confused about my expectations at point C in the diagram. I was hoping a white board session with others might clarify my understanding. One of the opportunities I miss in my retirement is the napkin discussion with technical minds during a coffee break at work. Using a drawing scribbled on a napkin, like minds worked to offer insight into solving a problem presented at the table.

 

The Microchip PoE to USB-CRegistered Power and Data Adapter provides power and data communication path. Can someone confirm my understanding that the Microchip adapter is acting as a Ethernet to USB adapter for communication? I found reference to a LAN7800 USB driver chip while drilling down through one of the documents. I assume that means the end device (i.e. Pi would require the driver support).

 

I'm not familiar with many devices that combine USB port functions of power and communication. The brochure for the product shows a tablet connected as a device. I have an Apple tablet that can act as device but that makes it rather difficult to take measurements under varying loads. In my test scenario I'm thinking I will need a breakout cable to separate Microchip adapter power from the USB signal. As an additional test in my review, I was hoping to use a Android laptop I have as an additional device to test the endpoint. But again I would need to separate power and USB signals.

 

Questions:

What are your expectations at connection point C?

  • Sign in to reply
  • Cancel
Parents
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago

    I like the idea to have discussions like that.

     

    My understanding would be that (at point C) you have a single USB-C interface providing power (as in USB Power delivery up to 20V 3A if the device is capable of active PD negotiation) and USB communication.

    The RPi uses the USB-C port only for power and this only for 'passive' PD with a max of 5V 3A. As the RPi is a USB host, you could not use the data part of that setup.

    I hope this makes sense.

    - W.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to wolfgangfriedrich

    To bad we didn't have the napkin between us. Here is my confusion. I agree the Micochip device is USB-C output but it does send the data out the otherside as Ethernet or that is what I assume (maybe I am wrong). That would lead me to see the Microchip as a USB to Ethernet adapter requiring a device driver. If I am wrong how is the data sent down the wire. At the other end the data has to be removed from a PoE injector (i.e. Ethernet).

     

    I appreciate taking the time to respond. Still searching. If you wanted to talk to the end device from laptop what would the end device been identified as a USB device or an Ethernet connection? If USB what are the protocol changes between the different points A, B & C.

     

    The more research I do for the Review the more I think it is a great opportunity to answer questions. Just because there is PoE to USB when would you want to use it and at what cost.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to colporteur

    I looked into the Quickstart guide for the Microchip adapter. It does need drivers for unit plugged into the USB port (the RPi4 in your case). And it also states that the USB port on the Microchip adapter is a USB device port so it would be possible to plug in the RPi if you have a USB splitter to separate power and data. My statement (Guess) in my 1st comment about the Micorchip adapter being a USB master port is incorrect.

    Asplitter like this might be usable:

    https://www.tindie.com/products/8086net/usb-cpwr-splitter/

    https://www.tindie.com/products/clarahobbs/pd-buddy-wye/

     

    The question still stands, as what kind of connection it would show up on the RPi? Now I would guess, it would present itself as a regular network connection through the custom driver, but not sure about this.

     

    The roadtest could be a straight functionality investigation with install instructions, performance data rate test as one part. Sounds like mostly software driver installation and IT work.

     

    The other part would be to exercise the USB PD part. A USB PD Sink would be required to request different power profiles between 5 V and 20 V with different max current settings.

    A device like this would be useful (shameles self plug image)

    https://www.tindie.com/products/pier42/usb-c-pd-sink/

     

    - W.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to Gough Lui

    Same here, I was not aware that the RPI USB power port was data enabled.

    So this discussion was useful in multiple directions.

    Thanks for the insights.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 5 years ago in reply to Jan Cumps

    Well, you'll have to just try it and see. The reason I say you may have to enable the overlay is because the OTG hardware on the Pi4 is configured "device only" by default -

    The OTG hardware present on previous models of Pi is still available and it has moved to a single connection on the USB-C port. The OTG hardware is intended to be used in device-only mode on Pi 4.

    from https://www.raspberrypi.org/documentation/hardware/raspberrypi/usb/README.md

     

    Instead, if you want to be able to talk to the Microchip LAN7800, you basically need the OTG port on the Pi4 (i.e. the USB-C port) to become a USB host as the adapter is very clearly a device-only role. I'm not sure if such a configuration will be stable or intended based on the documentation.

     

    But just to "try it out" is a perfectly good reason to apply for a RoadTest, because I'd have to say that some of the documentation is not quite as clear as it should be, and the way USB-C is implemented across devices is very very variable.

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 5 years ago in reply to Jan Cumps

    Well, you'll have to just try it and see. The reason I say you may have to enable the overlay is because the OTG hardware on the Pi4 is configured "device only" by default -

    The OTG hardware present on previous models of Pi is still available and it has moved to a single connection on the USB-C port. The OTG hardware is intended to be used in device-only mode on Pi 4.

    from https://www.raspberrypi.org/documentation/hardware/raspberrypi/usb/README.md

     

    Instead, if you want to be able to talk to the Microchip LAN7800, you basically need the OTG port on the Pi4 (i.e. the USB-C port) to become a USB host as the adapter is very clearly a device-only role. I'm not sure if such a configuration will be stable or intended based on the documentation.

     

    But just to "try it out" is a perfectly good reason to apply for a RoadTest, because I'd have to say that some of the documentation is not quite as clear as it should be, and the way USB-C is implemented across devices is very very variable.

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down