RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum White boarding a RoadTest Review of The Microchip PoE to USB-C®︎ adapter
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2667 subscribers
  • Views 5109 views
  • Users 0 members are here
Related

White boarding a RoadTest Review of The Microchip PoE to USB-C®︎ adapter

colporteur
colporteur over 4 years ago

image

What are your expectations at connection point C?

 

I am considering pitching an application for the Microchip PoE to USB-CRegistered Power and Data Adapter RoadTest review. I completed a review of a PoE device, Raspberry Pi4B (4GB) plus POE Hat - Review and figured why not leverage the knowledge into another PoE review.

 

The drawing shows my preferred setup for the RoadTest, a Linux laptop interfacing through a PoE Injector communicating with a Raspberry Pi4B. The injector is a device I acquired to resolve an issue I discovered during the RoadTest Review The Road to Raspberry Pi4B/ PoE Hat RoadTest Review (PoE insight needed) . I want to avoid more purchases.

 

After reviewing the documentation I'm confused about my expectations at point C in the diagram. I was hoping a white board session with others might clarify my understanding. One of the opportunities I miss in my retirement is the napkin discussion with technical minds during a coffee break at work. Using a drawing scribbled on a napkin, like minds worked to offer insight into solving a problem presented at the table.

 

The Microchip PoE to USB-CRegistered Power and Data Adapter provides power and data communication path. Can someone confirm my understanding that the Microchip adapter is acting as a Ethernet to USB adapter for communication? I found reference to a LAN7800 USB driver chip while drilling down through one of the documents. I assume that means the end device (i.e. Pi would require the driver support).

 

I'm not familiar with many devices that combine USB port functions of power and communication. The brochure for the product shows a tablet connected as a device. I have an Apple tablet that can act as device but that makes it rather difficult to take measurements under varying loads. In my test scenario I'm thinking I will need a breakout cable to separate Microchip adapter power from the USB signal. As an additional test in my review, I was hoping to use a Android laptop I have as an additional device to test the endpoint. But again I would need to separate power and USB signals.

 

Questions:

What are your expectations at connection point C?

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago +7
    I love this site! I miss the coffee break napkin discussions at work but this site provides the ideal replacement. My thanks to Gough Lui & Jan Cumps for making posts to my discussion. Your input enabled…
  • Gough Lui
    Gough Lui over 4 years ago in reply to Jan Cumps +5
    Well, you'll have to just try it and see. The reason I say you may have to enable the overlay is because the OTG hardware on the Pi4 is configured "device only" by default - The OTG hardware present on…
  • Gough Lui
    Gough Lui over 4 years ago in reply to Jan Cumps +4
    Funny that - I didn't realise they enabled USB-OTG on the USB-C connector. In that case, yes, the Pi would be able to detect a USB-Ethernet bridge and potentially transact data, but you do need to make…
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago in reply to Gough Lui

    Same here, I was not aware that the RPI USB power port was data enabled.

    So this discussion was useful in multiple directions.

    Thanks for the insights.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • hugohu
    hugohu over 4 years ago in reply to colporteur

    Wow, I also didn't know. Only knew the Pi 0 had such features. Thanks for sharing!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to hugohu

    Say again?

     

    I assumed the USB OTG was USB-C dependent. USB OTG is supported on the Pi Zero mini-sub connector? Hummm.... I will add that to the RoadTest Review scenario investigation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago in reply to colporteur

    Actually, USB-OTG has been a thing since the mini-USB-B connector came out (pre-dating microUSB) and is a way for mobile devices to assume a host role in addition to the (usual) device role so they could run things like USB memory sticks, card readers and other accessories. That being said, the OTG on earlier versions of the Pi B/B+ was used in the host role to supply USB to the USB Ethernet + Hub chip to produce the two/four downstream ports.

     

    But the Raspberry Pi Zero (and Model A/A+, although missing an ID pin for dynamic role switching) have a trick up their sleeve because they don't use this USB Ethernet + Hub chip, so they can act like a device as well using USB-OTG as the board has been designed with the necessary direct pin connections - https://gist.github.com/gbaman/50b6cca61dd1c3f88f41 . Since the Pi4 has a PCIe USB 3.0 controller, the USB ports are now supplied from this and the USB-C power in port now uses the OTG hardware for device role as default.

     

    But since the Microchip adapter is a device role, you really only want the port for the host mode. I would suspect that it might take some cable sleuthing to get the right combination to get a Pi Zero up with the adapter - perhaps a USB-OTG cable + A to C cable. But it should be achievable in some way.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to Gough Lui

    I'm thinking, (would like to test), that they Microchip is analogous to a USB network dongle. I have such a beast in my kit bag for when I encounter a laptop without an RJ45 Ethernet port. The Microchip documentation make reference to the LAN7000 chip. I assume the USB-C data connection establishes an Ethernet connection using this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago in reply to colporteur

    Well, it is a USB to Ethernet adapter, except it does PoE so it can backfeed power to the connected device using USB PD.

     

    Whether it can work as one when not connected to a PoE port (i.e. a regular port) may be worth testing and will depend on its design.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to colporteur

    colporteur  wrote:

     

    .... analogous to a USB network dongle ....

    I believe this is the best summary.

    Yes, with the additional function to power the device that's plugged in to it - if that's a device that can be powered via that USB port.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<