RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Ian Wraith, University of Sheffield, Texas Instruments' eZ430-RF2480 Development Kit review
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 2754 subscribers
  • Views 566 views
  • Users 0 members are here
  • development
  • ez430-rf2480
  • review
  • kit
Related

Ian Wraith, University of Sheffield, Texas Instruments' eZ430-RF2480 Development Kit review

awinning
awinning over 17 years ago
This kit consists of three eZ430-RF2480 target boards plus a MSP-eZ430U USB dongle interface and a couple of battery powered modules. The user connects one of the target boards to the USB dongle and the other two to the battery powered modules. This is everything you will need to build your own small test ZigBee network. Each target board consists of a MSP430F2274 microcontroller and a CC2480 network processor which communicate using SPI. There are also 5 GPIO lines available to use on the microcontroller.

 

 
The total documentation that arrived with the kit consisted of a single A4 sheet describing how to  launch a specially written Sensor Monitor program on a Microsoft Windows compatible PC by downloading software from the development kits web page located at ..

 

 
http://wwww.ti.com/eZ430-RF2480
 
The instructions were easy to follow and within 5 minutes I had a working ZigBee network consisting of a coordinator (the USB dongle) , a router and an end device (the battery powered target boards).  In the demonstration application these display their temperatures and battery voltages as shown in the screen shot below ..

 

 

 


 
I'm usually pleasantly surprised by the range of these low powered 2.4 GHz radio systems and ZigBee didn't disappoint  me as I found a target board could communicate through two brick walls in my 1950's built workplace. ZigBee extends this range further as its nodes automatically create networks to pass data between themselves. I can see this feature being very useful for my work which sometimes consists of designing sensors for use in the semiconductor clean rooms which pass data to a Texas central server via a radio link. In the past I used 433 MHz and then Bluetooth technology for this link but neither requires as little current as ZigBee and none can automatically form networks so I am keen to investigate this technology.

 

 
  Sadly the main drawback to this kit was the lack of documentation. As I mentioned earlier this consisted of a single A4 sheet of paper and web address. Annoyingly even the web site isn't that well organised and it took me a while to find the best documentation on the kit which is in a file called swru151a.pdf. If this document had been included in with the kit it would have saved me a lot of time and would have made it much friendly. Also when using the kit make sure you connect the target boards to the USB dongle and battery boards correctly. The connector isn't polarized and it is easy to connect them the wrong way. When you do this the target board becomes very warm but thankfully wasn't damaged when I accidentally did this for a few seconds a couple of times.

 

 
That small drawback aside this has to be the best ZigBee development kit I have come across so far and I will certainly be using it to prototype a number of projects I have planned in the future.

 

 
 
  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Ian - Thanks for the review. Regarding your comments on the lack of documentation, that is intentional to a point. We do try to keep the printing and paper usage in our kits to a minimum, but hopefully not at the expense of the experience. For kits and EVMs, we associate all the user guides and related application notes to our tool folders on ti.com.

     

    We also do have a great deal of forum discussions about the eZ430-RF2480 on TI's E2E Community and more user generated content in the MSP430 wiki when you are ready to try some additional programming and future projects.

     

    Thanks again for the feedback.

     

    Jeff

    Texas Instruments