Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Early Review: Freescale RD3803MMA7660FC evaluation kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 2752 subscribers
  • Views 1940 views
  • Users 0 members are here
  • freescaleroadtest
Related

Early Review: Freescale RD3803MMA7660FC evaluation kit

gordonmx
gordonmx over 16 years ago

I received my Freescale Acceleration Sensor (RD3803MMA7660FC) evaluation kit last Friday (01/05) and was excited to try it out.  This is an early review.

 

Everything needed was in the box I received, well almost.  The kit comes with a very easy to follow setup sheet and CD.  I inserted the CD into my HP laptop, as instructed, but the install program wouldn't run from the CD.  I finally had to manually copy the installation zip file to my laptop.  The USB to serial (VCP) driver would not install on my MS Vista operating system.  After hunting through the CD, I ended up at www.ftdichip.com for the latest driver (2.06.00), which loaded fine.  Well maybe not so fine since I lost USB connection to my printer.

 

But now I could run the demo software.  There are several demos provided with the kit and they ran without problems.  Each one demonstrates a different feature of the acceleration sensors.  There is certainly more to explore with the sensors.

 

I was very disappointed with a short video included with the kit.  Not with the content, but the quality.  It was the worst video I have seen in a long while (including some home videos).  The last few minutes are used to point out different components on the board, but the picture is so out-of-focus you can't see anything.

 

I hope to have more to say about the sensors in the near future and I look forward to the comments of other reviewers.

 

Thank you Alistair for the opportunity to evaluate this kit.

 

 

Gordon Margulieux

gordon.margulieux@garmin.com

  • Sign in to reply
  • Cancel
Parents
  • firatkocak
    firatkocak over 16 years ago

    hi Friends,

     

    I just recevied my Freescale RD3803MMA7660FCRD3803MMA7660FC evaluation kit. It is very compact. As soon as i got it, i started to install it. And it was installed easily with no any problem. Because i was in hurry to give it a try, i did not read the installation guide first and directly plugged it into usb port. Windows found a new hardware but it failed to find the necessary driver, even i point the driver directory in the cd. So i read the installation guide then and fallowed the steps. First i installed the application and then windows found the new hardware and then i pointed the driver as written in the guide and installation successfully  finished. And then i started the application. application remembered the new hardware and i faced a window including many selections for different test purposes. So it has 3-axis sensor and the senitivity is very precise for x-,x+,y-,y+ but for z-, z+ you should make suddent movements. I do not know, maybe it is just for demo purposes. After i finished detailed tests, this may be not true.

     

    Anyway, i am happy with my new kit. I think, a few days will be enough to write a detailed review. I will post it here when my review is ready.

     

    Best regards,

     

    FIRAT KOCAK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • firatkocak
    firatkocak over 16 years ago

    hi Friends,

     

    I just recevied my Freescale RD3803MMA7660FCRD3803MMA7660FC evaluation kit. It is very compact. As soon as i got it, i started to install it. And it was installed easily with no any problem. Because i was in hurry to give it a try, i did not read the installation guide first and directly plugged it into usb port. Windows found a new hardware but it failed to find the necessary driver, even i point the driver directory in the cd. So i read the installation guide then and fallowed the steps. First i installed the application and then windows found the new hardware and then i pointed the driver as written in the guide and installation successfully  finished. And then i started the application. application remembered the new hardware and i faced a window including many selections for different test purposes. So it has 3-axis sensor and the senitivity is very precise for x-,x+,y-,y+ but for z-, z+ you should make suddent movements. I do not know, maybe it is just for demo purposes. After i finished detailed tests, this may be not true.

     

    Anyway, i am happy with my new kit. I think, a few days will be enough to write a detailed review. I will post it here when my review is ready.

     

    Best regards,

     

    FIRAT KOCAK