Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum [RoadTest] "Freescale RD3803MMA7660FC Review - Serial Communication"
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 2751 subscribers
  • Views 2007 views
  • Users 0 members are here
  • rd3803mma7660fc
  • freescale
  • accelerometer
  • serial
Related

[RoadTest] "Freescale RD3803MMA7660FC Review - Serial Communication"

espanholito
espanholito over 16 years ago

Hello all,

 

First of all i would like to thank Alistair for giving me this opportunity to test this equipment.

 

I received my kit yesterday, and soon started exploring it.

 

As Xavier CHAZE said in the other discution(http://www.element-14.com/community/message/6561#6561), this kit is compose by three components: a freescale uC, a FTDI USB-serial chip, and the  accelerometer.

 

Also with the kit is some documentation and a cd to install a applications which allows to explore some of the features of the accelerometer, like tilt, shake, tap, and orientation detection.

 

As there are already some reviews on this kit, i decided not to talk about what others have already talk, and start to discover a bit of the kit. First i have installed the freescale application which didn't work on my windows 7 x64:(

I had to install it on a windows xp machine to work.

 

As the kit has a USB-Serial Converter, you can develop your computer applications to "talk" to the freescale uC in order to receive the sensor data. And this was what I have done, first I had to discover the communications parameteres:

 

Baudrate: 38400

Data Bits: 8

Stop Bits: 1

Parity: None

Handshake: None

 

Then, using a serial port monitor I spied the communication beetween the freescale application and the board.

 

In order to start receiving data from the board you have to send a couple of bytes:

 

Hexadecimal:

 

0x20; 0x48; 0x54; 0x31; 0x53; 0x31; 0x41; 0x41; 0x0D

0x20; 0x48; 0x54; 0x31; 0x53; 0x31; 0x41; 0x41; 0x0D

0x20; 0x73; 0x31; 0x41; 0x41; 0x0D

0x20; 0x62; 0x37; 0x41; 0x41; 0x0D

 

As you can see, all the messages start with 0x20 and end with 0x41; 0x41; 0x0D

 

From this point the uC will start to send the accelerometer data. Each message starts with 0x20; 0x43 and ends with 0x41; 0x41; 0x0D

 

Till this point i still haven't time to explore more of the kits commands, but hope to post them here soon.

 

Best Regards,

Marcos

  • Sign in to reply
  • Cancel
Parents
  • gandrewstone
    gandrewstone over 16 years ago
    There's a spec on the freescale site that describes the serial protocol.  That might save you some time!
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to gandrewstone

    Where can you find more information about this?

     

    I can only see the i2c specs for the chip itself but no further serial specs for the devkit itself.

     

    Do you know which mode is initialized with what you found?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gandrewstone
    gandrewstone over 16 years ago in reply to e14 Contributor

    Ok ok I'll dig it up again! :-)

     

    http://cache.freescale.com/files/sensors/doc/app_note/AN3945.pdf?fsrch=1


    Or just go the the freescale site and search for:

    RD3803MMA7660FCRD3803MMA7660FC protocol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gandrewstone
    gandrewstone over 16 years ago in reply to e14 Contributor

    Ok ok I'll dig it up again! :-)

     

    http://cache.freescale.com/files/sensors/doc/app_note/AN3945.pdf?fsrch=1


    Or just go the the freescale site and search for:

    RD3803MMA7660FCRD3803MMA7660FC protocol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    After a quick look it seems that

    0x20; 0x48; 0x54; 0x31; 0x53; 0x31; 0x41; 0x41; 0x0D

    is actually the handshake response which you would get if you send 0x20; 0x68; 0x0D; so that should not be required.

     

    0x20; 0x73; 0x31; 0x41; 0x41; 0x0D

    changes device mode to 1 (low power 4sps) although I'm not sure what are the two A's for

     

    0x20; 0x62; 0x37; 0x41; 0x41; 0x0D

    is start data logging with 1.2s timer interval (setting 7) , again not sure about the two A's they are not be required

     

    so if you want to start getting samples you can enter 20 73 31 0D and then 20 62 37 0D or in ASCII <space>s1<CR> and then <space>b7<CR>

     

    with 120sps I would only get samples when moving the device, low medium and scope settings work normally

     

    edit:

     

    "Command sent from S08 to PC
    Repeatedly sent when timer interval has elapsed, until stop timer command is sent.
    Byte 0-9 :-binary data from Device Register
    (0x00 – 0x07) and (0x1A – 0x1C)"

     

    this btw is not completely true as all received messages have the format of <space>CxxxxxAA<CR> where the x's are the the actual data so I'm not sure what is the complete output format

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to gandrewstone

    Thanks a plenty image

     

    Can't believe they did not attach this document to the RD3803MMA7660FCRD3803MMA7660FC product itself on the website, other application notes can be found but not this one.

     

     

    Elias