RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Help us select RoadTest kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 2766 subscribers
  • Views 6727 views
  • Users 0 members are here
  • RoadTest
  • international
  • rectifier
  • freescale
  • matrix
  • avago
  • development
  • ir
  • maxim
  • national
  • hawkboard
  • kits
Related

Help us select RoadTest kits

awinning
awinning over 16 years ago
Hi,

We'd like to hear your thoughts on dev kits in the market just now. What  kits interest you, or would you maybe like to see on future RoadTests?  Are there any other type of products you'd like to see on RoadTest?  (before anyone suggests, there's no chance of an iPad appearing in the  near term future image )

To get the conversation started we've pasted 9 possible kits below. Tell  us which of these interest you the most and why? As a disclaimer, I'm  not promising to give away the most popular, but we'll certainly talk to  the manufacturers and your views will help us greatly!


1. National Semiconductor’s LM26420 evaluation board demonstrates the  company's LM26420 based solution.

2. International Rectifier's IRS2540 IRS2540/1 buck converter based  development board helps develop HB-LED applications

3. ST's STM3210E-SK/HT helps start development for the company's ARM  core-based microcontrollers.

4. Maxim's MAX9830A evaluation kit uses a filterless class D amplifier to  drive a mono bridge-tied-load speaker.

5. Matrix Multimedia's EB018 E-blocks CAN bus board allows investigation  of the CAN bus protocol.

6. Avago's HFBR-0410HFBR-0410 fiber optics evaluation kit allows first hand  experience with simple DC to 5MBd TTL compatible components.

7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX 3-axis acceleration sensing demo  board combines demos available for accelerometer applications.

8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

9. Innovate Software Solutions Hawkboard is an open community board with a  feature set based on the TI OMAP L138 processor.
  • Sign in to reply
  • Cancel
Parents
  • Zad
    Zad over 16 years ago

    An interesting selection there! Predictably, I would go with the herd. The smaller products (Class D amp for example) I can hack together quickly and cheaply anyway, the more complex / delicate systems are way too much hassle to mock up a 1-off just to see if it will work, so I nominate:


    3.  ST's STM3210E-SK/HT helps start development for the company's ARM   core-based microcontrollers.

    9. Innovate Software  Solutions Hawkboard is an open community board with a  feature set based  on the TI OMAP L138 processor.

     

    Last year I had a customer come to me with a product design that fitted the Beagleboard Hawkboard pretty closely. It would be interesting to see if I could resurrect it. Who knows! Difficult times out here for pitching new products without having at least a prototype to show.

     

    I would also like to add my weight to the suggestion of a relatively simple FPGA board, maybe one of those with a DIP40 header. Not especially for my use, but because I think it will help many of the technicians and engineers out there get into a product area that is likely to be even bigger business in the not too distant future. They are very difficult to get into at a simple level, yet most engineers only need something fairly basic to use, rather than an all-singing all-dancing box which has so much to offer that it gets in the way of actually using the FPGA. Being greedy, a Xilinx eval board would be top of the list, but there are many 3rd party manufacturers who produce FPGA kits.

     

    More personally, I would like to see Analog Devices boards, particularly DDS and ADC/DAC. The lower end DDSes are very easy to develop with, but the faster gear, and the faster/wider ADC/DACs are very demanding  and need professional dev boards.

     

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Zad
    Zad over 16 years ago

    An interesting selection there! Predictably, I would go with the herd. The smaller products (Class D amp for example) I can hack together quickly and cheaply anyway, the more complex / delicate systems are way too much hassle to mock up a 1-off just to see if it will work, so I nominate:


    3.  ST's STM3210E-SK/HT helps start development for the company's ARM   core-based microcontrollers.

    9. Innovate Software  Solutions Hawkboard is an open community board with a  feature set based  on the TI OMAP L138 processor.

     

    Last year I had a customer come to me with a product design that fitted the Beagleboard Hawkboard pretty closely. It would be interesting to see if I could resurrect it. Who knows! Difficult times out here for pitching new products without having at least a prototype to show.

     

    I would also like to add my weight to the suggestion of a relatively simple FPGA board, maybe one of those with a DIP40 header. Not especially for my use, but because I think it will help many of the technicians and engineers out there get into a product area that is likely to be even bigger business in the not too distant future. They are very difficult to get into at a simple level, yet most engineers only need something fairly basic to use, rather than an all-singing all-dancing box which has so much to offer that it gets in the way of actually using the FPGA. Being greedy, a Xilinx eval board would be top of the list, but there are many 3rd party manufacturers who produce FPGA kits.

     

    More personally, I would like to see Analog Devices boards, particularly DDS and ADC/DAC. The lower end DDSes are very easy to develop with, but the faster gear, and the faster/wider ADC/DACs are very demanding  and need professional dev boards.

     

     

    Mike