RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Help us select RoadTest kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 2766 subscribers
  • Views 6741 views
  • Users 0 members are here
  • RoadTest
  • international
  • rectifier
  • freescale
  • matrix
  • avago
  • development
  • ir
  • maxim
  • national
  • hawkboard
  • kits
Related

Help us select RoadTest kits

awinning
awinning over 16 years ago
Hi,

We'd like to hear your thoughts on dev kits in the market just now. What  kits interest you, or would you maybe like to see on future RoadTests?  Are there any other type of products you'd like to see on RoadTest?  (before anyone suggests, there's no chance of an iPad appearing in the  near term future image )

To get the conversation started we've pasted 9 possible kits below. Tell  us which of these interest you the most and why? As a disclaimer, I'm  not promising to give away the most popular, but we'll certainly talk to  the manufacturers and your views will help us greatly!


1. National Semiconductor’s LM26420 evaluation board demonstrates the  company's LM26420 based solution.

2. International Rectifier's IRS2540 IRS2540/1 buck converter based  development board helps develop HB-LED applications

3. ST's STM3210E-SK/HT helps start development for the company's ARM  core-based microcontrollers.

4. Maxim's MAX9830A evaluation kit uses a filterless class D amplifier to  drive a mono bridge-tied-load speaker.

5. Matrix Multimedia's EB018 E-blocks CAN bus board allows investigation  of the CAN bus protocol.

6. Avago's HFBR-0410HFBR-0410 fiber optics evaluation kit allows first hand  experience with simple DC to 5MBd TTL compatible components.

7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX 3-axis acceleration sensing demo  board combines demos available for accelerometer applications.

8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

9. Innovate Software Solutions Hawkboard is an open community board with a  feature set based on the TI OMAP L138 processor.
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    hi alistar

    surely my favourite options are :

    2, International  Rectifier's IRS2540 IRS2540/1 buck converter based  development board  helps develop HB-LED applications

    because field of DCDC conveter is rapidly growing and there are lots of different good product especially from IR but also the

    high brightness LED field is a very interesting application


    9. Innovate Software Solutions Hawkboard  is an open community board with a  feature set based on the TI OMAP L138 processor.

    is very interesting because i have already use Beagle Board from TI and I think tha OMAP is an amazing microcontroller but at the same

    time I think Hawkboardis better than Beagle especially for the high number of peripheric like LAN, etc,,,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago

    hi alistar

    surely my favourite options are :

    2, International  Rectifier's IRS2540 IRS2540/1 buck converter based  development board  helps develop HB-LED applications

    because field of DCDC conveter is rapidly growing and there are lots of different good product especially from IR but also the

    high brightness LED field is a very interesting application


    9. Innovate Software Solutions Hawkboard  is an open community board with a  feature set based on the TI OMAP L138 processor.

    is very interesting because i have already use Beagle Board from TI and I think tha OMAP is an amazing microcontroller but at the same

    time I think Hawkboardis better than Beagle especially for the high number of peripheric like LAN, etc,,,